Last updated: November 9, 2010
This section is only applicable to the lab application.
PS
Data E-RGCH Information State
This setting determines whether the E-RGCH Information IE is signaled to the UE during the setup of a PDP context. If this IE is signaled, the UE will listen for up/down/hold commands on the E-RGCH. If it is not signaled, then the UE will not listen to an E-RGCH (and thus will determine its serving grant solely based upon the E-AGCH).
Note, this setting only affects whether the UE will listen to an E-RGCH. It does not affect whether an E-RGCH is transmitted by the test set. To transmit an E-RGCH from the test set, you must set HSPA Cell 1 Connected E-RGCH Level to on (it is on by default).
GPIB command: CALL:HSUPa:SERVice:PSData:ERGChannel:INFormation[:STATe]
This setting can only be changed when the connection status is Idle.
PS Data E-DPDCH Max Channel Codes
This setting is used to control the value for E-DPDCH Max Channelisation Codes that is signaled to the UE during the setup of a PDP context that uses a 10 ms TTI on the E-DCH.
GPIB command: CALL:HSUPa:SERVice:PSData:EDPDchannel:CCODes:MAX
This setting can only be changed when the connection status is Idle.
PS
Data Max Number of HARQ Retransmissions
GPIB command: CALL:HSUPa:HARQ:RETRans:MAXimum
PS Data SRB Mapping Mode
GPIB command: CALL:SERVice:PSData:SRBearer:MAPPing
PS
Data MAC-d PDU Size
GPIB command: CALL:HSUPa:SERVice:PSData:MACD:PDUSize
This setting specifies whether MAC-e/es or MAC-i/is is to be used as the underlying MAC layer entity when working in HSUPA PS Data mode in CELL_DCH state.
GPIB command: CALL:HSUPa:SERVice:PSData:EDCHannel:MAC
This setting can only be changed when the connection status is Idle.
This setting specifies whether uplink AM RLC working in fixed mode or flexible mode when MAC-i/is is used.
GPIB command: CALL:HSUPa:SERVice:PSData:RLC:UPLink:MODE
This setting can only be changed when the connection status is Idle.
Max Flexible AM
RLC PDU Payload Size
This setting specifies the maximum RLC PDU size in uplink AM RLC layer when flexible RLC PDU size is configured.
GPIB command: CALL:HSUPa:SERVice:PSData:RLC:UPLink:MAXimum:PDU:PSIZe
This setting can only be changed when the connection status is Idle.
Min Flexible AM
RLC PDU Payload Size
This setting specifies the minimum RLC PDU size in uplink AM RLC layer when flexible RLC PDU size is configured.
GPIB command: CALL:HSUPa:SERVice:PSData:RLC:UPLink:MINimum:PDU:PSIZe
This setting can only be changed when the connection status is Idle.
This setting specifies the Length Indicator size in uplink AM RLC layer when flexible RLC PDU size is configured.
GPIB command: CALL:HSUPa:SERVice:PSData:RLC:UPLink:LINDicatior:SIZE
This setting can only be changed when the connection status is Idle.