Current Service Type
indicates the type of service that is currently active. While in
Active Cell Operating Mode
,
Current Service Type
is displayed on the
Call Setup Screen
(and can be queried using the
CALL:STATus:SERVice:TYPe?
command).
Current Service Type
is set to the active service type upon completion of the establishment of the service.
The test set supports the following service types:
AMR Voice
(see
AMR Setup
)
AMR Voice + PS Data
(see
Simultaneous Services
) (lab application only)
- HSDPA
(
lab application or feature-licensed test application only
)
- HSPA
(lab application or feature-licensed test application only)
-
Video Call
(lab application only or feature-licensed test application only)
- Asynchronous
(lab application only)
- HSDPA
(
lab application only
)
- HSPA
(
lab application only
)
Current Service Type
is set to
None
whenever an event occurs that causes the service to be stopped. For example:
End Call
(base station release).