|
|
|
Last updated: October 30, 2013
The following AMR Sources are available in the test set:
While in ECHO , the test set loops the transport blocks arriving from the UE on the uplink back down to the UE (unaltered) on the downlink. There is a fixed voice echo delay of 0.5 seconds.
While in External 8960, the traffic data is routed from one UE through an 8960, over the LAN interface to a second 8960 and then to the second UE. The data flow is bidirectional and so the behaviour at each UE is like that of a real speech call.
While in PESQ (Perceptual Evaluation of Speech Quality), the test set generates the speech signal which complies with the ITU-T P.862 standard for the Perceptual Evaluation of Speech Quality measurement. See Perceptual Evaluation of Speech Quality (PESQ) Measurement Description .
GPIB command: CALL:SERVice:AMR:SOURce
This parameter can only be set when call/data status is idle.
The AMR Radio Access Bearer can be set to:
GPIB command: CALL:SERVice:AMR:RAB
This parameter can only be set when call/data status is idle. Note: "k" refers to kbps.
This setting specifies the data rate of DCCH used for AMR voice connection when AMR Radio Access Bearer is set to 5.15k Voice or 4.75k Voice .
BPS1700 , the TTI for DCCH is set to 80ms.BPS3400 , the TTI for DCCH is set to 40ms.GPIB command: CALL:SERVice:AMR:SRB
This parameter can not be changed in Active Cell operating mode and the Call/Data Status is not Idle .
|
|
Manual Operation: How Do I Configure the AMR Radio Access Bearer?
Downlink Channel Codes and Levels
|
|
|
|
|