RB Test Mode connection between the UE and
test set (see How Do I Set Up a
Call and Make a Connection? ). Code Domain . Code Domain Setup ( F1 ) and set the measurement parameters
as needed. Select Close
Menu ( F6 ). Cell Power (
F7 ) as needed. Trigger Arm is set
to Single , you
must press the START SINGLE key
to begin the measurement. Axis Control (
F2 ). Set the axis control parameters as needed.
Select Return ( F6 ). Marker (
F3 ) to turn on the marker on the graphical display.A typical result is shown below.
This section is applicable to the lab application or feature-licensed test application only.
Operating Mode (
F1 ) to Cell
Off . 34.121 Preset Call
Configurations (
F11 on Call
Parms 1 of 3 ) and select 5.2C,5.7A,5.13.1AA,5.13.2A:HSDPA:QPSK
. You may then skip any steps marked with [34.121 Call Config] in
this procedure. Channel (UARFCN) Parms
( F12 on Call Parms 1 of 3
). Set DL Channel
( F7 ) to the
appropriate "mid range" frequency
for your UE's operating band, as specified
by 3GPP TS 34.108 5.1.1 (for example, for
operating band II set
DL Channel =
9800 ).Call Control
2 of 6 ).Default
DPCH Offset
(DOFF) to
3 x 512 chips. Uplink Parameters
( F4 on Call Control 2 of
6 ).
Uplink DPCH Bc/Bd Control to Manual
.
Manual Uplink DPCH Bc to
2 (for 34.121-1 v8.10.0 Table C.10.1.4
sub-test 1).
Manual Uplink DPCH Bd to
15 (for 34.121-1 v8.10.0 Table
C.10.1.4 sub-test 1).
Maximum Uplink Transmit Power Level to +21 dBm
. Operating Mode to Active Cell
(pressing the CALL SETUP
key quickly brings you back to the top
level Call Control
menu). Cell Power ( F7 on
Call Parms 1 of 3 ) to
-86 dBm/3.84 MHz . Channel Type ( F8 ) to
12.2k RMC + HSDPA . Generator Info ( F3 on
Call Control 2 of 6 ), select Downlink
Channel Levels (
F3 ), select
Connected DL Channel Levels ( F3
), then select HSDPA
Conn DL Channel Levels (
F4 ).
HSDPA Cell 1 Connected CPICH Level to -10 dB (this
is the default value). HSDPA Cell 1 Connected
P-CCPCH/SCH Level to
-12 dB (this is the default value). HSDPA Cell 1 Connected
PICH Level to
-15 dB (this is the default value). HSDPA Cell 1 Connected
DPCH Level to
-9 dB. HSDPA Cell 1 Connected
HS-PDSCHs Level (Sum) to
-3 dB (this is the default value). HSDPA Cell 1 Connected
HS-SCCH 1 Level to
-8 dB . HSDPA Parameters (HSPA Parameters
( F10 ), F10
).
HSDPA
RB Test Mode Setup (
F8 ), then select HSDPA
RB Test Mode Settings (
F8 ).
RB Test HS-DSCH Configuration Type to FRC (this
is the default value).
FRC Type to
H-Set 1 QPSK (this is the default
value).
MAC-(e)hs Parameters (
F10 ).
HSDPA Uplink Parameters
( F11 ).
Cell
Parameters ( F2 ).
Cell Info ( F2 ),
then Cell Parameters
( F2 ). Call Control
2 of 6 menu)
PS Domain Information to
Present (this is the default value
in the lab application). Cell Info
, Reselection
Parameters ( F3
). RB Test Mode Setup ( F6 on
Call Control 3 of 6 ) and set
UE Loopback Type to
Type 1 (this is the default value). UL CL Power Ctrl Parameters
( F8 on
Call Parms 3 of 3 ) and set
UL CL Power Ctrl Algorithm to
Two (this is the default value). PS Domain
Information parameter must be set to Present when the
UE registers (attaches) with the test set. Originate Call ( F3 on
Call Control 1 of 6 ).
UL CL Power Ctrl Parameters (
F8 on Call
Parms 3 of 3 ) and set
UL CL Power Ctrl Mode to
Active bits (this is the default value)
. UE Target Power ( F7 on
Call Parms 3 of 3 ) to
0 dBm .UL CL Power Ctrl
Parameters ( F8
on Call Parms
3 of 3 ). Set UL
CL Power Ctrl Mode to Alternating
bits . Code Domain
. Code Domain Setup ( F1 ) . Set
Trigger Source to
HS-DPCCH. Set
Measurement Interval to
0.5 slot.| Measurement Point | Subframe Alignment | Slot Alignment | Subslot Alignment |
|---|---|---|---|
| 1 | 5 | CQI2 |
0.5 |
| 2 | 0 | ACKNACK |
0 |
| 3 | 0 | CQI1 | 0 |
| 4 | 1 | ACKNACK | 0 |
Graph Control ( F2
) and set Table
( F3 ) to 2 (so that you
can compare the NCDP result with 3GPP TS 34.121-1
Table 5.2C.4).
Marker ( F2 under
Graph Control ( F2
)) to ensure that the RCDPA result for each
code channel meets the specified requirements
in 34.121-1 Table 5.2C.3. The code channels
are located as follows:
| Code Channel | Location | Marker |
|---|---|---|
| DPCCH | Q Cch,256,0 | 0 |
| DPDCH | I Cch,64,16 | 64 |
| HS-DPCCH | Q Cch,256,64 | 64 |
Handovers ( F5 )) to change the following
settings:
| Setting | Sub-test 2 | Sub-test 3 | Sub-test 4 |
|---|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 12 |
15 | 15 |
| TCR Manual Uplink DPCH Bd | 15 | 8 |
4 |
| TCR DeltaACK, DeltaNACK | 8 | 8 | 8 |
| DeltaCQI | 7 | 7 | 7 |
| TCR Ack-Nack Repetition Factor | 1 | 1 | 1 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 1 | 1 | 1 |
This section is applicable to the lab application or feature-licensed test application only.
Operating Mode ( F1
) to Cell Off
. 34.121 Preset Call Configurations
( F11 on
Call Parms 1 of 3 ) and select 5.2D:HSPA:QPSK
. You may then skip any steps marked with
[34.121 Call Config] in this procedure. Channel (UARFCN) Parms
( F12 on
Call Parms 1 of 3 ). Set
DL Channel ( F7 )
to the appropriate "mid range" frequency
for your UE's operating band, as specified by
3GPP TS 34.108 5.1.1 (for example, for operating
band II set DL Channel
= 9800
). Uplink Parameters ( F4 on
Call Control 2 of 6 ).
Uplink DPCH Bc/Bd Control to
Manual . Manual Uplink DPCH
Bc to
11 (for 34.121-1 v8.10.0 Table C.11.1.3
sub-test 1). Manual Uplink DPCH
Bd to
15 (for 34.121-1 v8.10.0 Table C.11.1.3
sub-test 1). Maximum Uplink Transmit
Power Level to
+21 dBm . Operating Mode to Active Cell (pressing
the CALL SETUP key quickly
brings you back to the top level
Call Control menu). Cell Power (
F7 on Call Parms
1 of 3 ) to -86
dBm/3.84 MHz . Channel Type (
F8 ) to 12.2k RMC
+ HSPA . Generator Info ( F3 on
Call Control 2 of 6 ), select Downlink
Channel Levels (
F3 ), select Connected
DL Channel Levels ( F3
), then select HSPA Conn
DL Channel Levels ( F4
).
HSPA Cell 1 Connected CPICH Level to -10 dB (this is
the default value). HSPA Cell 1 Connected
P-CCPCH/SCH Level to
-12 dB (this is the default value). HSPA Cell 1 Connected
PICH Level to
-15 dB (this is the default value). HSPA Cell 1 Connected
(F-)DPCH Level to
-10 dB (this is the default value). HSPA Cell 1 Connected
E-AGCH Level to
-20 dB (this is the default value). HSPA Cell 1 Connected
E-HICH Level to
-20 dB (this is the default value). HSPA Cell 1 Connected
E-RGCH Level to
Off (this is the default value). HSPA Cell 1 Connected
HS-PDSCHs Level (Sum) to
-3 dB (this is the default value). HSPA Cell 1 Connected
HS-SCCH 1 Level to
-8 dB .
HSUPA Parameters (
HSPA Parameters ( F10
), F9 ).
HSUPA RB Test Mode Setup (
F8 ).
Common HSUPA Parameters
( F9 ).
E-DPCCH/DPCCH Power Offset (DeltaE-DPCCH)
to 6 (for
34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Note, 34.121-1 Table C.11.1.3 provides Beta ec (209/225 for sub-test
1). To determine what value of DeltaE-DPCCH
corresponds to this, use 3GPP TS 25.213 Table
1B and the value of Beta
c from 34.121-1 Table C.11.1.3 (11/15
for sub-test 1). For sub-test 1, A
ec = Beta ec
/Beta c = (209/225)/(11/15)
= 19/15; therefore DeltaE-DPCCH = 6. Reference E-TFCI Power
Offsets to
Definition 34.121-01 (for 34.121-1
v8.10.0 Table C.11.1.3 sub-test 1). Serving Grant ( F10 ).
RB Setup AG to
26: (119/15)^2 (for34.121-1 v8.10.0
Table C.11.1.3 sub-test 1). Note, 34.121-1
Table C.11.1.3 AG Index corresponds to 3GPP
TS 25.212 s4.10.1A.1 Table 16B, which maps
the Absolute Grants sent on the E-AGCH. To
send the equivalent Absolute Grant in the
RB Setup message, you must use the AG Index
in 3GPP TS 25.321 s9.2.5.2.1.1 Table 9.2.5.2.1.1.AG Mode
( F7 ) to Single
Shot (this is the default value). AG Pattern Parameters
( F11 ):
HSDPA Parameters ( HSPA Parameters ( F10 ), F10
).
Cell
Parameters ( F2 ).
Cell Info ( F2 ), then Cell Parameters ( F2 ). Call Control
2 of 6 menu)
PS Domain Information to
Present (this is the default value in the
lab application). Cell Info , Reselection Parameters
( F3 ). RB Test Mode Setup ( F6 on
Call Control 3 of 6 ) and set
UE Loopback Type to
Type 1 (this is the default value). UL CL Power Ctrl Parameters
( F8 on
Call Parms 3 of 3 ) and set
UL CL Power Ctrl Algorithm to
Two (this is the default value). PS Domain Information parameter
must be set to Present
when the UE registers (attaches) with the test
set. Originate Call ( F3 on
Call Control 1 of 6 ).
UL CL Power Ctrl Parameters (
F8 on Call Parms
3 of 3 ) and set
UL CL Power Ctrl Mode to
Active bits (this is the default value)
. UE Target Power ( F7 on
Call Parms 3 of 3 ) to
1 dBm (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test
1). This value is determined as follows:
UE Target Power only
sets the DPCCH+DPDCH power level of the UE. In
order to achieve a total output power of +15 dBm
+/-24 dB, you must set
UE Target Power to 15 dBm - Power
change due to HS-DPCCH, E-DPCCH and E-DPDCH
.
UE Target Power to 1 dBm for sub-test 1. UE Target Power
values for sub-tests 2-4 are as follows:
sub-test 2: 10 dBm, sub-test 3: 2 dBm, sub-test
4: 13 dBm.Additional Screens
( F1 from Call
Control 2 of 6 ), select HSPA
Information ( F2
) and observe the Last Received E-TFCI (it should
be 75 for 34.121-1 v8.10.0 Table C.11.1.3 sub-test
1, 67 for sub-test 2, 92 for sub-test 3, and 71
for sub-test 4). If the E-TFCI value is not correct,
fail the UE. Note that an E-TFCI of 75 corresponds
to an uplink data rate of 2421 bits/10 ms = 242
kbps. The uplink data rate for sub-test 2 = 175
kbps, sub-test 3 = 483 kbps, and sub-test 4 =
206 kbps.UL CL Power Ctrl
Parameters ( F8 on
Call Parms 3 of 3
). Set UL CL Power
Ctrl Mode to Alternating
bits . HSPA Parameters ( F10 ),
HSUPA Parameters ( F9
), Serving Grant ( F10 ) and set
AG Mode ( F7 ) to Pattern .
Code Domain . Code Domain Setup ( F1 ) and set
Trigger Source to
Even Frame .| Measurement Point | Timeslot | SFN Alignment |
|---|---|---|
| 1 | 14 | Odd |
| 2 | 0 | Even |
| 3 | 0 | Odd |
Graph Control ( F2
) and set Table ( F3 ) to 2
(so that you can compare the NCDP result
with 3GPP TS 34.121-1 table 5.2D.7).
Marker ( F2 under
Graph Control ( F2
)) to ensure that the RCDPA result for each code
channel meets the specified requirements in 34.121-1
table 5.2D.8. The code channels are located as
follows:
| Code Channel | Location | Marker |
|---|---|---|
| DPCCH | Q Cch,256,0 | 0 |
| DPDCH | I Cch,64,16 | 64 |
| HS-DPCCH | Q Cch,256,64 | 64 |
| E-DPCCH | I Cch,256,1 | 1 |
| E-DPDCH1 | I Cch,4,2 | 128 |
| E-DPDCH2 | Q Cch,4,2 | 128 |
HSPA Parameters ( F10
), HSUPA Parameters
( F9 ),
Serving Grant ( F10
) and set AG Mode
( F7 ) to Single
Shot .
Handovers ( F5 ))
to change the following settings:
| Setting | Sub-test 2 | Sub-test 3 | Sub-test 4 |
|---|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 6 | 15 | 2 |
| TCR Manual Uplink DPCH Bd | 15 | 9 | 15 |
| TCR DeltaACK, DeltaNACK, DeltaCQI | 8 | 8 | 8 |
| TCR Ack-Nack Repetition Factor | 3 | 3 | 3 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 2 | 2 | 2 |
| TCR E-DPCCH/DPCCH Power Offset | 8 | 8 | 5 |
| TCR Reference E-TFCI Power Offsets | 34121-01 | 34121-02 | 34121-01 |
| TCR Absolute Grant | 18: (47/15)^2 | 21: (67/15)^2 | 23: (84/15)^2 |
HSPA Parameters ( F10 ),
HSUPA Parameters ( F9
), Serving Grant
( F10 ),
AG Pattern Parameters (
F11 ) and set
Absolute Grant Pattern - Value 1 to 12: (47/15)^2 for
sub-test 2, 15: (67/15)^2
for sub-test 3 and 17:
(84/15)^2 for sub-test 4. AG Mode (
F7 ) to Pattern
.This section is applicable to the lab application or feature-licensed test application only.
UE Relative Code Domain Power Accuracy for HS-DPCCH and E-DCH with 16QAM from 3GPP TS 34.121-1 s5.2E measures RCDPA on any release 7 or later UE that supports E-DCH category 7, 16QAM with HSUPA.
The test is performed with the UE transmitting at the maximum power.
Operating
Mode ( F1 ) to Cell Off . 34.121 Preset Call
Configurations ( F11
on Call Parms
1 of 3 ) and select 5.2E:HSPA+:UL
16QAM . You may then skip any steps marked
with [34.121 Call Config]
in this procedure. Channel (UARFCN)
Parms ( F12 on Call Parms 1 of 3
). Set DL Channel
( F7 ) to the appropriate
"mid range" frequency for your UE's
operating band, as specified by 3GPP TS 34.108
s5.1.1 (for example, for operating band II set
DL Channel = 9800 ).Uplink Parameters
( F4 on Call
Control 2 of 6 ).
Uplink
DPCH Bc/Bd Control to Manual
. Manual Uplink
DPCH Bc to 15
(for 34.121-1 v8.10.0 table C.11.1.4 sub-test
1). Manual Uplink
DPCH Bd can remain at its default value.
34.121-1 v8.10.0 table C.11.1.4 sub-test 1
requires Beta d
set to zero. This is configured by selecting
a DL channel type with no DPDCH. The value
set here for Beta d
is not used because no DL DPDCH is generated.Maximum Uplink
Transmit Power Level to +21
dBm .Operating Mode
to Active Cell
(pressing the CALL SETUP
key quickly brings you back to the top level Call Control menu).Cell Power ( F7 on Call
Parms 1 of 3 ) to -86
dBm/3.84 MHz . Channel Type ( F8
) to HSPA . Generator Info
( F3 on Call
Control 2 of 6 ), select Downlink
Channel Levels ( F3 ),
Connected DL Channel
Levels ( F3 ), then select
HSPA Conn DL Channel
Levels ( F4 ).
HSPA
Cell 1 Connected CPICH Level to -10
dB (this is the default value). HSPA Cell 1 Connected
P-CCPCH/SCH Level to -12
dB (this is the default value). HSPA Cell 1 Connected
PICH Level to -15
dB (this is the default value). HSPA Cell 1 Connected
(F-)DPCH Level to -10
dB (this is the default value). HSPA Cell 1 Connected
E-AGCH Level to -20
dB (this is the default value). HSPA Cell 1 Connected
E-HICH Level to -20
dB (this is the default value). HSPA Cell 1 Connected
E-RGCH Level to Off
(this is the default value). HSPA Cell 1 Connected
HS-PDSCHs Level (Sum) to -3
dB (this is the default value). HSPA Cell 1 Connected
HS-SCCH 1 Level to -8
dB . Generator Info (
F3 on Call
Control 2 of 6 ), select Downlink
Channel Configs ( F4
), and then select HS-SCCH
Configs ( F3 ).
HSUPA Parameters
( HSPA Parameters (
F10 ), F9
).
HSUPA
RB Test Mode Setup ( F8
).
Common HSUPA Parameters
( F9 ).
E-DCH
TTI to 2
ms . E-DCH 16QAM
State to
On .E-DPCCH/DPCCH
Power Offset (DeltaE-DPCCH) to 8 (for 34.121-1
v8.10.0 table C.11.1.4 sub-test 1). Note,
34.121-1 table C.11.1.4 provides Beta ec (30/15 for sub-test
1). To determine what value of DeltaE-DPCCH
corresponds to this, use 3GPP TS 25.213 table
1B and the value of Beta
c from 34.121-1 table C.11.1.4 (15/15
for sub-test 1). For sub-test 1, A
ec = Beta ec
/Beta c = (30/15)/(15/15)
= 30/15; therefore DeltaE-DPCCH = 8. E-TFCI Table
Index (2 ms TTI with 16QAM) to 2 (this is the
default value).Reference
E-TFCI Power Offset Control to Predefined (this
is the default value). Reference
E-TFCI Power Offsets to Definition
34.121-04 (for 34.121-1 v8.10.0 table
C.11.1.4 sub-test 1). E-TFCI Boost
Information State to On
.E-TFCI Boost
Value to 105
.DeltaT2TP
to 2 (this
is the default value).BetaEd Gain
E-AGCH Table Selection to 1
(this is the default value).E-DPDCH Power
Calculation Formula to Extrapolation
(this is the default value).Serving Grant
( F10 ).
AG
Mode ( F7 ) = Single
Shot (this is the default value). RB Setup
AG to 17:
(75/15)^2 (for 34.121-1 v8.10.0 table
C.11.1.4 sub-test 1). Note, 34.121-1 table
C.11.1.4 AG Index corresponds to 3GPP TS 25.212
s4.10.1A.1 table 16B.1, which maps the Absolute
Grants sent on the E-AGCH. To send the equivalent
Absolute Grant in the RB Setup message, you
must use the AG Index in 3GPP TS 25.321 s9.2.5.2.1.1
table 9.2.5.2.1.2. AG Pattern Parameters
( F8 ):
HSDPA Parameters
( HSPA Parameters (
F10 ), F10
).
Cell
Parameters ( F2 ).
Lab
Application: Select Cell
Info ( F2 ), then Cell Parameters ( F2 ) from the Call
Control 2 of 6 menu.
PS
Domain Information to Present
(this is the default value in the lab application).
Cell Info , Reselection Parameters
( F3 ). RB Test Mode Setup
( F6 on Call
Control 3 of 6 ) and set UE
Loopback Type to
Type 1 (this is the default value). UL CL Power Ctrl Parameters
( F8 on Call
Parms 3 of 3 ) and set UL
CL Power Ctrl Algorithm to Two
(this is the default value). Originate Call
( F3 on Call
Control 1 of 6 ). UL
CL Power Ctrl Parameters ( F8
on Call Parms 3 of
3 ) and set UL
CL Power Ctrl Mode to Active
bits (this is the default value). UE Target Power
( F7 on Call
Parms 3 of 3 ) to 3
dBm (for 34.121-1 v8.10.0 table C.11.1.4
sub-test 1, power class 3 UE). This value is determined
as follows: Maximum power for a power class 3
UE is +24 dBm, but UE Target Power only sets the
DPCCH+DPDCH power level of the UE. In order to
achieve a total output power of +16.5 dBm (24
dBm - 7.5 dB as required in 34.121-1 s5.2B.4.2),
you must set UE Target Power to at most 16.5 dBm
- Power change due to HS-DPCCH, E-DPCCH and E
DPDCH.
Power Change Due to HS-DPCCH, E-DPCCH and E-DPDCH = 10log 10 (Beta c ^2 + Beta d ^2 + Beta hs ^2 + Beta ec ^2 + Beta ed1 ^2 + Beta ed2 ^2 + Beta ed3 ^2 + Beta ed4 ^2) - 10log 10 (Beta d ^2 + Beta c ^2) = 13.4 dB for sub-test 1, so you must set UE Target Power to 3 dBm for sub-test 1.
Channel Power .
UL CL Power Ctrl
Parameters ( F8 on
Call Parms 3 of 3
). Set UL CL Power
Ctrl Mode to Alternating
bits . Additional Screens
( F1 from
Call Control 2 of 6 ), select HSPA
Information ( F2
) and observe the
Last Received E-TFCI (it should be 105
for 34.121-1 v8.10.0 table C.11.1.4 sub-test 1).
E-TFCI Recording
Information ( F3
). HSPA Parameters
( F10 ), HSUPA
Parameters ( F9 ),
E-TFCI Recording
( F11 ), E-TFCI
Recording Parameters ( F7
).
E-TFCI
Recording Count to 15
(this is the default value). E-TFCI Recording
Behavior to All
. Send Step Up
TPC Bit Pattern ( F10 ) and then Start Recording E-TFCI
Values ( F8 ).
Send Step Down TPC
Bit Pattern ( F11
) and then Start
Recording E-TFCI Values ( F8
). HSPA Parameters (
F10 ), HSUPA
Parameters ( F9 ), Serving Grant ( F10
) and set AG Mode
to Pattern ( F7 ). Code
Domain Setup ( F1
).
| Measurement Point | Timeslot | SFN Alignment |
|---|---|---|
| 1 | 14 | Odd |
| 2 | 0 | Even |
| 3 | 0 | Odd |
Graph
Control ( F2 ) and
setting Table
( F3 ) = 2
so that you can compare NCDP with 3GPP TS 34.121
table 5.2D.7. Graph Control (
F2 ) ) to ensure that RCDPA
for each code channel meets the specified requirements
in 34.121-1 table 5.2E.6. The code channels are
located as follows (as defined in 3GPP TS 25.213):
| Code Channel | Location | Marker |
|---|---|---|
| DPCCH | Q Cch,256,0 | 0 |
| E-DPCCH | I Cch,256,1 | 1 |
| E-DPDCH1 | I Cch,2,1 | 128 |
| E-DPDCH2 | Q Cch,2,1 | 128 |
| E-DPDCH3 | I Cch,4,1 | 64 |
| E-DPDCH4 | Q Cch,4,1 | 64 |
This section is applicable to the lab application or feature-licensed test application only.
EVM and IQ Origin Offset for H-DPCCH and E-DCH with 16QAM from 3GPP TS 34.121-1 s5.13.1AAA measures EVM and IQ origin offset power on any release 7 or later UE that supports E-DCH category 7, 16QAM with HSUPA.
The test is performed with the UE transmitting at -28 dBm.
Operating
Mode ( F1 ) to Cell Off . 34.121 Preset Call
Configurations ( F11
on Call Parms 1 of
3 ) and select 5.13.1AAA,
5.13.2C:HSPA+:UL 16QAM . You may then skip
any steps marked with [34.121
Call Config] in this procedure. Channel (UARFCN)
Parms ( F12 on Call Parms 1 of 3
). Set DL Channel
( F7 ) and Uplink
Channel ( F8 ) to
the appropriate "low range" frequencies
for your UE's operating band, as specified by
3GPP TS 34.108 s5.1.1 (for example, for operating
band II, set DL Channel = 9663 ). Uplink Parameters
( F4 on Call
Control 2 of 6 ).
Uplink
DPCH Bc/Bd Control to Manual
. Manual Uplink
DPCH Bc to 15
(for 34.121-1 v8.10.0 table C.11.1.4 sub-test
1). Manual Uplink DPCH
Bd can remain at its default value.
34.121-1 v8.10.0 table C.11.1.4 sub-test 1
requires Beta d
set to zero. This is configured by selecting
a DL channel type with no DPDCH. The value
set here for Beta d
is not used because no DL DPDCH is generated.Maximum Uplink
Transmit Power Level to +21
dBm . Operating Mode
to Active Cell
(pressing the CALL SETUP
key quickly brings you back to the top level Call Control menu).
Cell Power ( F7 on Call
Parms 1 of 3 ) to -86
dBm/3.84 MHz . Channel Type ( F8
) to HSPA . Generator Info
( F3 on Call
Control 2 of 6 ), select Downlink
Channel Levels ( F3 ),
Connected DL Channel
Levels ( F3 ), then select
HSPA Conn DL Channel
Levels ( F4 ).
HSPA
Cell 1 Connected CPICH Level to -10
dB (this is the default value). HSPA Cell 1 Connected
P-CCPCH/SCH Level to -12
dB (this is the default value). HSPA Cell 1 Connected
PICH Level to -15
dB (this is the default value). HSPA Cell 1 Connected
(F-)DPCH Level to -10
dB (this is the default value). HSPA Cell 1 Connected
E-AGCH Level to -20
dB (this is the default value). HSPA Cell 1 Connected
E-HICH Level to -20
dB (this is the default value). HSPA Cell 1 Connected
E-RGCH Level to Off
(this is the default value). HSPA Cell 1 Connected
HS-PDSCHs Level (Sum) to -3
dB (this is the default value). HSPA Cell 1 Connected
HS-SCCH 1 Level to -8
dB . Generator Info
( F3 on Call
Control 2 of 6 ), select
Downlink Channel Configs ( F4
), and then select HS-SCCH
Configs ( F3 ).
HSUPA Parameters
( HSPA Parameters
( F10 ), F9
).
HSUPA
RB Test Mode Setup ( F8
).
Common HSUPA Parameters
( F9 ).
E-DCH
TTI to 2
ms .E-DCH 16QAM
State to On
.E-DPCCH/DPCCH
Power Offset (DeltaE-DPCCH) to 8 (for 34.121-1
v8.10.0 table C.11.1.4 sub-test 1). Note,
34.121-1 table C.11.1.4 provides Beta ec (30/15 for sub-test
1). To determine what value of DeltaE-DPCCH
corresponds to this, use 3GPP TS 25.213 table
1B and the value of Beta
c from 34.121-1 table C.11.1.4 (15/15
for sub-test 1). For sub-test 1, A ec
= Beta ec /Beta c = (30/15)/(15/15)
= 30/15; therefore DeltaE-DPCCH = 8. E-TFCI Table
Index (2 ms TTI with 16QAM) to 2 (this is the
default value).Reference
E-TFCI Power Offset Control to Predefined (this
is the default value). Reference
E-TFCI Power Offsets to Definition
34.121-04 (for 34.121-1 v8.10.0 table
C.11.1.4 sub-test 1). 34.121-1 v8.10.0 table
5.2E.2 is used for this configuration; however,
this table is identical to 34.121-1 table
5.13.1AAA.3.E-TFCI Boost
Information State to On
.E-TFCI Boost
Value to 105
.DeltaT2TP
to 2 (this
is the default value).BetaEd Gain
E-AGCH Table Selection to 1
(this is the default value).E-DPDCH Power
Calculation Formula to Extrapolation
(this is the default value).Serving Grant
( F10 ).
AG
Mode to Single
Shot (this is the default value).Single Shot
AG to 14:
(75/15)^2 (for 34.121-1 v8.10.0 table
C.11.1.4 sub-test 1).RB Setup
AG to 17:
(75/15)^2 (for 34.121-1 v8.10.0 table
C.11.1.4 sub-test 1). Note, 34.121-1 table
C.11.1.4 AG Index corresponds to 3GPP TS 25.212
s4.10.1A.1 table 16B.1, which maps the Absolute
Grants sent on the E-AGCH. To send the equivalent
Absolute Grant in the RB Setup message, you
must use the AG Index in 3GPP TS 25.321 s9.2.5.2.1.1
table 9.2.5.2.1.2.HSDPA Parameters
( HSPA Parameters
( F10 ), F10
).
Cell
Parameters ( F2 ).
Lab
Application: Select Cell
Info ( F2 ), then Cell Parameters ( F2 ) from the Call
Control 2 of 6 menu.
PS
Domain Information to Present
(this is the default value in the lab application).
RB Test Mode Setup
( F6 on Call
Control 3 of 6 ) and set UE
Loopback Type to Type
1 (this is the default value).UL CL Power Ctrl Parameters
( F8 on Call
Parms 3 of 3 ) and set UL
CL Power Ctrl Algorithm to Two
(this is the default value). Originate Call
( F3 on Call
Control 1 of 6 ). UL CL Power Ctrl Parameters
( F8 on Call
Parms 3 of 3 ) and set UL
CL Power Ctrl Mode to Active
bits (this is the default value). UE Target Power
( F7 on Call
Parms 3 of 3 ) to -41 dBm. This value is determined
as follows: 34.121-1 s5.13.1AAA requires a UE output
power of -28 dBm ± 2 dB, but UE Target Power only
sets the DPCCH+DPDCH power level of the UE. In order
to achieve a total output power of -28 dBm, you must
set UE Target Power to at most -28 dBm - Power change
due to HS-DPCCH, E-DPCCH and E-DPDCH.Power Change
Due to HS-DPCCH, E-DPCCH and E-DPDCH = 10log
10 (Beta
c ^2 + Beta d ^2
+ Beta hs ^2 + Beta ec ^2 + Beta
ed1 ^2 + Beta ed2
^2 + Beta ed3 ^2 + Beta ed4 ^2) - 10log
10 (Beta d ^2 +
Beta c ^2) = 13.4 dB
for sub-test 1, so you must set UE Target Power to
-41 dBm. UL CL Power Ctrl Parameters
( F8 on Call
Parms 3 of 3 ) and set UL
CL Power Ctrl Mode to Alternating
bits .Code
Domain .
Physical
Channel Reconfig ( F5
on Call Control 1 of
6 , F1 ) to perform a
hard handover to the next channel. Set the Handover
Downlink Channel (UARFCN) and Handover
Uplink Channel (UARFCN) parameters to the appropriate
"mid range" or "high range" frequencies
for your UE's operating band, as specified by 3GPP
TS 34.108 s5.1.1. Execute
Handover ( F5 ) and then
repeat steps 13 through 16.This section is applicable to the lab application or feature-licensed test application only.
Operating Mode ( F1
) to Cell Off
. 34.121 Preset Call Configurations
( F11 on
Call Parms 1 of 3 ) and select 5.2C,
5.7A, 5.13.1A, 5.13.1AA, and 5.13.2A:HSDPA:QPSK
, then select the desired sub-test. You may then
skip any steps marked with
[34.121 Call Config] in this procedure. Channel (UARFCN) Parms
( F12 on
Call Parms 1 of 3 ). Set
DL Channel ( F7 )
to the appropriate "low range" frequency
for your UE's operating band, as specified by
3GPP TS 34.108 5.1.1 (for example, for operating
band II set DL Channel
= 9663
).Cell Info
(
F2
on Call Control 2 of 6
).Cell Parameters
(
F2 ).
Set Default
DPCH Offset (DOFF)to
3 x 512 chips. Uplink Parameters ( F4 on
Call Control 2 of 6 ).
Uplink DPCH Bc/Bd Control to
Manual . Manual Uplink DPCH
Bc to
2 (for 34.121-1 v8.10.0 Table C.10.1.4
sub-test 1). Manual Uplink DPCH
Bd to
15 (for 34.121-1 v8.10.0 Table C.10.1.4
sub-test 1). Maximum Uplink Transmit
Power Level to
+21 dBm . Operating Mode to Active Cell (pressing
the CALL SETUP key quickly
brings you back to the top level
Call Control menu). Cell Power (
F7 on Call Parms
1 of 3 ) to -86
dBm/3.84 MHz . Channel Type (
F8 ) to 12.2k RMC
+ HSDPA . Generator Info ( F3 on
Call Control 2 of 6 ), select
Downlink Channel Levels (
F3 ), select Connected
DL Channel Levels ( F3
), then select HSDPA
Conn DL Channel Levels (
F4 ).
HSDPA Cell 1 Connected CPICH Level to -10 dB (this is
the default value). HSDPA Cell 1 Connected
P-CCPCH/SCH Level to
-12 dB (this is the default value). HSDPA Cell 1 Connected
PICH Level to
-15 dB (this is the default value). HSDPA Cell 1 Connected
DPCH Level to
-9 dB. HSDPA Cell 1 Connected
HS-PDSCHs Level (Sum) to
-3 dB (this is the default value). HSDPA Cell 1 Connected
HS-SCCH 1 Level to
-8 dB . HSDPA
Parameters ( HSPA
Parameters ( F10 ), F10 ).
HSDPA RB Test Mode Setup (
F8 ), then select
HSDPA RB Test Mode Settings (
F8 ).
MAC-(e)hs Parameters (
F10 ).
HSDPA Uplink Parameters
( F11 ).
Cell
Parameters ( F2 ).
Cell Info ( F2 ), then Cell Parameters ( F2 ).
Call Control 2 of 6 menu)
PS Domain Information to
Present (this is the default value in the
lab application). Cell Info , Reselection Parameters
( F3 ). RB Test Mode Setup ( F6 on
Call Control 3 of 6 ) and set
UE Loopback Type to
Type 1 (this is the default value). UL CL Power Ctrl Parameters
( F8 on
Call Parms 3 of 3 ) and set
UL CL Power Ctrl Algorithm to
Two (this is the default value). PS Domain Information parameter
must be set to Present
when the UE registers (attaches) with the test
set. Originate Call ( F3 on
Call Control 1 of 6 ). UE Target Power ( F7 on
Call Parms 3 of 3 ) to a high value, such
as 24 dBm. The test set
drives the UE to the specified level (or simply
continues to send all up bits if the UE does not
reach that level), while also appropriately ranging
the test set's measurement receiver.
UL CL Power Ctrl Parameters (
F8 on Call Parms
3 of 3 ) and set
UL CL Power Ctrl Mode to
All Up bits . Code Domain
.
Graph Control ( F2
) and set Table ( F3 ) to 2
(so that you can compare the NCDP and ECDP
results with 3GPP TS 34.121-1 Table 5.13.2A.4).
Marker ( F2 under Graph Control ( F2 )) to ensure that the RCDE
result for each code channel meets the specified
requirements in 34.121-1 Table 5.13.2A.5.| Code Channel | Location | Marker |
|---|---|---|
| DPCCH | Q Cch,256,0 | 0 |
| DPDCH | I Cch,64,16 | 64 |
| HS-DPCCH | Q Cch,256,64 | 64 |
Handovers ( F5 ))
to change the following settings:
| Setting | Sub-test 3 | Sub-test 4 |
|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 15 | 15 |
| TCR Manual Uplink DPCH Bd | 8 | 4 |
| TCR DeltaACK and DeltaNACK | 8 | 8 |
| TCR DeltaCQI | 7 | 7 |
| TCR Ack-Nack Repetition Factor | 1 |
1 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 1 |
1 |
Handovers
( F5 )) to change the following
settings:
| Setting | Sub-test 1 |
|---|---|
| TCR DPCH Bc/Bd Control | Manual |
| TCR Manual Uplink DPCH Bc | 2 |
| TCR Manual Uplink DPCH Bd | 15 |
| TCR DeltaACK and DeltaNACK | 8 |
| TCR DeltaCQI | 7 |
| TCR Ack-Nack Repetition Factor | 1 |
| TCR CQI Feedback Cycle (k) | 4 ms |
| TCR CQI Repetition Factor | 1 |
Handovers ( F5 ))
to change the following settings: | Setting | Sub-test 3 | Sub-test 4 |
|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 15 | 15 |
| TCR Manual Uplink DPCH Bd | 8 | 4 |
| TCR DeltaACK and DeltaNACK | 8 | 8 |
| TCR DeltaCQI | 7 | 7 |
| TCR Ack-Nack Repetition Factor | 1 |
1 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 1 |
1 |
Handovers ( F5 )) to
repeat the testing at mid- and high- range frequencies.This section is applicable to the lab application or feature-licensed test application only.
Operating Mode ( F1
) to Cell Off
. 34.121 Preset Call Configurations
( F11 on
Call Parms 1 of 3 ) and select 5.2B,
5.9B, 5.10B, and 5.13.2B:HSPA:QPSK , then
select the desired sub-test. You may then skip
any steps marked with [34.121
Call Config] in this procedure. Channel (UARFCN) Parms
( F12 on
Call Parms 1 of 3 ). Set
DL Channel ( F7 )
to the appropriate "low range" frequency
for your UE's operating band, as specified by
3GPP TS 34.108 5.1.1 (for example, for operating
band II set DL Channel
= 9663
). Uplink Parameters ( F4 on
Call Control 2 of 6 ).
Uplink DPCH Bc/Bd Control to
Manual . Manual Uplink DPCH
Bc to
11 (for 34.121-1 v8.10.0 Table C.11.1.3
sub-test 1). Manual Uplink DPCH
Bd to
15 (for 34.121-1 v8.10.0 Table C.11.1.3
sub-test 1). Maximum Uplink Transmit
Power Level to
21 dBm . Operating Mode to Active Cell (pressing
the CALL SETUP key quickly
brings you back to the top level
Call Control menu). Cell Power (
F7 on Call Parms
1 of 3 ) to -86
dBm/3.84 MHz . Channel Type (
F8 ) to 12.2k RMC
+ HSPA . Generator Info ( F3 on
Call Control 2 of 6 ), select
Downlink Channel Levels (
F3 ), select Connected
DL Channel Levels ( F3
), then select HSPA Conn
DL Channel Levels ( F4
).
HSPA Cell 1 Connected CPICH Level to -10 dB (this is
the default value). HSPA Cell 1 Connected
P-CCPCH/SCH Level to
-12 dB (this is the default value). HSPA Cell 1 Connected
PICH Level to
-15 dB (this is the default value). HSPA Cell 1 Connected
(F-)DPCH Level to
-10 dB (this is the default value). HSPA Cell 1 Connected
E-AGCH Level to
-20 dB (this is the default value). HSPA Cell 1 Connected
E-HICH Level to
-20 dB (this is the default value). HSPA Cell 1 Connected
E-RGCH Level to
Off (this is the default value). HSPA Cell 1 Connected
HS-PDSCHs Level (Sum) to
-3 dB (this is the default value). HSPA Cell 1 Connected
HS-SCCH 1 Level to
-8 dB . HSUPA Parameters ( HSPA Parameters ( F10 ), F9
).
HSUPA RB Test Mode Setup (
F8 ).
Common HSUPA Parameters
( F9 ).
E-DPCCH/DPCCH Power Offset (DeltaE-DPCCH)
to 6 (for
34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Note, 34.121-1 Table C.11.1.3 provides Beta ec (209/225 for sub-test
1). To determine what value of DeltaE-DPCCH
corresponds to this, use 3GPP TS 25.213 Table
1B and the value of Beta
c from 34.121-1 Table C.11.1.3 (11/15
for sub-test 1). For sub-test 1, A
ec = Beta ec
/Beta c = (209/225)/(11/15)
= 19/15; therefore DeltaE-DPCCH = 6. Reference E-TFCI Power
Offsets to
Definition 34.121-01 (for 34.121-1
v8.10.0 Table C.11.1.3 sub-test 1). Serving Grant ( F10 ).
RB Setup AG to
26: (119/15)^2 (for 34.121-1 v8.10.0
Table C.11.1.3 sub-test 1). Note, 34.121-1
Table C.11.1.3 AG Index corresponds to 3GPP
TS 25.212 s4.10.1A.1 Table 16B, which maps
the Absolute Grants sent on the E-AGCH. To
send the equivalent Absolute Grant in the
RB Setup message, you must use the AG Index
in 3GPP TS 25.321 s9.2.5.2.1.1 Table 9.2.5.2.1.1. HSDPA Parameters ( HSPA Parameters ( F10 ), F10
).
Cell
Parameters ( F2 ).
Cell Info ( F2 ), then Cell Parameters ( F2 ).
Call Control 2 of 6 menu)
PS Domain Information to
Present (this is the default value in the
lab application). Cell Info , Reselection Parameters
( F3 ). RB Test Mode Setup ( F6 on
Call Control 3 of 6 ) and set
UE Loopback Type to
Type 1 (this is the default value). UL CL Power Ctrl Parameters
( F8 on
Call Parms 3 of 3 ) and set
UL CL Power Ctrl Algorithm to
Two (this is the default value). PS Domain Information parameter
must be set to Present
when the UE registers (attaches) with the test
set. Originate Call ( F3 on
Call Control 1 of 6 ).
UL CL Power Ctrl Parameters (
F8 on Call Parms
3 of 3 ) and set
UL CL Power Ctrl Mode to
Active bits (this is the default value). UE Target Power ( F7 on
Call Parms 3 of 3 ) to
1 dBm (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test
1). This value is determined as follows:
UE Target Power only
sets the DPCCH+DPDCH power level of the UE. In
order to achieve a total output power of +15 dBm,
you must set UE Target
Power to at most 15 dBm - Power
change due to HS-DPCCH, E-DPCCH and E-DPDCH
.
UE Target Power to 1 dBm for sub-test 1. UE Target Power
values for sub-tests 2-4 are as follows:
sub-test 2: 10 dBm, sub-test 3: 2 dBm, sub-test
4: 13 dBm. Additional Screens ( F1 from
Call Control 2 of 6 ), select
HSPA Information ( F2
) and confirm that the
Last Received E-TFCI is equal to the target
E-TFCI (it should be 75 for 34.121-1 v8.10.0 Table
C.11.1.3 sub-test 1, 67 for sub-test 2, 92 for
sub-test 3, and 71 for sub-test 4). E-TFCI Recording Information
( F3 ). Code Domain
.
Graph Control ( F2
) and set Table ( F3 ) to 2
(so that you can compare the NCDP and ECDP
results with 3GPP TS 34.121-1 table 5.13.2B.8).Use the
Marker ( F2 under Graph Control ( F2 )) to ensure that the RCDE
result for each code channel meets the specified
requirements in 34.121-1 table 5.13.2B.9.
The code channels are located as follows:
| Code Channel | Location | Marker |
|---|---|---|
| DPCCH | Q Cch,256,0 | 0 |
| DPDCH | I Cch,64,16 | 64 |
| HS-DPCCH | Q Cch,256,64 | 64 |
| E-DPCCH | I Cch,256,1 | 1 |
| E-DPDCH1 | I Cch,4,2 | 128 |
| E-DPDCH2 | Q Cch,4,2 | 128 |
Handovers ( F5 ))
to change the following settings:
| Setting | Sub-test 2 | Sub-test 3 | Sub-test 4 |
|---|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 6 | 15 | 2 |
| TCR Manual Uplink DPCH Bd | 15 | 9 | 15 |
| TCR DeltaACK, DeltaNACK, DeltaCQI | 8 | 8 | 8 |
| TCR Ack-Nack Repetition Factor | 3 | 3 | 3 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 2 | 2 | 2 |
| TCR E-DPCCH/DPCCH Power Offset | 8 | 8 | 5 |
| TCR Reference E-TFCI Power Offsets | 34121-01 | 34121-02 | 34121-01 |
| TCR Absolute Grant | 18: (47/15)^2 | 21: (67/15)^2 | 23: (84/15)^2 |
Handovers
( F5 )) to change the following
settings:
| Setting | Sub-test 1 |
|---|---|
| TCR DPCH Bc/Bd Control | Manual |
| TCR Manual Uplink DPCH Bc | 11 |
| TCR Manual Uplink DPCH Bd | 15 |
| TCR DeltaACK, DeltaNACK, DeltaCQI | 8 |
| TCR Ack-Nack Repetition Factor | 3 |
| TCR CQI Feedback Cycle (k) | 4 ms |
| TCR CQI Repetition Factor | 2 |
| TCR E-DPCCH/DPCCH Power Offset | 6 |
| TCR Reference E-TFCI Power Offsets | 34121-01 |
| TCR Absolute Grant | 26: (119/15)^2 |
UE Target Power ( F7
on Call Parms 3 of
3 ) to -32
dBm (for 34.121-1 v8.10.0 Table C.11.1.3
sub-test 1). In order to achieve a total output
power of -18 dBm, you must set
UE Target Power to -18 dBm - Power
change due to HS-DPCCH, E-DPCCH and E-DPDCH
.
UE Target Power to -32 dBm for sub-test
1. UE Target Power
values for sub-tests 2-4 are as follows:
sub-test 2: -23 dBm, sub-test 3: -31 dBm, sub-test
4: -20 dBm.
Handovers ( F5 ))
to change the following settings:
| Setting | Sub-test 2 | Sub-test 3 | Sub-test 4 |
|---|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 6 | 15 | 2 |
| TCR Manual Uplink DPCH Bd | 15 | 9 | 15 |
| TCR DeltaACK, DeltaNACK, DeltaCQI | 8 | 8 | 8 |
| TCR Ack-Nack Repetition Factor | 3 | 3 | 3 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 2 | 2 | 2 |
| TCR E-DPCCH/DPCCH Power Offset | 8 | 8 | 5 |
| TCR Reference E-TFCI Power Offsets | 34121-01 | 34121-02 | 34121-01 |
| TCR Absolute Grant | 18: (47/15)^2 | 21: (67/15)^2 | 23: (84/15)^2 |
Handovers ( F5 )) to repeat the testing at
mid and high range frequencies.This section is applicable to the lab application or feature-licensed test application only.
Relative Code Domain Error for HS-DPCCH and E-DCH with 16QAM from 3GPP TS 34.121-1 s5.13.2C measures RCDE on any release 7 or later UE that supports E-DCH category 7, 16QAM with HSUPA.
The test is performed with the UE transmitting at maximum power and then repeated with the UE transmitting at -18 dBm.
Operating
Mode ( F1 ) to Cell Off . 34.121 Preset Call
Configurations ( F11
on Call Parms 1 of
3 ) and select 5.13.1AAA,
5.13.2C:HSPA+:UL 16QAM . You may then skip
any steps marked with [34.121
Call Config] in this procedure.Channel (UARFCN)
Parms ( F12 on Call Parms 1 of 3
). Set DL Channel
( F7 ) to the appropriate
"low range" frequency for your UE's
operating band, as specified by 3GPP TS 34.108
s5.1.1 (for example, for operating band II set
DL Channel = 9663 ). Uplink Parameters
( F4 on Call
Control 2 of 6 ).
Uplink
DPCH Bc/Bd Control to
Manual . Manual Uplink
DPCH Bc to 15
(for 34.121-1 v8.10.0 table C.11.1.4
sub-test 1). Manual Uplink
DPCH Bd can remain at its default value.
34.121-1 v8.10.0 table C.11.1.4 sub-test 1
requires Beta d
set to zero. This is configured by selecting
a DL channel type with no DPDCH. The value
set here for Beta d
is not used because no DL DPDCH is generated.
Maximum Uplink
Transmit Power Level to +21
dBm . Operating Mode
to Active Cell
(pressing the CALL SETUP
key quickly brings you back to the top level Call Control menu).Cell Power ( F7 on Call
Parms 1 of 3 ) to -86
dBm/3.84 MHz . Channel Type ( F8
) to HSPA . Generator Info
( F3 on Call
Control 2 of 6 ), select Connected
DL Channel Levels ( F4
), and then select HSPA
Conn DL Channel Levels ( F5
).
HSPA
Cell 1 Connected CPICH Level to -10
dB (this is the default value). HSPA Cell 1 Connected
P-CCPCH/SCH Level to -12
dB (this is the default value). HSPA Cell 1 Connected
PICH Level to -15
dB (this is the default value). HSPA Cell 1 Connected
DPCH Level to -10
dB (this is the default value). HSPA Cell 1 Connected
E-AGCH Level to -20
dB (this is the default value). HSPA Cell 1 Connected
E-HICH Level to -20
dB (this is the default value). HSPA Cell 1 Connected
E-RGCH Level to Off
(this is the default value). HSPA Cell 1 Connected
HS-PDSCHs Level (Sum) to -3
dB (this is the default value). HSPA Cell 1 Connected
HS-SCCH 1 Level to -8
dB . Generator Info
( F3 on Call
Control 2 of 6 ), select Downlink
Channel Configs ( F4
), and then then select HS-SCCH Configs ( F3
).
HSUPA Parameters
( HSPA Parameters
( F10 ), F9
).
HSUPA
RB Test Mode Setup ( F8
).
Common HSUPA Parameters
( F9 ).
E-DCH
TTI to 2 ms.E-DCH 16QAM
State to On
.E-DPCCH/DPCCH
Power Offset (DeltaE-DPCCH) to 8 (for 34.121-1
v8.10.0 table C.11.1.4 sub-test 1). Note,
34.121-1 table C.11.1.4 provides Beta ec (30/15 for sub-test
1). To determine what value of DeltaE-DPCCH
corresponds to this, use 3GPP TS 25.213 table
1B and the value of Beta
c from 34.121-1 table C.11.1.4 (15/15
for sub-test 1). For sub-test 1, A ec
= Beta ec /Beta c = (30/15)/(15/15)
= 30/15; therefore DeltaE-DPCCH = 8. E-TFCI Table
Index (2 ms TTI with 16QAM) to 2 (this is the
default value).Reference
E-TFCI Power Offset Control to Predefined (this
is the default value). Reference
E-TFCI Power Offsets to Definition
34.121-04 (for 34.121-1 v8.10.0 table
C.11.1.4 sub-test 1). 34.121-1 v8.10.0 table
5.2E.2 is used for this configuration; however,
this table is identical to 34.121-1 table
5.13.2C.4.E-TFCI Boost
Information State to On
.E-TFCI Boost
Value to 105
.DeltaT2TP
to 2 (this
is the default value).BetaEd Gain
E-AGCH Table Selection to 1
(this is the default value).E-DPDCH Power
Calculation Formula to Extrapolation
(this is the default value).Serving Grant
( F10 ).
AG
Mode to Single
Shot (this is the default value).Single Shot
AG to 14:
(75/15)^2 (for 34.121-1 v8.10.0 table
C.11.1.4 sub-test 1).RB Setup
AG to 17:
(75/15)^2 (for 34.121-1 v8.10.0 table
C.11.1.4 sub-test 1). Note, 34.121-1 table
C.11.1.4 AG Index corresponds to 3GPP TS 25.212
s4.10.1A.1 table 16B.1, which maps the Absolute
Grants sent on the E-AGCH. To send the equivalent
Absolute Grant in the RB Setup message, you
must use the AG Index in 3GPP TS 25.321 s9.2.5.2.1.1
table 9.2.5.2.1.2.HSDPA Parameters
( HSPA Parameters ( F10 ), F10 ).
Cell
Parameters ( F2 ).
Lab
Application: Select Cell
Info ( F2 ) , then Cell Parameters ( F2 ) from the Call
Control 2 of 6 menu.
PS
Domain Information to Present
(this is the default value in the lab application).
Cell Info , Reselection Parameters
( F3 ).RB Test Mode Setup
( F6 on Call
Control 3 of 6 ) and set UE
Loopback Type to Type
1 (this is the default value).UL CL Power Ctrl Parameters
( F8 on Call
Parms 3 of 3 ) and set UL
CL Power Ctrl Algorithm to Two
(this is the default value).Originate Call
( F3 on Call
Control 1 of 6 ).UL CL Power Ctrl Parameters
( F8 on Call
Parms 3 of 3 ) and set UL
CL Power Ctrl Mode to Active
bits (this is the default value).UL
CL Power Ctrl Parameters ( F8
on Call Parms 3 of
3 ) and set UL
CL Power Ctrl Mode to Active
bits (this is the default value). UE Target Power
( F7 on Call
Parms 3 of 3 ) to 3
dBm (for 34.121-1 v8.10.0 table C.11.1.4
sub-test 1, power class 3 UE). This value is determined
as follows: Maximum power for a power class 3
UE is +24 dBm, but UE Target Power only sets the
DPCCH+DPDCH power level of the UE. In order to
achieve a total output power of +16.5 dBm (24
dBm - 7.5 dB as required by 34.121-1 s5.2B.4.2),
you must set UE Target Power to at most 16.5 dBm
- Power change due to HS-DPCCH, E-DPCCH and E-DPDCH.
Power
Change Due to HS-DPCCH, E-DPCCH and E-DPDCH =
10log 10 (Beta c ^2 + Beta
d ^2 + Beta hs
^2 + Beta ec ^2 +
Beta ed1 ^2 + Beta ed2 ^2 + Beta
ed3 ^2 + Beta ed4
^2) - 10log 10 (Beta d ^2 + Beta
c ^2) = 13.4 dB for sub-test 1, so you must
set UE Target Power
to 3 dBm for
sub-test 1.
Channel
Power . UL CL Power Ctrl
Parameters ( F8 on
Call Parms 3 of 3
). Set UL CL Power
Ctrl Mode to Alternating
bits . Additional Screens
( F1 from Call
Control 2 of 6 ), select HSPA
Information ( F2
) and observe the Last
Received E-TFCI (it should be 105 for 34.121-1
v8.10.0 table C.11.1.4 sub-test 1). E-TFCI Recording
Informatio n ( F3
). HSPA Parameters
( F10 ), HSUPA
Parameters ( F9 ),
E-TFCI Recording
( F11 ), E-TFCI
Recording Parameters ( F7
).
E-TFCI
Recording Count to 15
(this is the default value). E-TFCI Recording
Behavior to All
. Send Step Up
TPC Bit Pattern ( F10
) and then Start
Recording E-TFCI Values ( F8
). Send Step Down
TPC Bit Pattern ( F11
) and then Start
Recording E-TFCI Values ( F8
). Code Domain
.
Code
Domain Setup ( F1
).
Graph
Control ( F2 ) and
setting Table
( F3 ) = 2 so that you can
compare NCDP and ECDP with 3GPP TS 34.121-1 table
5.13.2C.7.Graph Control (
F2 ) ) to ensure that RCDE
for each code channel meets the specified requirements
in 34.121-1 tables 5.13.2C.8 and 5.13.2C.9.UL CL Power Ctrl Parameters
( F8 on Call
Parms 3 of 3 ) and set UL
CL Power Ctrl Mode to Active
bits (this is the default value). UE Target Power
( F7 on Call
Parms 3 of 3 ) to -31
dBm . This value is determined as follows:
34.121-1 s5.13.1AAA requires a UE output power of
-18 dBm, but UE Target Power only sets the DPCCH+DPDCH
power level of the UE. In order to achieve a total
output power of -18 dBm, you must set UE
Target Power to at most -18 dBm - Power change
due to HS-DPCCH, E-DPCCH and E DPDCH.Power Change
Due to HS-DPCCH, E-DPCCH and E-DPDCH = 10log
10 (Beta
c ^2 + Beta d ^2
+ Beta hs ^2 + Beta ec ^2 + Beta
ed1 ^2 + Beta ed2
^2 + Beta ed3 ^2 + Beta ed4 ^2) - 10log
10 (Beta d ^2 +
Beta c ^2) = 13.4 dB
for sub-test 1, so you must set UE
Target Power to -31
dBm . UL CL Power Ctrl Parameters
( F8 on Call
Parms 3 of 3 ) and set UL
CL Power Ctrl Mode to Alternating
bits .Graph Control (
F2 ) and setting Table
( F3 ) = 2
so that you can compare NCDP and ECDP with 3GPP
TS 34.121 table 5.13.2C.7.Graph Control (
F2 ) ) to ensure that RCDE
for each code channel meets the specified requirements
in 34.121-1 tables 5.13.2C.8 and 5.13.2C.9.Physical
Channel Reconfig ( F5 on
Call Control 1 of 6
, F1 ) to perform a hard handover
to the next channel. Set the Handover
Downlink Channel (UARFCN) and Handover
Uplink Channel (UARFCN) parameters to the appropriate
"mid range" or "high range" frequencies
for your UE's operating band, as specified by 3GPP
TS 34.108 s5.1.1. Execute
Handover ( F5 ) and then
repeat steps 13 through 19.