Last updated: January 15, 2009
 Operating Mode 
(
F1
) to
 Cell Off
.
 DL Channel 
(
F10
) and
 Uplink Channel 
(
F11
) to the appropriate "mid range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band I,
 DL Channel 
=
 10700 
and
 Uplink Channel 
=
 9750
).
 Operating Mode 
to
 Active Cell
.
 RB Test Mode 
connection between the UE and test set (see 
How Do I Set Up a Call and Make a Connection?
).
 Connected DL Channel Levels 
are set to their default values, as required by 3GPP TS 34.121 Table E.3.1 (select
 Generator Info
, 
F3 
on
 Call Control 2 of 5
).
 Cell Power 
(
F7
) to
 -93 dBm
.
Inner Loop Power
. 
 Inner Loop Power Setup 
(
F1
).
 Pass
.
 Axis Control 
(
F2
).
 Marker 
(
F3
) to turn on the marker on the graphical display and move the highlighted bar in the numerical results display area.
 Inner Loop Power Setup 
(
F1
).
 Pass
.
 Test Segment E
. For test segments E through H, ensure that
 Maximum Power Threshold for Test Control 
is set to
 Auto
,
 Maximum Output Power Test Tolerance 
is set to
 0.70 dB
,
 Minimum Power Threshold for Test Control 
is set to
 Manual
, and
 Minimum Power Threshold for Test Manual 
is set to
 -49 dBm 
(these are the default values), as required by 3GPP TS 34.121