Last updated: January 15, 2009
 RB Test Mode 
connection between the UE and test set (see 
How Do I Set Up a Call and Make a Connection?
).
IQ Tuning
. 
 Trigger Arm 
is set to
 Single
, you must press the
 START SINGLE 
key to begin the measurement.
 IQ Tuning Setup 
(
F1
) and set the measurement parameters as needed. Select
 Close Menu 
(
F6
).
 Cell Power 
(
F7
) as needed.
 Axis Control 
(
F2
). Set the axis control parameters as needed. Select
 Return 
(
F6
).
 Marker 
(
F3
) to turn on the marker on the graphical display. The EVM for the selected chip is displayed.A typical result is shown below.