Last updated: January 16, 2009
 HS-DPCCH
.
 HS-DPCCH
.
 HS-DPCCH Trigger Subslot Alignment 
setting, you must first decrease the
 HS-DPCCH Measurement Interval 
setting appropriately.
 Trigger Source 
is set to
 Immediate 
or
 External
.
Timing Error 
results are not available when 
Trigger Source 
is set to
 Immediate
.
 AckNack
, a valid result is returned for Beta
hsacknak
, NaN is returned for Beta
hscqi
. Likewise, when 
HS-DPCCH Trigger Slot Alignment
 is set to
 CQI1
 or
 CQI2
, a valid result is returned for Beta
hscqi
, NaN is returned for Beta
hsacknak
.
 
If 
Over Range
 (5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set. 
 
If 
 (6) is returned, the measured signal is below the expected input level. 
Under Range
 
If 
Cannot Correlate
 (17) is returned, the test set cannot demodulate the signal from the mobile station (UE). Make sure the uplink scrambling code from the mobile station matches the UL Scrambling setting on the test set (see 
CALL:UPLink
).
 
If 
Uncalibrated Due to Temperature
 (19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. See 
Calibrating the Test Set
.
See Integrity Indicator .