Last updated: January 16, 2009
The IQ tuning measurement includes all of the measurements available in the Waveform Quality measurement (see Waveform Quality Measurement Results ), along with the following measurement results:
Chip EVM is the calculated EVM at each chip in the measured timeslot. Chip EVM is measured as a 2560 element array of 32-bit floating point numbers. The first element in the array corresponds to the measured EVM for the first chip in the measured time slot, the second element to the EVM for the second chip in the measured time slot, and so on. These results are available graphically on the front panel display and numerically via the GPIB commands.
The IQ constellation is the measured IQ signal with origin offset included. IQ constellation is measured as a 2560 element array of ordered pairs. Each ordered pair consists of two 32-bit floating point numbers corresponding to one point in the IQ constellation. The first member in the ordered pair is the I coordinate, the second is the Q coordinate. The array is scaled so all points fall within a unit circle. The first ordered pair in the IQ constellation array corresponds to the first chip in the measured time slot, the second ordered pair in the array corresponds to the second chip in the measured time slot, and so on. The IQ constellation result is only available graphically on the front panel display. It is not be accessible via the GPIB commands.
When on a non-HSDPA connection, you must set
Trigger Source
to any value other than
HS-DPCCH
. When operating in this mode, the measurement is made during one timeslot (666.7 us). You can choose in which timeslot of the W-CDMA frame the measurement is performed using the
Timeslot
setting.
This section is only applicable to the lab application or feature-licensed test application .
To measure IQ tuning on an HSDPA connection, you must set
Trigger Source
to
HS-DPCCH
. When
Trigger Source
is set to HS-DPCCH, you can specify the measurement interval and its placement within any of the 6 HSDPA subframes.
AckNack
= the first slot of the subframe,
CQI1
= the second slot of the subframe and
CQI2
= the third slot of the subframe).
HS-DPCCH Trigger Subslot Alignment
and
HS-DPCCH Measurement Interval
cannot exceed 1.0 slot.
HS-DPCCH Trigger Subslot Alignment
and
HS-DPCCH Measurement Interval
cannot exceed 1.0 slot. If you wish to place the measurement interval after the slot boundary using the
HS-DPCCH Trigger Subslot Alignment
setting, you must first decrease the
HS-DPCCH Measurement Interval
setting appropriately.
HS-DPCCH Measurement Interval
to
0.5 slot
(333.3 us or 1280 chips) and set
Transient Period
to
Exclude
, the measurement is performed over 283.3 us (or 1088 chips).
When
Trigger Source
is set to any value other than
HS-DPCCH
, you can specify which timeslot of the W-CDMA frame (0 to 14) is evaluated by the IQ tuning measurement. See
Measurement Interval in Non-HSDPA Mode
.
Triggering choices are immediate, protocol, external, auto and HS-DPCCH ( lab application or feature-licensed test application only ). See Trigger Source Description for more information.
Auto triggering is the default choice. In most cases, auto triggering provides the optimum measurement triggering condition for the IQ tuning measurement. For example, if the UE is synchronized to the test set, auto triggering causes protocol triggering to be used. Auto triggering causes immediate triggering is used if the UE is not synchronized. When immediate triggering is used, the measurement result returned for timing error is always
NAN
(Not a Number) because it is not possible to evaluate a timing error in this measurement situation.
This section is only applicable to the lab application or feature-licensed test application .
These settings are only applicable when
Trigger Source
=
HS-DPCCH
.
See Measurement Interval in HSDPA Mode for more information about using these parameters to specify the duration and placement of the measurement interval.
When
Transient Period
is set to
Include
, the measurement is performed over the interval specified by the
HS-DPCCH Measurement Interval
setting.
When
Transient Period
is set to
Exclude
, the 25 us at the start of the measurement interval and the 25 us at the end of the measurement interval are excluded from the measurement. Thus, the measurement is performed over an interval equal to
HS-DPCCH Measurement Interval
minus 50 us. See
Measurement Interval in HSDPA Mode
.
Selects which 2 ms subframe (0 to 5) contains the measurement interval.
Selects which slot in the 2 ms subframe contains the measurement interval (
AckNack
= the first slot in the subframe,
CQI1
= the second slot in the subframe and
CQI2
= the third slot in the subframe).
See Measurement Interval in HSDPA Mode .
Note, the sum of
HS-DPCCH Trigger Subslot Alignment
and
HS-DPCCH Measurement Interval
cannot exceed 1.0 slot.
Selects where to place the measurement interval within the slot, in 0.1 slot (66.7 us) increments. This is useful because depending upon the Current DPCH Offset , the uplink DPCH and HS-DPCCH can be offset in time by increments of 0.1 slot (see HS-DPCCH/DPCCH Alignment vs. DPCH Frame Offset ).
Note, the sum of
HS-DPCCH Trigger Subslot Alignment
and
HS-DPCCH Measurement Interval
cannot exceed 1.0 slot.
Chip EVM and the IQ constellation are graphed together on the same screen. See figure
IQ Tuning Graph Display
for an example display. You can use the
Axis Control
(
F2
) and the
Marker
(
F3
) settings to control the Chip EVM trace graph and the IQ constellation diagram. The IQ constellation diagram is always redrawn to reflect the latest Chip EVM settings. For example, if the chip EVM for chips 512 through 1023 are plotted, then the IQ constellation is shown for just chips 512 through 1023. The I and Q values for the IQ constellation all range between -1.0 and +1.0.
The IQ tuning measurement also returns all of the measurement results of the Waveform Quality measurement. Waveform Quality Measurement Results
This measurement should be calibrated using the Calibrate Measurements function ( CALibration:MEASurements? ) when the temperature has changed by ± 10° C or more since the last calibration. If this situation exists, the integrity indicator value becomes 19 and a message is displayed indicating "Uncalibrated Due to Temperature".