Last updated: January 15, 2009
Before performing any of these procedures, ensure that you have specified the proper Amplitude Offset for your test setup, and that the test set has been properly calibrated (see Calibrating the Test Set ).
Operating Mode
(
F1
) to
Cell Off
.
DL Channel
(
F10
) and
Uplink Channel
(
F11
) to the appropriate "low range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band I,
DL Channel
=
10563
and
Uplink Channel
=
9613
).
Downlink Channel Levels
are set to their default values, as required by 3GPP TS 34.121 Table E.2.2 (select
Generator Info
,
F3
on
Call Control 2 of 5
).
Operating Mode
to
Active Cell
.
Uplink Parameters
(
F4
from the
Call Control 2 of 5
menu).
PRACH Preambles
to
4
.
PRACH Ramping Cycles (MMAX)
to
1
(see
Recommended PRACH Preambles and PRACH Ramping Cycles (MMAX) settings
).
Available Subchannels (Bit Mask)
to only allow one available subchannel (for example, the default value of 000000000001).
Set
Maximum Uplink Transmit Power Level
to the specified maximum output power of your UE (for example, 21 dBm for power class 4).
Note: Qqualmin and Qrxlevmin are fixed to -24 dB and -115 dBm in the test set, as required by 3GPP TS 34.121 Table 5.4.1.1a.
Close Menu
(
F6
).
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Call Control 2 of 5
menu)
Primary CPICH TX Power
is set to its default value of
19 dBm
.
Uplink Interference
to
-75 dBm
.
Constant Val
ue is set to its default value of
-10 dB
.
Close Menu
(
F6
).
Cell Power
(
F7
on
Call Parms 1 of 3
) to
-25 dBm
.
Call Limit State
(
F10
on
Call Parms 2 of 3
) is set to its default value of
Off
(see
Importance of Setting Call Limit State to Off before Initiating a PRACH Measurement
).
PRACH Transmit On/Off Power
.
PRACH TX On/Off Pwr Setup
(
F1
).
Open Loop Power Error
test result is
Pass
.
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Call Control 2 of 5
menu)
BCCH Update Page
to
Auto
so the test set will notify the UE when you change the next two cell parameters.
Primary CPICH TX Power
to
28 dBm
or
19 dBm
.
Uplink Interference
to
-101 dBm
or
-110 dBm
.
Constant Value
is still set to
-10 dB
.
Close Menu
(
F6
).
Cell Power
(
F7
) to
-65.7 dBm
or
-106.7 dBm
.
Measurement/Instrument
screen.
Idle
state (see
Test set may lock up if operations are attempted before the UE completes its PRACH sequence
), then press the
START SINGLE
key to begin the measurement.
Open Loop Power Error
test result is
Pass
.See Measuring 3GPP TS 34.121 5.5.2 Transmit ON/OFF Time Mask .
Operating Mode
(
F1
) to
Cell Off
.
DL Channel
(
F10
) and
Uplink Channel
(
F11
) to the appropriate "low range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band I,
DL Channel
=
10563
and
Uplink Channel
=
9613
).
Downlink Channel Levels
are set to their default values as required by 3GPP TS 34.121 Table E.2.2. (select
Generator Info
,
F3
on
Call Control 2 of 5
).
Operating Mode
to
Active Cell
.
Uplink Parameters
(
F4
from the
Call Control 2 of 5
menu).
PRACH Preambles
to
4
.
PRACH Ramping Cycles (MMAX)
to
1
(see
Recommended PRACH Preambles and PRACH Ramping Cycles (MMAX) settings
).
Available Subchannels (Bit Mask)
to only allow one available subchannel (for example, the default value of 000000000001).
Set
Maximum Uplink Transmit Power Level
to the specified maximum output power of your UE (for example, 21 dBm for power class 4).
Note: Qqualmin and Qrxlevmin are fixed to -24 dB and -115 dBm in the test set, as required by 3GPP TS 34.121 Table 5.4.1.1a.
Close Menu
(
F6
).
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Call Control 2 of 5
menu)
Primary CPICH TX Power
is set to its default value of
19 dBm
.
Uplink Interference
to the proper value for your UE's power class as required by 3GPP TS 34.121 Table 5.5.2.3 (for example,
-98 dBm
for power class 4).
Constant Val
ue is set to its default value of
-10 dB
.
Close Menu
(
F6
).
Cell Power
(
F7
) to
-106.7 dBm
.
Call Limit State
(
F10
on
Call Parms 2 of 3
) is set to its default value of
Off
(see
Importance of Setting Call Limit State to Off before Initiating a PRACH Measurement
).
PRACH Transmit On/Off Power
.
PRACH TX On/Off Pwr Setup
(
F1
).
Off Power Limit
is set to its default value of
-55 dBm
.
Open Loop Power Error Upper Limit
to
1.7 or 2.7 dB
, depending upon your UE's power class, as required by 3GPP TS 34.121 Table 5.2.2.
Open Loop Power Error Lower Limit
is set to its default value of
-9 dB
.
Close Menu
(
F6
).
Pre Burst Off Power
,
Open Loop Power Error
and
Post Burst Off Power
test results are
Pass
.
PRACH Transmit On/Off Power Measurement Description