Last updated: January 16, 2009
 PRACH Preambles 
and
 PRACH Ramping Cycles (MMAX) 
settings
 
The measurement requires a minimum of 3 PRACH preambles, but it is recommended that you set 
PRACH Preambles
to
 4 
to ensure that the test set is able to capture two PRACH bursts for analysis. It is also recommended that you set
 PRACH Preambles 
to no greater than 4 and set 
PRACH Ramping Cycles (MMAX)
 to
 1 
to allow the UE's PRACH sequence to end as soon as possible. This helps avoid the following issue: 
Test set may lock up if operations are attempted before the UE completes its PRACH sequence
.
 Call Limit State 
to
 Off 
before Initiating a PRACH Measurement
 
It is recommended that you set 
Call Limit State
 to
 Off 
before initiating this measurement. Then, when the measurement completes, if the UE is still sending PRACH preambles to the test set, the test set will acknowledge the UE. Note, when the test set acknowledges the UE, the call is not completed because the UE is attempting to establish a test set-originated call, whereas the test set acknowledges the UE expecting a UE-originated call. Acknowledging the UE helps prevent the UE from placing the test set into its cell barred list (see 
Test Set in Cell Barred List
). When the test set acknowledges the UE, you will see the call status move from
 Paging 
to 
Idle
, to
 Setup
, to
 Releasing 
and then back to
 Idle
. Do not attempt to stop or re-initiate the measurement, or to start any new measurements until the test set has reached
 Idle 
state (see 
Test set may lock up if operations are attempted before the UE completes its PRACH sequence
).
Setting call limit mode to off before initiating the measurement also avoids another issue: When the measurement completes, if you try to send signalling to the UE while it is still sending PRACH preambles to the test set, the UE will ignore the incoming messages and the signalling will fail. If call limit mode is set to off, the test set will acknowledge the UE and cause it to stop sending PRACH preambles, and then send the signalling you have requested to the UE.
When the measurement completes, you must wait until the UE has finished its PRACH sequence before turning off or re-initiating the measurement, or before starting any new measurements. Otherwise, the test set may lock up. If you are controlling the test set via remote program, you must include a wait period after the measurement completes (see Programming a PRACH Transmit On/Off Power Measurement ).
 
If you set
 Call Limit Mode 
to
 Off 
before initiating the measurement, you will know that the UE's PRACH sequence is complete when you see the call status move from
 Paging 
to 
Idle
, to
 Setup
, to
 Releasing 
and then back to
 Idle 
(see 
Importance of Setting Call Limit State to Off before Initiating a PRACH Measurement
). Do not attempt any of the above listed operations until the test set has reached
 Idle 
state.
 
To allow the UE to complete its PRACH sequence as quickly as possible, it is recommended that you set
 PRACH Preambles 
to
 4 
and
 PRACH Ramping Cycles (MMAX) 
to
 1 
(see 
Recommended PRACH Preambles and PRACH Ramping Cycles (MMAX) settings
).
 Primary CPICH TX Power
,
 Uplink Interference
, or
 Constant Value
, you must force the UE to re-read the BCCH before initiating the measurement (so that it will use the same values for these settings as the test set when calculating the power of its initial PRACH preamble). If your UE supports the 
Broadcast Channel (BCCH) Update Procedure (SIB Contents)
, set 
BCCH Update Page
 to
 Auto
 to force the UE to re-read the BCCH. If your UE does not support the BCCH Update procedure, see 
BCCH Update Page
 for suggestions on forcing the UE to re-read the BCCH.
 
If 
Over Range
 (5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set. 
 
If 
Under Range
 (6) is returned, the measured signal is below the expected input level. 
 
If 
Uncalibrated Due to Temperature
 (19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. 
Calibrating the Test Set
See Integrity Indicator .