Last updated: February 12, 2011
RB Test Mode
connection between the UE and test set (see
How Do I Set Up a Call and Make a Connection?
).
Spectrum Emission Mask
.
SEM Setup
(
F1
) and set the measurement parameters as needed. Select
Close Menu
(
F6
).
Trigger Arm
is set to
Single
, you must press the
START SINGLE
key to begin the measurement.
Change View
(
F2
) key to display the measurement results in either graphical or numeric format.A typical result is shown below.
This section is applicable to the lab application or feature-licensed test application only.
Operating Mode
(
F1
) to
Cell Off
.
34.121 Preset Call Configurations
(
F11
on
Call Parms 1 of 3
) and select
5.2B, 5.9B, 5.10B, and 5.13.2B:HSPA:QPSK
, then select the desired sub-test. You may then skip any steps marked with
[34.121 Call Config]
in this procedure.
Channel (UARFCN) Parms
(
F12
on
Call Parms 1 of 3
). Set
DL Channel
(
F7
) to the appropriate "low range" frequency for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band II set
DL Channel
=
9663
).
Uplink Parameters
(
F4
on
Call Control 2 of 6
).
Uplink DPCH Bc/Bd Control
to
Manual
.
Manual Uplink DPCH Bc
to
11
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Manual Uplink DPCH Bd
to
15
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Maximum Uplink Transmit Power Level
to
+21 dBm
.
Operating Mode
to
Active Cell
(pressing the
CALL SETUP
key quickly brings you back to the top level
Call Control
menu).
Cell Power
(
F7
on
Call Parms 1 of 3
) to
-86 dBm/3.84 MHz
.
Channel Type
(
F8
) to
12.2k RMC + HSPA
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Generator Info
(
F3
on
Call Control 2 of 6
), select
Downlink Channel Levels
(
F3
), select
Connected DL Channel Levels
(
F3
), then select
HSPA Conn DL Channel Levels
(
F4
).
HSPA Cell 1 Connected CPICH Level
to
-10 dB
(this is the default value).
HSPA Cell 1 Connected P-CCPCH/SCH Level
to
-12 dB
(this is the default value).
HSPA Cell 1 Connected PICH Level
to
-15 dB
(this is the default value).
HSPA Cell 1 Connected (F-)DPCH Level
to
-10 dB
(this is the default value).
HSPA Cell 1 Connected E-AGCH Level
to
-20 dB
(this is the default value).
HSPA Cell 1 Connected E-HICH Level
to
-20 dB
(this is the default value).
HSPA Cell 1 Connected E-RGCH Level
to
Off
(this is the default value).
HSPA Cell 1 Connected HS-PDSCHs Level (Sum)
to
-3 dB
(this is the default value).
HSPA Cell 1 Connected HS-SCCH 1 Level
to
-8 dB
.
HSUPA Parameters
(
HSPA Parameters
(
F10
),
F9
).
HSUPA RB Test Mode Setup
(
F8
).
Common HSUPA Parameters
(
F9
).
E-DPCCH/DPCCH Power Offset (DeltaE-DPCCH)
to
6
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1). Note, 34.121-1 Table C.11.1.3 provides Beta
ec
(209/225 for sub-test 1). To determine what value of DeltaE-DPCCH corresponds to this, use 3GPP TS 25.213 Table 1B and the value of Beta
c
from 34.121-1 Table C.11.1.3 (11/15 for sub-test 1). For sub-test 1, A
ec
= Beta
ec
/Beta
c
= (209/225)/(11/15) = 19/15; therefore DeltaE-DPCCH = 6.
Reference E-TFCI Power Offsets
to
Definition 34.121-01
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Serving Grant
(
F10
).
RB Setup AG
to
26: (119/15)^2
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1). Note, 34.121-1 Table C.11.1.3 AG Index corresponds to 3GPP TS 25.212 s4.10.1A.1 Table 16B, which maps the Absolute Grants sent on the E-AGCH. To send the equivalent Absolute Grant in the RB Setup message, you must use the AG Index in 3GPP TS 25.321 s9.2.5.2.1.1 Table 9.2.5.2.1.1.
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Call Control 2 of 6
menu)
PS Domain Information
to
Present
(this is the default value in the lab application).
Cell Info
,
Reselection Parameters
(
F3
).
RB Test Mode Setup
(
F6
on
Call Control 3 of 6
) and set
UE Loopback Type
to
Type 1
(this is the default value).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Algorithm
to
Two
(this is the default value) (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
PS Domain Information
parameter must be set to
Present
when the UE registers (attaches) with the test set.
Originate Call
(
F3
on
Call Control 1 of 6
).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Mode
to
Active bits
(this is the default value).
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
2 dBm
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1, power class 3 UE). This value is determined as follows: Maximum power for a power class 3 UE is +24 dBm, but
UE Target Power
only sets the DPCCH+DPDCH power level of the UE. In order to achieve a total output power of +16.5 dBm (24 dBm - 7.5 dB), you must set
UE Target Power
to at most 16.5 dBm -
Power change due to HS-DPCCH, E-DPCCH and E-DPDCH
.
UE Target Power
to 2 dBm for sub-test 1.
UE Target Power
values for sub-tests 2-5 are as follows: sub-test 2: 11 dBm, sub-test 3: 3 dBm, sub-test 4: 14 dBm, sub-test 5: 6 dBm.
Channel Power
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Alternating bits
(for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
Additional Screens
(
F1
from
Call Control 2 of 6
), select
HSPA Information
(
F2
) and observe the
Last Received E-TFCI
(it should be 75 for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1, 67 for sub-test 2, 92 for sub-test 3, 71 for sub-test 4 and 67 for sub-test 5).
E-TFCI Recording Information
(
F3
) (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1).
HSPA Parameters
(
F10
),
HSUPA Parameters
(
F9
),
E-TFCI Recording
(
F11
),
E-TFCI Recording Parameters
(
F7
) (for 34.121-1 v8.10.0 Table C.11.1.3 sub-test 1):
E-TFCI Recording Count
to
15
(this is the default value).
Send Step Up TPC Bit Pattern
(
F10
) and then
Start Recording E-TFCI Values
(
F8
).
Send Step Down TPC Bit Pattern
(
F11
) and then
Start Recording E-TFCI Values
(
F8
).
Spectrum Emission Mask
.
Handovers
(
F5
)) to change the following settings:| Setting | Sub-test 2 | Sub-test 3 | Sub-test 4 | Sub-test 5 |
|---|---|---|---|---|
| TCR DPCH Bc/Bd Control | Manual | Manual | Manual | Manual |
| TCR Manual Uplink DPCH Bc | 6 | 15 | 2 | 15 |
| TCR Manual Uplink DPCH Bd | 15 | 9 | 15 | 0 |
| TCR DeltaACK, DeltaNACK, DeltaCQI | 8 | 8 | 8 | 0 |
| TCR Ack-Nack Repetition Factor | 3 | 3 | 3 | 3 |
| TCR CQI Feedback Cycle (k) | 4 ms | 4 ms | 4 ms | 4 ms |
| TCR CQI Repetition Factor | 2 | 2 | 2 | 2 |
| TCR E-DPCCH/DPCCH Power Offset | 8 | 8 | 5 | 0 |
| TCR Reference E-TFCI Power Offsets | 34121-01 | 34121-02 | 34121-01 | 34121-03 |
| TCR Absolute Grant | 18: (47/15)^2 | 21: (67/15)^2 | 23: (84/15)^2 | 18: (47/15)^2 |
Channel Type
(
F8
) to
HSPA
.
HSUPA RB Test Mode Setup
(
F8
) and set
RB E-DPDCH Max Channel Codes (HSPA)
to
SF4
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Algorithm
to
One
.
Originate Call
(
F3
on
Call Control 1 of 6
).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
) and set
UL CL Power Ctrl Mode
to
Active bits
.
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
6 dBm
(for power class 3 UE).
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
All Up bits
. Spectrum Emission Mask Measurement Description