Last updated: January 15, 2009
This procedure assumes the test set is in Active Cell Operating Mode . However, this measurement is also available in FDD Test Operating Mode and CW Operating Mode .
 TX Dynamic Power
. 
 TX Dynamic Pwr Setup 
(
F1
).
 Power Step Time
, then proceed with its step down power sequence. When the power sequence is complete, the power results are displayed on the test set's screen.
 
An example result is shown below. Note that the number of power results is always equal to the
 Number of Power Steps 
setting plus one, as the power in slot 0 is the initial power of the UE, before its first step down in power.
 Graph Control 
(
F2
).
 Start Step 
(
F3
) and
 Span 
(
F4
) as needed to view some or all of the power sequence.
 Marker 
(
F2
) to turn on the marker on the graphical display and move the highlighted bar in the numerical results display area.TX Dynamic Power Measurement Description
TX Dynamic Power Measurement Troubleshooting