When in CW operating mode, the test set operates like a signal generator. The basic features provided by CW operating mode are:
Manual receiver control settings made while using the CW operating mode can affect manual receiver settings made in other operating modes. When changing operating modes and using manual receiver settings, always verify that the manual receiver settings are correct for the new operating mode.
The test set in CW operating mode provides any one of three test signals: CW (no modulation), AM (fixed 56% amplitude modulation), and DSB-SC (dual side-band suppressed carrier). An example usage of the test signals is for calibrating mobile stations that use Qualcomm's radioOne Zero Intermediate Frequency (Zero IF) architecture.
You can select any one of three signals with adjustable power level and frequency for output to the currently selected front panel RF connector.
Cell Power
(
F7
). The Cell Power refers to the power found in the entire signal including sidebands if applicable.
RF Gen Freq
(
F8
).
Use the following commands to control each function for CW operating mode: