CALL:HANDoff:RRC:CRELease:REDirect[:STATe]
CALL:HANDoff:RRC:CRELease:REDirect:EUTRa:EARFcn
CALL:HANDoff:RRC:CRELease:REDirect:EUTRa[:BLACklist]
|
THIS COMMAND IS OBSOLETE. Please use the CALL:HANDoff:PCReconfig[:IMMediate] and CALL:HANDoff:SYSTem[:GSM][:IMMediate] commands to perform physical channel reconfigurations and system handoffs. Initiates a handoff while on a call (and in Active Cell mode). Any measurements that have been initiated are aborted when a handoff is initiated. See Handovers . A handoff can initiate a change of downlink UARFCN ( CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:DOWNlink ), a change of uplink UARFCN ( CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink[:MCHannel] ), or a change from W-CDMA system to GSM system ( CALL:SETup[:HANDoff]:SYSTem[:TYPE] ) while maintaining the connection. The W-CDMA to GSM handoff is only available when both the E1963A and E1968A test applications (TAs) are present in the test set and licensed for operation. |
|
| Requirements |
Test Application Revision: A.03 and above: add handoff from W-CDMA to GSM. |
OUTPUT 714;"CALL:HANDoff" |
|
Initiates the
Execute External 8960 Handover
immediate action. See
External 8960 Handover
and
Two-Cell Test System
. |
|
| Requirements |
Lab Application Revision: D.00.04 and above. Test Application Revision: A.18.00 and above, with the required feature license |
OUTPUT 714;"CALL:HANDoff:EXTernal" |
|
|
Sets/queries the Activation Time . This parameter can only be changed when connection status is idle. |
|
| Same as setting | |
| 0 frames | |
| Test Application Revision: A.18.00 and above, with the required feature license | |
OUTPUT 714;"CALL:HANDoff:EXTernal:ATIMe 100" ! Sets Activation Time to 100 frames. |
|
| Performs a Physical Channel Reconfiguration . | |
| Requirements | |
OUTPUT 714;"CALL:HANDoff:PCReconfig" |
|
|
Sets/queries the PCR Activation Time . |
|
| Same as setting | |
| 0 | |
OUTPUT 714;"CALL:HANDoff:PCReconfig:ATIMe 100" ! Sets PCR Activation Time to 1 s (100 x 10 ms = 1 s). |
|
|
Sets/queries PCR Timing Indication (CFN Handling) . |
|
| AUTO | |
|
Test Application Revision: A.07 and above Test Application Revision A.11, added AUTO, changed default from INIT to AUTO Lab Application Revision: C.02 and above Lab Application Revision D.02, added AUTO, changed default from INIT to AUTO |
|
OUTPUT 714;"CALL:HANDoff:PCReconfig:CFNHandling MAINtain" ! Sets PCR Timing Indication (CFN Handling) to Maintain. |
|
|
Sets/queries the RB Test Mode PCR Loopback Messaging State . |
|
| 0 (off) | |
OUTPUT 714;"CALL:HANDoff:PCReconfig:RBTest:LMESsaging:STATe On" ! Sets RB Test Mode PCR Loopback Messaging State to On. |
|
|
For external PS handover, this command performs an Outbound PS Handover action. The transparent message must be set before trying to execute the handover. See CALL:HANDoff:PS:OUTBound:TMessage . |
|
| Requirements | |
OUTPUT 714;"CALL:HANDoff:PS:OUTBound" |
|
|
Sets/queries the Activation Time .
This parameter specifies the time delay (in frame) from issuing the outbound handover command to the handover actually taking effect . If this value is set to |
|
| 0 - 255 | |
| 0 | |
OUTPUT 714;"CALL:HANDoff:PS:OUTBound:ATIMe 0" ! Sets the outbound PS handover activation time to 0 frame. |
|
|
Sets/queries the "E-UTRA message" IE (transparent message) of the HANDOVER FROM UTRAN COMMAND message. The same data should be generated externally to describe the waiting dedicated resources on LTE. The test set will not parse or act on any of the data contained in this message. This setting is for GIPB command only. See also Execute Handover . |
|
| Ascii string of hex digits | |
| Same as setting | |
| Empty string | |
OUTPUT 714;"CALL:HANDoff:PS:OUTBound:TMESsage "200601C83A1008783200078880081000EA900E08482FF7F7F7F7D7D7D7D03A0B3B4B632B73A0280CE46B86D2C192805FB007888009180D55DE6000BA7B4381A93B80327A03EA05B1C419AA81C0"" ! Sets up the transparent hex string to be copied to the HandoverFromUtranCommand message. |
|
| For PS/SRVCC handover, this command performs an Abort Inbound action. | |
| Requirements | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:ABORt" |
|
|
For inbound PS/SRVCC handover (handover from another RAT to WCDMA), when the test set's set up dedicated resources for the UE, this command returns a hex string defining the HANDOVER TO UTRAN COMMAND message. The source RAT treats this as a transparent message to be blindly passed to the UE. Note that the information contained in this message is only valid while the resources are set up for an inbound handover. See Setup Inbound . It will be removed when the handover state is terminated (either by aborting, preset or a successful handover). This setting is for GIPB command only. . |
|
| A hex string describing the set up channels | |
| Empty string | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:HOCommand?" |
|
| For PS/SRVCC handover, this command performs a Setup Inbound action. | |
| Requirements | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound" |
|
|
Sets/queries the PS EPS Bearer ID . |
|
| Same as setting | |
| 5 | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:PS:EBID 10" ! Sets the EPS Bearer ID on LTE for PS handover to 10. |
|
|
Sets/queries the PS State . |
|
| Range: 1|0 | |
| 0 (off) | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:PS:STATe On" ! Enables PS handover. |
|
|
Sets/queries the Security . |
|
| Same as setting | |
| RENegotiate | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:SECurity RENegotiate" ! Sets the inbound handover security type to RENegotiate. |
|
|
Sets/queries the SRVCC EPS Bearer ID . |
|
| Same as setting | |
| 5 | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:SRVCC:EBID 10" ! Sets the EPS Bearer ID on LTE for SRVCC handover to 10. |
|
|
Sets/queries the automatic state of the RTP Payload Type parameter. |
|
| Range: 1|ON|0|OFF | |
| 1 | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:SRVCc:RPT:AUTO 1" ! Sets the RTP payload type to the value found in any inbound RTP frame. |
|
| The setting form of this command performs two functions: (1) sets the RTP payload type manually (2) sets the CALL:HANDoff:PSSRvcc:INBound:SRVCc:RPT:VALue | |
| Range:1 to 255 | |
| 98 | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:SRVCc:RPT:MVALue 5" ! Sets the RTP value to 5 manually. |
|
| Sets/queries the RTP Payload Type | |
| Range:1 to 255 | |
| 98 | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:SRVCc:RPT:VALue 5" ! Sets the RTP value to 5. |
|
|
Sets/queries the SRVCC State . |
|
| 1|0 | |
| 0 (off) | |
OUTPUT 714;"CALL:HANDoff:PSSRvcc:INBound:SRVCC:STATe On" ! Enables SRVCC handover. |
|
| Performs a Radio Bearer Reconfiguration . | |
| Requirements | |
OUTPUT 714;"CALL:HANDoff:RBReconfig" |
|
|
Sets/queries the RBR Timing Indication (CFN Handling) . |
|
| AUTO | |
|
Test Application Revision: A.09 and above Test Application Revision A.11, added AUTO, changed default from INIT to AUTO Lab Application Revision: C.04 or D.00.04 and above Lab Application Revision D.02, added AUTO, changed default from INIT to AUTO |
|
OUTPUT 714;"CALL:HANDoff:RBReconfig:CFNHandling MAINtain" ! Sets RBR Timing Indication (CFN Handling) to Maintain. |
|
|
Sets/queries the RBR Channel (UARFCN) State . |
|
| 0 (off) | |
OUTPUT 714;"CALL:HANDoff:RBReconfig:CHANnel:STATe OFF" ! Sets RBR Channel (UARFCN) State to Off. |
|
|
Sets/queries the Redirection IE Inclusion State . |
|
| 0 (Off) | |
OUTPUT 714;"CALL:HANDoff:RRC:CRELease:REDirect:STATe ON" ! Sets the `Redirect Info' element be included in the RRC-Release message being sent. |
|
|
Sets/queries the E-UTRA Blacklisted Cell Inclusion State . |
|
| 0 (Off) | |
OUTPUT 714;"CALL:HANDoff:RRC:CRELease:REDirect:EUTRa:BLACklist OFF" ! Sets the E-UTRA Blacklisted Cells list be not included in the RRC-Release redirection information. |
|
|
Sets/queries the E-UTRA Blacklisted Cell Physical Cell ID . |
|
| Same with setting. | |
| 0 | |
OUTPUT 714;"CALL:HANDoff:RRC:CRELease:REDirect:EUTRa:BLACklist:CID 1" ! Sets the E-UTRA physical cell ID used in the RRC-Release redirection blacklist to 1. |
|
|
Sets/queries the E-UTRA EARFCN . |
|
| 300 | |
OUTPUT 714;"CALL:HANDoff:RRC:CRELease:REDirect:EUTRa:EARFcn 500" ! Sets the E-UTRA EARFCN used in the RRC-Release redirection information to 500. |
|
| Performs a System Handover . | |
| Requirements |
GSM/GPRS_W-CDMA Fast Switching Test Application Revision: B.04 and above. E1987A GSM/GPRS_W-CDMA Fast Switching Test Application Revision A.03.20, :GSM is optional. GSM/GPRS_W-CDMA Fast Switching Lab Application Revision: B.01 and above. E6785C GSM/GPRS_W-CDMA Fast Switching Lab Application Revision C.03, :GSM is optional. |
OUTPUT 714;"CALL:HANDoff:SYSTem" |
|
| This command sets/queries Wait for RLC Ack of Handover From UTRAN . | |
| 1 (on) | |
| Requirements |
E1987A GSM/GPRS_W-CDMA Fast Switching Test Application Revision A.03.20 and above. E6785C GSM/GPRS_W-CDMA Fast Switching Lab Application Revision C.03 and above. |
OUTPUT 714;"CALL:HANDoff:SYSTem:RLCack:WAIT Off" ! Sets Wait for RLC Ack of Handover From UTRAN to Off. |
|
| Performs a Transport Channel Reconfiguration . | |
| Requirements | |
OUTPUT 714;"CALL:HANDoff:TCReconfig" |
|
|
Sets/queries the TCR Timing Indication (CFN Handling) . |
|
| AUTO | |
|
Test Application Revision: A.07 and above Test Application Revision A.11, added AUTO, changed default from INIT to AUTO Lab Application Revision: C.02 Lab Application Revision D.02, added AUTO, changed default from INIT to AUTO |
|
OUTPUT 714;"CALL:HANDoff:TCReconfig:CFNHandling MAINtain" ! Sets TCR Timing Indication (CFN Handling) to Maintain. |
|
|
Sets/queries the TCR Channel (UARFCN) State . |
|
| 0 (off) | |
OUTPUT 714;"CALL:HANDoff:TCReconfig:CHANnel:STATe OFF" ! Sets TCR Channel (UARFCN) State to Off. |
|
|
Sets/queries the RB Test Mode TCR Loopback Messaging State . |
|
| 0 (off) | |
OUTPUT 714;"CALL:HANDoff:TCReconfig:RBTest:LMESsaging:STATe OFF" ! Sets RB Test Mode TCR Loopback Messaging State to Off. |
|