The following handovers are available in the test set:
The following table outlines the RAB reconfigurations that may be performed within a single test set while on a connection. For information on handovers available between two test sets ( lab application only ), see Two-Cell Test System .
|
GSM Voice ( Fast Switching applications only ) |
HSDPA RB Test Mode: FRC (CS/PS Domain) |
HSDPA RB Test Mode: User Defined (CS Domain) |
HSDPA RB Test Mode: User Defined (PS Domain) |
HSDPA RB Test Mode: User Defined (CS/PS Domain) |
HSPA RB Test Mode |
||||
| System Handover | |||||||||
| System Handover | Transport Channel Reconfig | ||||||||
| System Handover | Radio Bearer Reconfig | Transport Channel Reconfig 2 | Transport Channel Reconfig 2 | ||||||
| Transport Channel Reconfig 2 | Transport Channel Reconfig 2 | ||||||||
| System Handover 1 | Radio Bearer Reconfig | Transport Channel Reconfig 2 | Transport Channel Reconfig 2 | ||||||
| System Handover | Radio Bearer Reconfig | Transport Channel Reconfig 2 | Transport Channel Reconfig | ||||||
| Transport Channel Reconfig 2 | Transport Channel Reconfig | ||||||||
| System Handover 1 | Radio Bearer Reconfig | Transport Channel Reconfig 2 | Transport Channel Reconfig | ||||||
| System Handover | Radio Bearer Reconfig | ||||||||
|
1 You can perform a System Handover while on an CS/PS Domain HSDPA RB Test Mode connection. However, if you end the resulting GSM/GPRS/EGPRS connection and switch back to the W-CDMA format, your initial attempt to establish a CS Domain or CS/PS Domain HSDPA RB Test Mode connection may fail; you may need to initiate the connection attempt a second time.
2
This RAB reconfiguration cannot be performed when |
|||||||||
A Physical Channel Reconfiguration can be used for inter-frequency hard handovers and also to change power control algorithm and step size while on a connection (you cannot simply change the
DL Channel
and
Uplink Channel
or power control algorithm settings while on a call, you must perform a handover to change them).
You must be on a call to perform a Physical Channel Reconfiguration.
Before executing a Physical Channel Reconfiguration, you must first specify the settings you wish to change (for example, downlink and uplink UARFCNs to which to handover). You must then select
Execute Handover
(
F5
) or send the
CALL:HANDoff:PCReconfig[:IMMediate]
command to initiate the reconfiguration.
Upon completion of the handover (successful or not, and regardless of any errors), the handover settings are copied to their corresponding non-handover parameters (for example, the
DL Channel
and
Uplink Channel
settings are set to the value of
Handover Downlink Channel (UARFCN)
and
Handover Uplink Channel (UARFCN)
upon completion of the Physical Channel Reconfiguration).
Handover Downlink Channel (UARFCN)
This setting determines the downlink channel the UE is instructed to use after completion of the Physical Channel Reconfiguration. See DL Channel for more information.
GPIB command: CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:DOWNlink .
You can directly set the
Handover Uplink Channel (UARFCN)
setting to a specific uplink UARFCN value. The UE is instructed to use this uplink channel after completion of the Physical Channel Reconfiguration.
GPIB command: CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink[:MCHannel] .
When
Handover Uplink Channel
is set to
Auto
, the handover uplink UARFCN is automatically determined by the
Handover Downlink Channel (UARFCN)
setting. The test set subtracts the frequency separation associated with the handover downlink channel's band from the
Handover Downlink Channel (UARFCN)
setting, and instructs the UE to use this uplink channel after completion of the Physical Channel Reconfiguration.
GPIB command: CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO
See Uplink Channel for more information.
When you set
Handover Downlink Channel (UARFCN)
to a value in Band VI, you must specify whether you want the test set to send a Band V or Band VI Frequency Band Indicator using the
Handover Band Arbitrator
setting. See
Band Arbitrator
for more information.
GPIB command: CALL:SETup[:PCReconfig]:CHANnel:BARBitrator
This setting determines the closed loop power control algorithm the UE is instructed to use after completion of the Physical Channel Reconfiguration procedure. See UL CL Power Ctrl Algorithm for more information.
GPIB command: CALL:SETup:CLPControl:UPLink:ALGorithm
This setting determines the power control step size the UE is instructed to use after completion of the Physical Channel Reconfiguration procedure when
Handover UL CL Power Ctrl Algorithm
is set to
One
. This setting can only be changed when
Handover UL CL Power Ctrl Algorithm
is set to
One
. Also, if
Handover UL CL Power Ctrl Algorithm
is set to
Two
, this setting is returned to its default value of
1 dB
. See
UL CL Power Ctrl Stepsize
for more information
.
GPIB command: CALL:SETup:CLPControl:UPLink:STEPsize
You can specify whether the UE should maintain or initialise its CFN counter when performing the Physical Channel Reconfiguration. See RB setup Timing Indication (CFN Handling): for additional details. Note that 3GPP 25.331 v5.17.0 s8.6.6.28 states that the UE's behavior is undefined if the network sets the Timing Indication IE to Initialise on a non-hard handover (i.e. where the UARFCNs and one or more Primary Scrambling Codes remain unchanged as part of the reconfiguration).
PCR Timing Indication (CFN Handling)
is set to
Auto
, the Timing Indication information element sent in the Physical Channel Reconfiguration message is set to Initialise if
Handover Downlink Channel (UARFCN)
and
Handover Uplink Channel (UARFCN)
are set such that a hard handover will occur (UARFCNs will change). Otherwise, the Timing Indication information element sent in the Physical Channel Reconfiguration message is set to Maintain.GPIB command: CALL:HANDoff:PCReconfig:CFNHandling .
You can specify whether the UE loopback is opened or closed as part of a Physical Channel Reconfiguration. This parameter only affects the Physical Channel Reconfiguration procedure when an RB Test Mode call is active (as the loopback is never closed on any other call type).
On
: The test set sends an Open UE Test Loop message before sending the Physical Channel Reconfiguration message and a Close UE Test Loop message after receiving the Physical Channel Reconfiguration Complete message from the UE.
Note, opening and closing the UE test loop clears the UE's buffer and resets its loopback delay (see BER Synchronization requirements ).
Note, if a Close UE Test Loop message is not sent to the UE when establishing an asymmetrical RMC, you cannot send an Open UE Test Loop message as part of the Physical Channel Reconfiguration (see
Asymmetric RMC Loopback Messaging
). If
RB Test Mode PCR Loopback Messaging State
is set to
On
and
Asymmetric RMC Loopback Messaging
is set to
Off
and the current connection is an asymmetrical RMC, the test set will not send the Open/Close UE Test Loop messages.
Off
: The test set does not send any loopback control messages as part of the Physical Channel Reconfiguration procedure.GPIB command: CALL:HANDoff:PCReconfig:RBTest:LMESsaging:STATe
This parameter allows you to set the Activation Time that is signaled to the UE in the Physical Channel Reconfiguration message (see 3GPP TS 25.331 s10.3.3.1). Activation Time controls the frame number at which the operation caused by the related message shall take effect (in other words, how long the UE should wait before moving to the new frequency). It can be set between 0 and 255, and indicates the absolute value of the CFN (Connection Frame Number) at which the UE should perform the handover. If set to 0, the Activation Time IE is not sent in the Physical Channel Reconfiguration message.
For most UEs, an Activation Time of 0 ("now") is appropriate. But for some UEs, the handover will fail if Activation Time is left at its default value of 0, as explained in the following:
When the test set orders a Physical Channel Reconfiguration, it takes a finite amount of time for the test set to move to and settle at the new frequency. When the Physical Channel Reconfiguration is ordered, most UEs wait a time of T312 at the new frequency before determining that the handover has failed (T312 is signalled by the test set in SIB1 with a value of 5 seconds). If your UE does not wait once moving to the new frequency, the handover may fail. If it does, set the Activation Time as needed to cause the UE to wait until the test set has moved to the new frequency (a setting of 100 (100 x 10 ms = 1 s) is usually sufficient).
Do not set
PCR Activation Time
to a value other than 0 unless necessary, as it slows down the handover procedure.
GPIB command: CALL:HANDoff:PCReconfig:ATIMe
This parameter specifies whether the N th serving cell downlink UARFCN should use UARFCNs that are in the single band, dual band, or any customized band during the Physical Channel Reconfiguration procedure.
GPIB command: CALL:SETup[:PCReconfig]:HSDPa:MCARrier:BAND:CONFig[:TYPE]
This parameter specifies whether
Handover Secondary Cell DL Adjacent UARFCN
or
Handover Secondary Cell DL Manual UARFCN
is used as the UARFCN of the secondary serving cell for
Physical Channel Reconfiguration
. This setting applies when
Handover Dual Carrier Band Configuration
is set to
Single Band
.
GPIB command: CALL:SETup[:PCReconfig]:SSCell:CHANnel:CONFig[:TYPE]
This parameter specifies the target downlink UARFCN of the secondary serving cell, whether to be
Higher
or
Lower
compared to the serving cell by
Physical Channel Reconfiguration
. This setting applies when
Handover Dual Carrier Band Configuration
is set to
Single Band
and
Handover Secondary Cell DL Channel Config
is set to
Adjacent
.
GPIB command: CALL:SETup[:PCReconfig]:SSCell:CHANnel:ADJacent
This parameter specifies the target downlink UARFCN of the secondary serving cell by Physical Channel Reconfiguration . This setting is available when:
Single Band
and
Handover Secondary Cell DL Channel Config
is set to
Manual
.
Dual Band
or
User Defined
.GPIB command: CALL:SETup[:PCReconfig]:SSCell:CHANnel:MANual:UARFcn
This parameter determines whether the test set sends a Band V or Band VI Frequency Band Indicator. See Band Arbitrator for more information.
This parameter is available when:
Manual
.
Single Band
.GPIB command: CALL:SETup[:PCReconfig]:SSCell:CHANnel:MANual:BARBitrator
This parameter specifies the Mobile Country Code that is signalled to the UE during the Physical Channel Reconfiguration procedure.
GPIB command: CALL:SETup[:PCReconfig]:MCCode
This parameter specifies the Mobile Network Code that is signalled to the UE during the Physical Channel Reconfiguration procedure.
GPIB command: CALL:SETup[:PCReconfig]:MNCode
This parameter specifies the length of Handover MNC (Mobile Network Code) .
Handover MNC (Mobile Network Code) Length
is set to
Auto
, the MNC will be transmitted in 2 digits if the MNC is less or equal to 99 and 3 digits otherwise.
Handover MNC (Mobile Network Code) Length
is set to
3 Digits
, the MNC will be transmitted in 3 digits, prepending one or two zeros if necessary.GPIB command: CALL:SETup[:PCReconfig]:MNCode:LENGth
When the
Current MIMO Configuration Status
is set to
Active
, this parameter controls the
N_cqi_typeA/M_cqi Ratio
on the UL HS-DPCCH that is signalled to the UE during the
Physical Channel Reconfiguration
procedure.
GPIB command: CALL:SETup[:PCReconfig]:MIMO:NMRatio
When the
Current MIMO Configuration Status
is set to
Active
, this parameter controls the pilot channel the UE uses for the antenna 2 that is signalled to the UE during the
Physical Channel Reconfiguration
procedure.
GPIB command: CALL:SETup[:PCReconfig]:ANTenna2:PILot:CONFig
SIB11 Inter-Freq Cell Info List
(see
Inter-frequency Cells
).The Transport Channel Reconfiguration provides three main functions:
Before executing a Transport Channel Reconfiguration, you must first specify the settings you wish to change (for example, RMC to which to handover). You must then select
Execute Handover
(
F5
) or send the
CALL:HANDoff:TCReconfig[:IMMediate]
command to initiate the reconfiguration.
Upon completion of the Transport Channel Reconfiguration (successful or not, and regardless of any errors), the handover settings are copied to their corresponding non-handover parameters (for example, the
Channel Type
setting is set to the value of the
RB Test Mode TCR RAB
setting).
The Transport Channel Reconfiguration operation allows you to handover between Symmetrical RMCs while on a Radio Bearer Test Mode call. You must be on a (non-HSDPA/non-HSPA) RB test mode symmetrical RMC connection to perform a Transport Channel Reconfiguration between RMCs.
This setting determines the symmetrical RMC the UE is instructed to use after completion of the Transport Channel Reconfiguration. See Channel Type for more information.
GPIB command: CALL:SETup:TCReconfig:RBTest:RAB
Cell Off Operating Mode
or
Idle
Connection Status while on a Connection
Some
Cell Parameters
and
Uplink Parameters
cannot be changed when in
Active Cell Operating Mode
or while on a connection. The Transport Channel Reconfiguration operation allows you to change some of the key cell and uplink settings while on a connection. The Transport Channel Reconfiguration also allows you to perform an inter-frequency hard handover.
You must be on an RB test mode symmetrical RMC connection (non-HSDPA, HSDPA or HSPA) to change these settings.
You can perform a hard handover (change UARFCNs) as part of the Transport Channel Reconfiguration. This allows you to perform a legal timing re-initialised handover (see RB setup Timing Indication (CFN Handling): and Current DPCH Offset for more details).
When
TCR Channel (UARFCN) State
is set to
On
,
TCR Downlink Channel (UARFCN)
and
TCR Uplink Channel (UARFCN)
are signalled to the UE during the Transport Channel Reconfiguration if either differs from the current UARFCNs. When
TCR Channel (UARFCN) State
is set to
Off
, no UARFCN information is sent to the UE.
GPIB command: CALL:HANDoff:TCReconfig:CHANnel:STATe
This setting determines the downlink channel the UE is instructed to use after completion of the Transport Channel Reconfiguration. See DL Channel for more information.
GPIB command: CALL:SETup:TCReconfig:CHANnel:DOWNlink
This setting is only applicable when
TCR Channel (UARFCN) State
is set to
On
.
You can directly set the
TCR Uplink Channel (UARFCN)
setting to a specific uplink UARFCN value. The UE is instructed to use this uplink channel after completion of the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:CHANnel:UPLink[:MCHannel]
This setting is only applicable when
TCR Channel (UARFCN) State
is set to
On
.
When
TCR Uplink Channel
is set to
Auto
, the handover uplink UARFCN is automatically determined by the
TCR Downlink Channel (UARFCN)
setting. The test set subtracts the frequency separation associated with the handover downlink channel's band from the
TCR Downlink Channel (UARFCN)
setting, and instructs the UE to use this uplink channel after completion of the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:CHANnel:UPLink:CONTrol:AUTO
This setting is only applicable when
TCR Channel (UARFCN) State
is set to
On
.
See Uplink Channel for more information.
When you set
TCR Downlink Channel (UARFCN)
to a value in Band VI, you must specify whether you want the test set to send a Band V or Band VI Frequency Band Indicator using the
TCR Band Arbitrator
setting. See
Band Arbitrator
for more information.
GPIB command: CALL:SETup:TCReconfig:CHANnel:BARBitrator
This parameter selects whether the DPCH gain settings signalled to the UE during the Transport Channel Reconfiguration are set manually (using the TCR Manual Uplink DPCH Bc and TCR Manual Uplink DPCH Bd settings) or automatically by the test set (using the RB Test Mode TCR RAB setting). Note that configuring Bc and Bd such that neither is set to 15 is undefined in the standards, and may result in unexpected behavior. See Uplink DPCH Bc/Bd Control for more information about how the test set automatically determines the gain settings.
You can query the beta c and beta d values that the test set will signal to the UE during the Transport Channel Reconfiguration using the CALL:STATus:SETup:TCReconfig:DPCHannel:CBETa? and CALL:STATus:SETup:TCReconfig:DPCHannel:DBETa? commands.
GPIB command: CALL:SETup:TCReconfig:DPCHannel:BETA:AUTO
When
TCR DPCH Bc/Bd Control
is set to
Manual
, this parameter controls the uplink DPCCH gain setting (beta
c
) signalled to the UE during the Transport Channel Reconfiguration. Range is 1 to 15 (see 3GPP TS 25.213 s4.2.1.1 Table 1 for a mapping of the signalled values to the resulting quantized amplitude ratios).
See Manual Uplink DPCH Bc for more information.
GPIB command: CALL:SETup:TCReconfig:DPCHannel:MANual:CBETa
When
TCR DPCH Bc/Bd Control
is set to
Manual
, this parameter controls the uplink DPDCH gain setting (beta
d
) signalled to the UE during the Transport Channel Reconfiguration.
See Manual Uplink DPCH Bd for more information.
GPIB command: CALL:SETup:TCReconfig:DPCHannel:MANual:DBETa
You can specify whether the UE should maintain or initialise its CFN counter when performing the Transport Channel Reconfiguration. See RB setup Timing Indication (CFN Handling): for additional details. Note that 3GPP 25.331 v5.17.0 s8.6.6.28 states that the UE's behavior is undefined if the network sets the Timing Indication IE to Initialise on a non-hard handover (i.e. where the UARFCNs and one or more Primary Scrambling Codes remain unchanged as part of the reconfiguration).
TCR Timing Indication (CFN Handling)
is set to
Auto
, the Timing Indication information element sent in the Transport Channel Reconfiguration message is set to Initialise if
TCR Downlink Channel (UARFCN)
and
TCR Uplink Channel (UARFCN)
are set such that a hard handover will occur (UARFCNs will change) or if
TCR Default DPCH Offset (DOFF)
is set to a value other than the
Current DPCH Offset
(this latter condition is to maintain backwards-compatibility with earlier releases). Otherwise, the Timing Indication information element sent in the Transport Channel Reconfiguration message is set to Maintain.GPIB command: CALL:HANDoff:TCReconfig:CFNHandling .
When
TCR Timing Indication (CFN Handling)
is set to
Initialise
, the test set includes both the
Default DPCH Offset
and
DPCH Frame Offset
information elements in the Transport Channel Reconfiguration message. Both information elements are sent with a value equal to the
TCR Default DPCH Offset (DOFF)
setting. Note, however, that the resolution of the
Default DPCH Offset
information element is 512 chips and the resolution of the
DPCH Frame Offset
information element is 256 chips. Thus, if
TCR Default DPCH Offset (DOFF)
is set to 3 x 512 chips, for example, then
Default DPCH Offset
is sent with a value of 3 (x 512 chips) and
DPCH Frame Offset
is sent with a value of 6 (x 256 chips). Thus, the
TCR Default DPCH Offset (DOFF)
setting can be used to change the DPCH Frame Offset (tau
DPCH
) to 0, 1, ..., 75 x 512 chips while on a connection.
The Current DPCH Offset result indicates the DPCH Frame Offset currently in use by the test set (for the current operating mode).
Note, 3GPP TS 25.331 v5.17.0 s8.6.6.28 states that the timing re-initialized reconfiguration required to send the Default DPCH Offset IE must also include a change in UARFCN or Primary Scrambling Code, or the UE's behavior is undefined.
GPIB command: CALL:SETup:TCReconfig:DPCHannel:DOFFset
When
TCR Timing Indication (CFN Handling)
is set to
Maintain
, the test set sends only the
DPCH Frame Offset
information element in the Transport Channel Reconfiguration message. The value of the
DPCH Frame Offset
information element is determined by the
Current DPCH Offset
and the
TCR Relative DPCH Frame Offset
setting. The
TCR Relative DPCH Frame Offset
setting can be used to change the current DPCH Frame Offset (tau
DPCH
) by -256, 0 or +256 chips while on a connection.
The Current DPCH Offset result indicates the DPCH Frame Offset currently in use by the test set (for the current operating mode).
GPIB command: CALL:SETup:TCReconfig:DPCHannel:RFOFfset
RB Test Mode TCR Loopback Messaging State
This parameter controls whether the UE loopback is opened and closed as part of a Transport Channel Reconfiguration procedure.
On
- the test set will send an Open UE Test Loop message before sending the Transport Channel Reconfiguration message and a Close UE Test Loop message after receiving the Transport Channel Reconfiguration Complete message from the UE.
Off
- the test set will not send any loopback control messages as part of the Transport Channel Reconfiguration procedure.GPIB command: CALL:HANDoff:TCReconfig:RBTest:LMESsaging:STATe
This section is only applicable to the lab application or feature-licensed test application.
Some of the HSPA parameters cannot be changed while on a connection. The Transport Channel Reconfiguration operation allows you to change these parameters while on a connection.
You must be on an HSDPA or HSPA RB Test Mode connection to change these settings using a Transport Channel Reconfiguration.
Controls the DeltaACK value signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:UPLink:DACK
Controls the DeltaNACK value signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:UPLink:DNACk
Controls the DeltaCQI value signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:UPLink:DCQI
Controls the Ack-Nack Repetition Factor value signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:UPLink:ANACk:RFACtor
Controls the
CQI Feedback Cycle (k)
value signalled to the UE during the Transport Channel Reconfiguration.
TCR CQI Feedback Cycle (k)
must be greater than or equal to
TCR CQI Repetition Factor
* 2ms (except for the case when
TCR CQI Feedback Cycle (k)
equals 0 ms).
GPIB command: CALL:SETup:TCReconfig:UPLink:CQI:FCYCle
Controls the
CQI Repetition Factor
value signalled to the UE during the Transport Channel Reconfiguration.
TCR CQI Feedback Cycle (k)
must be greater than or equal to
TCR CQI Repetition Factor
* 2ms (except for the case when
TCR CQI Feedback Cycle (k)
equals 0 ms).
GPIB command: CALL:SETup:TCReconfig:UPLink:CQI:RFACtor
The following parameters are only available while on a
User Defined
HSDPA or HSPA RB Test Mode connection.
Controls the User Defined Number of HARQ Processes value signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:HARQ:PROCess:COUNt
Controls the User Defined UE IR Buffer Allocation value signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:MS:IREDundancy:BUFFer:ALLocation
Controls the User Defined Explicit UE IR Buffer Size value signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:MS:IREDundancy:BUFFer:SIZe[:EXPLicit]
This setting is only applicable when
TCR UE IR Buffer Allocation
is set to
Explicit
.
Controls the Meas Pow Offset value signaled to the UE during the Transport Channel Reconfiguration.
GPIB commands: CALL:SETup:TCReconfig:MPOWer[:MOFFset] , CALL:SETup:TCReconfig:MPOWer:OFFSet:CONTrol:AUTO , CALL:SETup:TCReconfig:MPOWer:OFFSet:MANual
The following parameters are only available while on an HSPA RB Test Mode connection:
Controls the E-DPCCH/DPCCH Power Offset (DeltaE-DPCCH) signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:EDPCchannel[:DPCChannel]:POFFset
Controls the Predefined Reference E-TFCI Power Offsets signalled to the UE during the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:ETFCi:POFFsets:REFerence
Controls whether the test set signals the UE to operate in UL 16QAM mode for E-DCH during Transport Channel Reconfiguration procedure.
This parameter should be set while the HSPA call is setup and the
E-DCH TTI
is
2 ms
.
GPIB command: CALL:SETup:TCReconfig:EDCHannel:QAM16[:STATE]
Controls the serving grant that is signalled to the UE during the Transport Channel Reconfiguration. This serving grant is specified in terms of the 3GPP TS 25.321 s9.2.5.2.1.1 Scheduling Grant Table (and is not determined by the 3GPP TS 25.212 s4.10.1A.1 table that is used to communicate absolute grants on the E-AGCH). See Serving Grant for more information.
Unlike the other Transport Channel Reconfiguration parameters, the value of this setting is not copied to any of the serving grant parameters (such as Single Shot AG or RB Setup AG ) upon completion of the Transport Channel Reconfiguration.
GPIB command: CALL:SETup:TCReconfig:SGRant:ABSolute[:VALue]
Controls the serving grant that is signalled to the UE when the
E-DCH TTI
is
2 ms
and the
TCR 16QAM State
is
On
. If any of the condition is not met,
TCR Absolute Grant
will be sent to the UE.
GPIB command: CALL:SETup:TCReconfig:SGRant:ABSolute:QAM16[:VALue]
RB TCR E-DPDCH Max Channelisation Codes
When the
Channel Type
is
12.2k RMC + HSPA
, this parameter controls the value of E-DPDCH Max Channelisation Codes that is signalled to the UE during Transport Channel Reconfiguration procedure.
GPIB Command: CALL:SETup:TCReconfig:RBTest:EDPDchannel:CCODes:MAX[:HSPARMC12]
RB TCR E-DPDCH Max Channelisation Codes (HSPA Only)
When the
Channel Type
is
HSPA
, this parameter controls the value of E-DPDCH Max Channelisation Codes that is signalled to the UE during Transport Channel Reconfiguration procedure.
GPIB Command: CALL:SETup:TCReconfig:RBTest:EDPDchannel:CCODes:MAX:HSPA
TCR N_cqi_typeA/M_cqi Ratio
This parameter controls the
N_cqi_typeA/M_cqi Ratio
on the UL HS-DPCCH that is signalled to the UE during the
Transport Channel Reconfiguration
procedure. This setting applies when the
Current
Service Type
is
HSDPA RB Test Mode
or
HSPA RB Test Mode,
and the
Current MIMO Configuration Status
is set to
Active
.
If the
Current
Service Type
is set to
None
, the
Channel Type
should be set to
12.2k RMC+HSDPA
or
12.2k RMC+HSPA
to enable the setting TCR Number of HARQ Processes for MIMO.
GPIB Command: CALL:SETup:TCReconfig:MIMO:NMRatio
TCR HSDPA MIMO Antenna 2 Pilot Configuration
This parameter controls the pilot channel the UE uses for the antenna 2, which is signalled to the UE during the
Transport Channel Reconfiguration
procedure. This setting applies when the
Current
Service Type
is HSDPA RB Test Mode or HSPA RB Test Mode, and the
Current MIMO Configuration Status
is set to
Active
, .
If the Current
Service Type
is set to
None
, the
Channel Type
should be set to
12.2k RMC+HSDPA
or
12.2k RMC+HSPA
to enable the setting TCR Number of HARQ Processes for MIMO.
If
TCR HSDPA MIMO Antenna 2 Pilot Configuration
is set to
S-CPICH
, the power offset of S-CPICH relative to P-CPICH would be calculated and rounded to the nearest 1.00 dB (the resolution of the signalled parameter) and limited to -6.00 dB or 0.00 dB (the min/max value of the signalled parameter) automatically and signalled to the UE. There are two calculation ways depending on the current service type:
Current Service Type
is set to HSDPA only (
RB Test Mode/PS Data-HSDPA)
, the calculation is:
UTRA FDD (HSDPA) Serving Cell Antenna 2 S-CPICH Power Offset
minus
UTRA FDD (HSDPA) Serving Cell Antenna 1 P-CPICH Power Offset
. If either
UTRA FDD (HSDPA) Serving Cell Antenna 1 P-CPICH State
or
UTRA FDD (HSDPA) Serving Cell Antenna 2 S-CPICH State
is set to
Off
, then -20.00 dB will be assumed as the relative channel power.
Current Service Type
is set to HSPA (
RB Test Mode/PS Data-HSPA)
, the calculation is:
UTRA FDD (HSPA) Serving Cell Antenna 2 S-CPICH Power Offset
minus
UTRA FDD (HSPA) Serving Cell Antenna 1 P-CPICH Power Offset
. If either
UTRA FDD (HSPA) Serving Cell Antenna 1 P-CPICH State
or
UTRA FDD (HSPA) Serving Cell Antenna 2 S-CPICH State
is set to
Off
, then -20.00 dB will be assumed as the relative channel power.GPIB Command: CALL:SETup:TCReconfig:ANTenna2:PILot:CONFig
TCR Number of HARQ Processes for MIMO
This parameter controls the number of active HARQ processes in the MAC-ehs layer that is signalled to the UE during the
Transport Channel Reconfiguration
procedure. This setting applies when the
Current
Service Type
is HSDPA RB Test Mode or HSPA RB Test Mode, the
Current MIMO Configuration Status
is set to
Active
, and the
HS-DSCH Configuration Type
is set to
User Defined
.
If the current
Service Type
is set to
None
, the
Channel Type
should be set to
12.2k RMC+HSDPA
or
12.2k RMC+HSPA
to enable the setting TCR Number of HARQ Processes for MIMO.
GPIB Command: CALL:SETup:TCReconfig:MIMO:HARQ:PROCess:COUNt
SIB11 Inter-Freq Cell Info List
(see
Inter-frequency Cells
).This functionality is only available in GSM/GPRS_W-CDMA fast switching test and lab applications.
The System Handover functionality allows you to handover to a GSM voice call from any of the following connection types:
CS Domain
(
lab application or feature licensed test application only
)You must be on one of these types of connections to perform a System Handover.
Before executing a System Handover you must specify the characteristics of the target GSM cell. You must also ensure that the GSM/GPRS format is set to
Active Cell
operating mode. You must then select
Execute Handover
(
F5
) or send the
CALL:HANDoff:SYSTem[:GSM][:IMMediate]
command to initiate the handover.
Changing any of the GSM cell settings while operating in the W-CDMA format changes the corresponding parameter settings in the GSM/GPRS format of the fast switching application. Presetting the test set while operating in the W-CDMA format will not reset these parameters to their default settings. Presetting the test set while operating in the GSM/GPRS format will reset these parameters to their default values. When operating in the W-CDMA format, these settings are not saved when using the SAVE REGISTERS utility.
On
, when performing a handover from (non-HSDPA) RB test mode to a GSM voice call, the UE will ring. You must answer the ring for the connection to be completed and testing to progress (note also that the fast switch between the two applications will not complete until you answer the ring).
RB Test Mode to GSM Handover Alerting State
is set to
On
, the test set then continues to establish a CC Connection for voice service. As a result, once the test set and UE have transitioned to GSM service, the UE will alert. See
System Handover from W-CDMA RB Test Mode to GSM Voice (with RB Test Mode to GSM Handover Alerting State = On)
.
Off
, when performing a handover from (non-HSDPA) RB test mode to a GSM voice call, the UE will not ring. When the handover is completed, the connection is left in the RR Connected state. Data loopback (for BER testing) is available in this state, but voice echo is not. See
System Handover from W-CDMA RB Test Mode to GSM Voice (with RB Test Mode to GSM Handover Alerting State = Off)
.GPIB command: CALL:SETup:SYSTem:GSM:ALERting[:STATe] .
This parameter controls whether the test set waits for the UE to confirm reception of the Handover From UTRAN Command message before initiating the fast switch to the GSM/GPRS/EGPRS format (see
Handover Ladder Diagrams
) or whether it switches immediately upon sending the Handover From UTRAN Command message. By default, the test set does not initiate the switch from the W-CDMA to GSM/GPRS/EGPRS application until it receives an RLC Ack confirming reception of the Handover From UTRAN Command message. To shorten the handover time, some UEs do not send any W-CDMA layer 2 acknowledgments for the handover command. If your UE does not acknowledge the Handover From UTRAN command, you must set
Wait for RLC Ack of Handover From UTRAN
to
Off
. Otherwise, the test set will not continue with the handover until it receives the expected acknowledgment, and the handover will fail.
Setting
Wait for RLC Ack of Handover From UTRAN
to
Off
speeds up the System Handover, but is a less robust handover method.
GPIB command: CALL:HANDoff:SYSTem[:GSM]RLCack:WAIT[:STATe]
Note, you MUST include the mnemonic:GSM at the end of this command, i.e. you must issue the command as CALL:BCCode:GSM.
Note, you MUST include the mnemonic:GSM at the end of this command, i.e. you must issue the command as CALL:NCCode:GSM.
Note, you MUST include the mnemonic:GSM at the end of this command, i.e. you must issue the command as CALL:BAND:GSM.
Note, you MUST include the mnemonic:GSM at the end of this command, i.e. you must issue the command as CALL:BCHannel[:ARFCn]:GSM.
This section is only applicable to the lab application or feature-licensed test application.
The Radio Bearer Reconfiguration allows you to handover from a CS Domain or CS/PS Domain HSDPA RB Test Mode connection or HSPA RB Test Mode connection to a (non-HSDPA/non-HSPA) symmetrical RMC. See CN Domain and the following ladder diagram: Radio Bearer Reconfiguration from CS Domain or CS/PS Domain HSDPA RB Test Mode Connection or HSPA RB Test Mode Connection . The Radio Bearer Reconfiguration also allows you to change many other parameters as part of the reconfiguration.
Before executing the Radio Bearer Reconfiguration, you must specify to which symmetrical RMC you wish to handover, and set any other reconfiguration parameters as desired. You must then select
Execute Handover
(
F5
) or send the
CALL:HANDoff:RBReconfig[:IMMediate]
command to initiate the reconfiguration.
Upon completion of the Radio Bearer Reconfiguration (successful or not, and regardless of any errors), the handover settings are copied to their corresponding non-handover parameters (for example, the
Channel Type
setting is set to the value of the
RB Test Mode RBR RAB
setting).
This setting determines the (non-HSDPA) symmetrical RMC the UE is instructed to use after completion of the Radio Bearer Reconfiguration. See Channel Type for more information.
GPIB command: CALL:SETup:RBReconfig:RBTest:RAB
You can perform a hard handover (change UARFCNs) as part of the Radio Bearer Reconfiguration. The change in UARFCNs is performed as part of the RB Setup portion of the procedure (see Radio Bearer Reconfiguration from CS Domain or CS/PS Domain HSDPA RB Test Mode Connection or HSPA RB Test Mode Connection ). This allows you to perform a legal timing re-initialised handover (see RB setup Timing Indication (CFN Handling): and Current DPCH Offset for more details).
When
RBR Channel (UARFCN) State
is set to
On
,
RBR Downlink Channel (UARFCN)
and
RBR Uplink Channel (UARFCN)
are signalled to the UE during the Radio Bearer Reconfiguration if either differs from the current UARFCNs. When
RBR Channel (UARFCN) State
is set to
Off
, no UARFCN information is sent to the UE.
GPIB command: CALL:HANDoff:RBReconfig:CHANnel:STATe
This setting determines the downlink channel the UE is instructed to use after completion of the Radio Bearer Reconfiguration. See DL Channel for more information.
GPIB command: CALL:SETup:RBReconfig:CHANnel:DOWNlink
This setting is only applicable when
RBR Channel (UARFCN) State
is set to
On
.
You can directly set the
RBR Uplink Channel (UARFCN)
setting to a specific uplink UARFCN value. The UE is instructed to use this uplink channel after completion of the Radio Bearer Reconfiguration.
GPIB command: CALL:SETup:RBReconfig:CHANnel:UPLink[:MCHannel]
This setting is only applicable when
RBR Channel (UARFCN) State
is set to
On
.
When
RBR Uplink Channel
is set to
Auto
, the handover uplink UARFCN is automatically determined by the
RBR Downlink Channel (UARFCN)
setting. The test set subtracts the frequency separation associated with the handover downlink channel's band from the
RBR Downlink Channel (UARFCN)
setting, and instructs the UE to use this uplink channel after completion of the Radio Bearer Reconfiguration.
GPIB command: CALL:SETup:RBReconfig:CHANnel:UPLink:CONTrol:AUTO
This setting is only applicable when
RBR Channel (UARFCN) State
is set to
On
.
See Uplink Channel for more information.
When you set
RBR Downlink Channel (UARFCN)
to a value in Band VI, you must specify whether you want the test set to send a Band V or Band VI Frequency Band Indicator using the
RBR Band Arbitrator
setting. See
Band Arbitrator
for more information.
GPIB command: CALL:SETup:RBReconfig:CHANnel:BARBitrator
This setting determines the Uplink DTCH RMC CRC Presence state the UE is instructed to use after completion of the Radio Bearer Reconfiguration.
GPIB command: CALL:SETup:RBReconfig:DTCHannel:CRC[:PRESence]
This setting determines the UE Loopback Type the UE is instructed to use after completion of the Radio Bearer Reconfiguration.
GPIB command: CALL:SETup:RBReconfig:MS:LOOPback:TYPE
This setting determines the Uplink Dummy DCCH Data state the UE is instructed to use after completion of the Radio Bearer Reconfiguration.
GPIB command: CALL:SETup:RBReconfig:UPLink:DCCHannel:DDATa
This parameter selects whether the DPCH gain settings signalled to the UE during the Radio Bearer Reconfiguration are set manually (using the RBR Manual Uplink DPCH Bc and RBR Manual Uplink DPCH Bd settings) or automatically by the test set (using the RB Test Mode RBR RAB setting). Note that configuring Bc and Bd such that neither is set to 15 is undefined in the standards, and may result in unexpected behavior. See Uplink DPCH Bc/Bd Control for more information about how the test set automatically determines the gain settings.
GPIB command: CALL:SETup:RBReconfig:DPCHannel:BETA:AUTO
When
RBR Uplink DPCH Bc/Bd Control
is set to
Manual
, this parameter controls the uplink DPCCH gain setting (beta
c
) signalled to the UE during the Radio Bearer Reconfiguration. Range is 1 to 15 (see 3GPP TS 25.213 s4.2.1.1 Table 1 for a mapping of the signalled values to the resulting quantized amplitude ratios).
See Manual Uplink DPCH Bc for more information.
GPIB command: CALL:SETup:RBReconfig:DPCHannel:MANual:CBETa
When
RBR Uplink DPCH Bc/Bd Control
is set to
Manual
, this parameter controls the uplink DPDCH gain setting (beta
d
) signalled to the UE during the Radio Bearer Reconfiguration. See
Manual Uplink DPCH Bd
for more information.
GPIB command: CALL:SETup:RBReconfig:DPCHannel:MANual:DBETa
You can specify whether the UE should maintain or initialise its CFN counter when performing the Radio Bearer Reconfiguration. See RB setup Timing Indication (CFN Handling): for additional details. Note that 3GPP 25.331 v5.17.0 s8.6.6.28 states that the UE's behavior is undefined if the network sets the Timing Indication IE to Initialise on a non-hard handover (i.e. where the UARFCNs and one or more Primary Scrambling Codes remain unchanged as part of the reconfiguration).
RBR Timing Indication (CFN Handling)
is set to
Auto
, the Timing Indication information element sent in the RB Setup message (sent as part of the Radio Bearer Reconfiguration) is set to Initialise if
RBR Downlink Channel (UARFCN)
and
RBR Uplink Channel (UARFCN)
are set such that a hard handover will occur (UARFCNs will change) or if
RBR Default DPCH Offset (DOFF)
is set to a value other than the
Current DPCH Offset
(this latter condition is to maintain backwards-compatibility with earlier releases). Otherwise, the Timing Indication information element sent in the RB Setup message (sent as part of the Radio Bearer Reconfiguration) is set to Maintain.A timing-maintained Radio Bearer Reconfiguration cannot be performed when compressed mode is enabled.
GPIB command: CALL:HANDoff:RBReconfig:CFNHandling
When
RBR Timing Indication (CFN Handling)
is set to
Initialise
, the test set includes both the
Default DPCH Offset
and
DPCH Frame Offset
information elements in the RB Setup message sent as part of the Radio Bearer Reconfiguration. Both information elements are sent with a value equal to the
RBR Default DPCH Offset (DOFF)
setting. Note, however, that the resolution of the
Default DPCH Offset
information element is 512 chips and the resolution of the
DPCH Frame Offset
information element is 256 chips. Thus, if
RBR Default DPCH Offset (DOFF)
is set to 3 x 512 chips, for example, then
Default DPCH Offset
is sent with a value of 3 (x 512 chips) and
DPCH Frame Offset
is sent with a value of 6 (x 256 chips). Thus, the
RBR Default DPCH Offset (DOFF)
setting can be used to change the DPCH Frame Offset (tau
DPCH
) to 0, 1, ..., 75 x 512 chips (or 0, 2, 4, ..., 150 x 256 chips) while on a connection.
The Current DPCH Offset result indicates the DPCH Frame Offset currently in use by the test set (for the current operating mode).
Note, 3GPP TS 25.331 v5.17.0 s8.6.6.28 states that the timing re-initialized reconfiguration required to send the Default DPCH Offset IE must also include a change in UARFCN or Primary Scrambling Code, or the UE's behavior is undefined.
GPIB command: CALL:SETup:RBReconfig:DPCHannel:DOFFset
When
RBR Timing Indication (CFN Handling)
is set to
Maintain
, the test set sends only the
DPCH Frame Offset
information element in the RB Setup message sent as part of the Radio Bearer Reconfiguration. The value of the
DPCH Frame Offset
information element is determined by the
Current DPCH Offset
and the
RBR Relative DPCH Frame Offset
setting. The
RBR Relative DPCH Frame Offset
setting can be used to change the current DPCH Frame Offset (tau
DPCH
) by -256, 0 or +256 chips while on a connection.
The Current DPCH Offset result indicates the DPCH Frame Offset currently in use by the test set (for the current operating mode).
GPIB command: CALL:SETup:RBReconfig:DPCHannel:RFOFfset
SIB11 Inter-Freq Cell Info List
(see
Inter-frequency Cells
).This section is only applicable to the lab application.
You can connect two test sets using an External Device Connection to create a Two-Cell Test System for testing your UE's ability to transition between cells while in idle mode and while actively transferring data.
You must have an
External Device Connection
between the two test sets to perform the
Execute External 8960 Handover
immediate action. Also, your UE must have an active PDP context (or simply be attached if your test set is emulating a GSM/GPRS/EGPRS cell), or be actively transferring data (voice, PS data, HSDPA, etc.) before initiating the external 8960 handover.
When the
Execute External 8960 Handover
action is performed, the originating test set queries the configuration of the destination test set to determine what type of handover/cell reselection to order. Note that while strictly speaking, a handover is the process by which a mobile transitions from one cell to another while maintaining a circuit-switched call, the same
Execute External 8960 Handover
action is used both to initiate a handover and to perform a network-initiated cell reselection, depending upon the configuration of the two test sets and the UE's current connection state.
Note that the contents of the Handover command (circuit-switched connections) or Cell Change Order (packet-switched connections) sent by the originating test set during an external 8960 handover are not based on the information in its neighbor cell lists; it is strictly based on the configuration of the destination test set. However, it is recommended that you configure the SIB11 Cell Info List to contain the other test set's information. This enables the mobile to measure the other test set before transitioning to it (some mobiles will not perform a "blind" handover) and allows you to view the mobile's measurement reports for the test set.
See Two-Cell Test System for more information on the external 8960 handover.
When performing a circuit-switched handover, you can specify the following setting in the Handover from UTRAN message:
This parameter allows you to set the Activation Time that is signaled to the UE in the Handover from UTRAN message (see 3GPP TS 25.331 s10.3.3.1). Activation Time controls the frame number at which the operation caused by the related message shall take effect (in other words, how long the UE should wait before performing the handover). It can be set between 0 and 255, and indicates the absolute value of the CFN (Connection Frame Number) at which the UE should perform the handover. If set to 0, the Activation Time IE is not sent in the Handover from UTRAN message.
GPIB command: CALL:HANDoff:EXTernal:ATIMe
This parameter can only be changed when connection status is idle.
This section is only applicable to the lab application.
When a UE performs a Circuit Switched Fallback (CSFB), it is moved from E-UTRAN to WCDMA network for the CS services (the AMR voice call) using an LTE RRC Release message. When the AMR voice call is ended, a RRC release message will redirect the UE back to E-UTRAN.
Note that when simultaneous services {AMR voice call and PSD (packet switched data) }are activated, the AMR voice will not be released with a redirect to E-UTRAN. In this case, you need to terminates AMR call first before using the RRC release to perform the redirection, because the AMR service is terminated with a Radio Bearer Release instead of the RRC Release message.
You can use the test set as a WCDMA network simulator to test the RRC Release with Redirect capabilities of your UE, by setting up a connection between the test set and the Keysight E6621A PXT. See E-UTRAN / WCDMA Interworking on how to set up the connections.
For RRC Release with Redirect, you can specify the following parameters and actions:
Redirection IE Inclusion State
Specifies whether to include the `Redirect info' element when sending the RRC-Release message.
GPIB Command: CALL:HANDoff:RRC:CRELease:REDirect[:STATe]
E-UTRA EARFCN
Specifies the E-UTRA EARFCN to be used in the RRC-Release redirection information.
GPIB Command: CALL:HANDoff:RRC:CRELease:REDirect:EUTRa:EARFcn
E-UTRA Blacklisted Cell Inclusion State
Specifies whether to include the E-UTRA blacklisted cells list in the RRC-Release redirection information.
GPIB Command: CALL:HANDoff:RRC:CRELease:REDirect:EUTRa[:BLACklist]
E-UTRA Blacklisted Cell Physical Cell ID
Specifies the E-UTRA physical cell ID to be used in the RRC-Release redirection blacklist.
GPIB Command: CALL:HANDoff:RRC:CRELease:REDirect:EUTRa:BLACklist:CID