|
Sets/queries the PCR HSDPA MIMO Antenna 2 Pilot Configuration . |
|
| Same as setting | |
| PCPichannel | |
| Requirements | |
OUTPUT 714;"CALL:SETup:ANTenna2:PILot:CONFig PCPichannel" |
|
|
Sets/queries the Handover Band Arbitrator . This setting is only applicable when Handover Downlink Channel (UARFCN) is set to a channel in Band VI. |
|
| Same as setting | |
| Requirements |
Test Application Revision: A.09 and above Test Application Revision A.11, added [:PCReconfig] Lab Application Revision: C.04 and above |
OUTPUT 714;"CALL:SETup:CHANnel:BARBitrator BAND5" |
|
|
Sets/queries the Handover Downlink Channel (UARFCN) .
If the entered |
|
|
|
| Same as setting | |
| Requirements |
Test Application Revision: A.02 and above. Lab Application Revision: A.01 and above. Test Application Revision A.05.28, Lab Application Revision B.01.29, added 1037 - 1062. Test Application Revision A.08 and Lab Application Revision C.03, changed channel ranges to match 3GPP TS 25.101 v6.7.0 (previously, channels supported were: 412-687, 1037-1062, 4320-4495, 4600-4825, 9000-9425, 9625-9975, and 10,525-10,875, resolution = 1). Test Application Revision A.09 and Lab Application Revision C.04 and D.00, changed channel ranges to match 3GPP TS 25.101 v7.2.0 (previously channels supported were: 412, 437, 462, 487, 512, 537, 562, 587, 612, 637, 662, 687, 1007, 1012, 1032, 1037, 1062, 1087, 1462, 1487, 1512, 1537, 1562, 1587, 1612, 1637, 1662, 4357-4458 -- resolution = 1, 9037-9388 -- resolution = 1, 9662-9938 -- resolution = 1, and 10562-10838 -- resolution = 1). Test Application Revision A.10 and Lab Application Revision D.01, added 2237 - 2563, 2587, 2612, 2637, 2662, 2687, 2712, 2737, 2762, 2787, 2812, 2837, 2862, 2887, 2912 Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, added 3112 to 3388, 3412, 3437, 3462, 3487, 3512, 3537, 3562, 3587, 3612, 3637, 3662, 3687 Test Application Revision A.11 and Lab Application Revision D.02, added [:PCReconfig] Test Application Revision A.14 and Lab Application Revision F.00, added 3837 - 3903, 3927, 3932, 3957, 3962, 3987, 3992, 4017 - 4043, 4067, 4092, 4117 - 4143, 4167, 4192 Test Application Revision A.18.00 and Lab Application Revision H.00.00 and above, added 712 to 763, 787, 812, 837, 4512 to 4638 and 862 to 912 |
OUTPUT 714;"CALL:SETup:CHANnel:DOWNlink 10735" |
|
|
The setting form of this command performs two functions: (1) sets Handover Uplink Channel (UARFCN) to a specific UARFCN (see CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CHANnel ), and (2) sets handover uplink channel control to off (manual) (see CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO ). The query form of this command returns the handover uplink UARFCN that is used by the test set when CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO is set to off (manual). Note, when CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO is set to on (auto), the handover uplink UARFCN used by the test set is determined by CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:DOWNlink . The handover uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>UPLink[:CHANnel]? .
If the entered handover |
|
|
Range: see CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CHANnel |
|
| Same as setting | |
|
Handover uplink UARFCN = 9780, handover uplink channel control = on (auto) |
|
| Requirements |
Test Application Revision: A.02 and above. Lab Application Revision: A.01 and above. Test Application Revision A.05.28 and Lab Application Revision B.01.29, added 812 - 837. Test Application Revision A.08 and Lab Application Revision C.03, changed channel ranges to match 3GPP TS 25.101 v6.7.0 (previously, channels supported were: 12-287, 812-837, 4095-4270, 4375-4600, 8525-8950 and 9225-9925, resolution = 1). Test Application Revision A.09 and Lab Application Revision C.04 and D.00, changed channel ranges to match 3GPP TS 25.101 v7.2.0 (previously channels supported were: 12, 37, 62, 87, 112, 137, 162, 187, 212, 237, 262, 287, 782, 787, 807, 812, 837, 862, 1162, 1187, 1212, 1237, 1262, 1287, 1312, 1337, 1362, 4132-4233 -- resolution = 1, 8562-8913 -- resolution = 1, 9262-9538 -- resolution = 1, 9612-9888 -- resolution = 1). Test Application Revision A.10 and Lab Application Revision D.01, added 2012 - 2338, 2362, 2387, 2412, 2437, 2462, 2487, 2512, 2537, 2562, 2587, 2612, 2637, 2662, 2687 Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, added 2887 to 3163, 3187, 3212, 3237, 3262, 3287, 3312, 3337, 3362, 3387, 3412, 3437, 3462 Test Application Revision A.11 and Lab Application Revision D.02, added [:PCReconfig] Lab Application Revision: E.00.34 and above, added 3487 - 3587. |
OUTPUT 714;"CALL:SETup:CHANnel:UPLink 9785" ! Sets the handover uplink channel UARFCN to 9785 and selects manual control mode ! for handover uplink channel. |
|
|
The setting form of this command sets Handover Uplink Channel (UARFCN) to a specific UARFCN. Note, this handover uplink UARFCN is only used by the test set when CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO is set to off (manual). When CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO is set to on (auto), the handover uplink UARFCN used by the test set is determined by CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:DOWNlink . The query form of this command returns the handover uplink UARFCN that is used by the test set when CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO is set to off (manual). The handover uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>UPLink[:CHANnel]? .
If the entered handover |
|
|
|
| Same as setting | |
| 9780 | |
| Requirements |
Test Application Revision: A.06 and above Lab Application Revision: C.01 and above Test Application Revision A.08 and Lab Application Revision C.03, changed channel ranges to match 3GPP TS 25.101 v6.7.0 (previously, channels supported were: 12-287, 812-837, 4095-4270, 4375-4600, 8525-8950 and 9225-9925, resolution = 1). Test Application Revision A.09 and Lab Application Revision C.04 and D.00, changed channel ranges to match 3GPP TS 25.101 v7.2.0 (previously channels supported were: 12, 37, 62, 87, 112, 137, 162, 187, 212, 237, 262, 287, 782, 787, 807, 812, 837, 862, 1162, 1187, 1212, 1237, 1262, 1287, 1312, 1337, 1362, 4132-4233 -- resolution = 1, 8562-8913 -- resolution = 1, 9262-9538 -- resolution = 1, 9612-9888 -- resolution = 1). Test Application Revision A.10 and Lab Application Revision D.01, added 2012 - 2338, 2362, 2387, 2412, 2437, 2462, 2487, 2512, 2537, 2562, 2587, 2612, 2637, 2662, 2687 Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, added 2887 to 3163, 3187, 3212, 3237, 3262, 3287, 3312, 3337, 3362, 3387, 3412, 3437, 3462 Test Application Revision A.11 and Lab Application Revision D.02, added [:PCReconfig] Lab Application Revision: E.00.34 and above, added 3487 - 3587. Test Application Revision A.14 and Lab Application Revision F.00 and above, added 3612 - 3678, 3702, 3707, 3732, 3737, 3762, 3767, 3792 - 3818, 3842, 3867, 3892 - 3918, 3942, 3967 Test Application Revision: A.18.00 and Lab Application Revision H.00.00 and above, added 312 to 363, 387, 412, 437, 4287 to 4413 and 462 to 512 |
OUTPUT 714;"CALL:SETup:CHANnel:UPLink:CHANnel 9785" ! Sets the handover uplink channel UARFCN to 9785. |
|
|
Sets/queries the Handover Uplink Channel (UARFCN) control mode.
The handover uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>UPLink[:CHANnel]? . |
|
| Range: 1|0 | |
| Requirements |
Test Application Revision: A.06 and above Test Application Revision A.11, added [:PCReconfig] |
OUTPUT 714;"CALL:SETup:CHANnel:UPLink:CONTrol:AUTO OFF" ! Sets handover uplink control mode to manual. |
|
|
Sets/queries the Handover Dual Carrier Band Configuration . |
|
| Range: SBANd|DBANd|UDEFined | |
| Requirements | |
OUTPUT 714;"CALL:SETup:PCReconfig:HSDPa:MCARrier:BAND:CONFig:TYPE DBANd" ! Sets the Nth Serving Cell's UARFCN to be used as dual band during Physical Channel Reconfiguration procedure. |
|
|
Sets/queries the PCR MCC (Mobile Country Code) . |
|
| Same with setting | |
| Requirements |
Test Application Revision A.20.00 and above, with the required feature license |
OUTPUT 714;"CALL:SETup:PCReconfig:MCCode 9" ! Sets the PCR Mobile Country Code to 9. |
|
|
Sets/queries PCR N_cqi_typeA/M_cqi ratio . |
|
| Range: R1To2|R2To3|R3To4|R4To5|R5To6|R6To7|R7To8|R8To9|R9To10|R1To1 | |
| Same as setting | |
| Requirements | |
OUTPUT 714;"CALL:SETup:MIMO:NMRatio R6To7" ! Sets the N_cqi_typeA/M_cqi ratio on the UL HS-DPCCH to 6/7, which is signalled to the UE during Physical Channel Reconfiguration procedure. |
|
|
Sets/queries Handover MNC (Mobile Network Code) . |
|
| Same as setting | |
| Requirements |
Test Application Revision A.20.00 and above, with the required feature license |
OUTPUT 714;"CALL:SETup:MNCode 5" ! Sets PCR Mobile Network Code to 5. |
|
|
Sets/queries Handover MNC (Mobile Network Code) Length . |
|
| Same as setting | |
| Requirements |
Test Application Revision A.20.00 and above, with the required feature license |
OUTPUT 714;"CALL:SETup:MNCode:LENGth Digits3" ! Transmits PCR Mobile Network Code using 3 digits, prepending one or two zeros if necessary. |
|
|
Sets/queries the Handover Secondary Cell DL Adjacent UARFCN . |
|
| Requirements |
Test Application Revision: A.19.00 and above, with the required feature license |
OUTPUT 714;"CALL:SETup:SSCell:CHANnel:ADJacent HIGHer" ! Sets the DC-HSDPA secondary cell handover DL UARFCN to be adjacent higher than the serving cell. |
|
|
Sets/queries the Handover Secondary Cell DL Channel Config . |
|
| ADJacent | |
| Requirements | |
OUTPUT 714;"CALL:SETup:SSCell:CHANnel:CONFig:TYPE MANual" ! Sets the DC-HSDPA secondary serving cell DL UARFCN mode to manual for the Physical Channel Reconfiguration. |
|
|
Sets/queries the Handover Secondary Cell DL Manual UARFCN . |
|
|
Range:
|
|
| 3012 | |
| Requirements | |
OUTPUT 714;"CALL:SETup:SSCell:CHANnel:MANual:UARFcn 3012" ! Sets the destination DL UARFCN of the secondary serving cell for PCR to 3012. |
|
|
Sets/queries the Handover Secondary Cell Manual Band Arbitrator . |
|
| BAND6 | |
| Requirements | |
OUTPUT 714;"CALL:SETup:SSCell:CHANnel:MANual:BARBitrator BAND6" ! Sets the DC-HSDPA secondary serving cell's band arbitrator for PCR to Band VI. |
|
|
THIS COMMAND IS OBSOLETE. The
Sets/queries
When
CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO
is set to on (auto), the handoff uplink UARFCN used by the test set is determined by this
If
CALL:SETup[:PCReconfig]:CHANnel<[:SELected]|:FDD>:UPLink:CONTrol:AUTO
is set to on (auto) and you attempt to set |
|
| Same as setting | |
| MHZ190 | |
| Requirements |
Test Application Revision: A.06 and above Test Application Revision A.08 and Lab Application Revision C.03, added VMHZ45 |
OUTPUT 714;"CALL:SETup:CHANnel:UPLink:SEParation MHZ80" |
|
|
Sets/queries Handover UL CL Power Ctrl Algorithm . |
|
| Same as setting | |
| *RST setting | ALG2 |
OUTPUT 714;"CALL:SETup:CLPControl:UPLink:ALGorithm ALG1" ! Sets Handover UL CL Power Ctrl Algorithm to One. |
|
|
Sets/queries Handover UL CL Power Ctrl Step Size .
This setting can only be changed when
CALL:SETup:CLPControl:UPLink:ALGorithm
is set to |
|
| Same as setting | |
| *RST setting | 1 dB |
OUTPUT 714;"CALL:SETup:CLPControl:UPLink:STEPsize 2" ! Sets Handover UL CL Power Ctrl Step Size to 2 dB. |
|
|
Sets/queries the RBR Band Arbitrator . This setting is only applicable when RBR Downlink Channel (UARFCN) is set to a channel in Band VI.
This setting is only applicable when
RBR Channel (UARFCN) State
is set to |
|
| Same as setting | |
| Requirements | |
OUTPUT 714;"CALL:SETup:RBReconfig:CHANnel:BARBitrator BAND6" |
|
|
Sets/queries the RBR Downlink Channel (UARFCN) .
This setting is only applicable when
RBR Channel (UARFCN) State
is set to
If the entered |
|
|
|
| Same as setting | |
| Requirements |
Test Application Revision A.11 and above. Lab Application Revision D.02 and above. Test Application Revision A.14 and Lab Application Revision F.00, added 3837 - 3903, 3927, 3932, 3957, 3962, 3987, 3992, 4017 - 4043, 4067, 4092, 4117 - 4143, 4167, 4192 Test Application Revision A.18.00 and Lab Application Revision H.00.00 and above, added 712 to 763, 787, 812, 837, 4512 to 4638 and 862 to 912 |
OUTPUT 714;"CALL:SETup:RBReconfig:CHANnel:DOWNlink 10730" |
|
|
The setting form of this command performs two functions: (1) sets RBR Uplink Channel (UARFCN) to a specific UARFCN (see CALL:SETup:RBReconfig:CHANnel:UPLink:CHANnel ), and (2) sets RBR uplink channel control to off (manual) (see CALL:SETup:RBReconfig:CHANnel:UPLink:CONTrol:AUTO ). The query form of this command returns the RBR uplink UARFCN that is used by the test set when CALL:SETup:RBReconfig:CHANnel:UPLink:CONTrol:AUTO is set to off (manual). Note, when CALL:SETup:RBReconfig:CHANnel:UPLink:CONTrol:AUTO is set to on (auto), the RBR uplink UARFCN used by the test set is determined by CALL:SETup:RBReconfig:CHANnel:DOWNlink .
This setting is only applicable when
RBR Channel (UARFCN) State
is set to The RBR uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup:RBReconfig:CHANnel:UPLink[:CHANnel]? .
If the entered |
|
|
Range: see CALL:SETup:RBReconfig:CHANnel:UPLink:CHANnel |
|
| Same as setting | |
|
RBR uplink UARFCN = 9780, RBR uplink channel control = on (auto) |
|
| Requirements | |
OUTPUT 714;"CALL:SETup:RBReconfig:CHANnel:UPLink 9780" ! Sets the RBR uplink channel UARFCN to 9780 and selects manual control mode ! for RBR uplink channel. |
|
|
The setting form of this command sets RBR Uplink Channel (UARFCN) to a specific UARFCN.
This setting is only applicable when
RBR Channel (UARFCN) State
is set to Note, this RBR uplink UARFCN is only used by the test set when CALL:SETup:RBReconfig:CHANnel:UPLink:CONTrol:AUTO is set to off (manual). When CALL:SETup:RBReconfig:CHANnel:UPLink:CONTrol:AUTO is set to on (auto), the RBR uplink UARFCN used by the test set is determined by CALL:SETup:RBReconfig:CHANnel:DOWNlink . The query form of this command returns the RBR uplink UARFCN that is used by the test set when CALL:SETup:RBReconfig:CHANnel:UPLink:CONTrol:AUTO is set to off (manual). The RBR uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup:RBReconfig:CHANnel:UPLink[:CHANnel]? .
If the entered |
|
|
|
| Same as setting | |
| 9780 | |
| Requirements |
Test Application Revision A.11 and above. Lab Application Revision D.02 and above. Lab Application Revision: E.00.34 and above, added 3487 - 3587. Test Application Revision A.14 and Lab Application Revision F.00 and above, added 3612 - 3678, 3702, 3707, 3732, 3737, 3762, 3767, 3792 - 3818, 3842, 3867, 3892 - 3918, 3942, 3967 Test Application Revision: A.18.00 and Lab Application Revision H.00.00 and above, added 312 to 363, 387, 412, 437, 4287 to 4413 and 462 to 512 |
OUTPUT 714;"CALL:SETup:RBReconfig:CHANnel:UPLink:CHANnel 9780" ! Sets the RBR uplink channel UARFCN to 9780. |
|
|
Sets/queries the RBR Uplink Channel (UARFCN) control mode.
This setting is only applicable when
RBR Channel (UARFCN) State
is set to
The RBR uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup:RBReconfig:CHANnel:UPLink[:CHANnel]? . |
|
| Range: 1|0 | |
| Requirements | |
OUTPUT 714;"CALL:SETup:RBReconfig:CHANnel:UPLink:CONTrol:AUTO ON" ! Sets RBR uplink control mode to auto. |
|
|
Sets/queries RBR Uplink DPCH Bc/Bd Control . |
|
| *RST setting | 1 (auto) |
OUTPUT 714;"CALL:SETup:RBReconfig:DPCHannel:BETA:AUTO OFF" ! Sets RBR Uplink DPCH Bc/Bd Control to Manual. |
|
|
Sets/queries RBR Default DPCH Offset (DOFF) . This command is only applicable when CALL:HANDoff:RBReconfig:CFNHandling is set to INITialise. |
|
| Same as setting | |
| 0 (0 x 512 chips) | |
|
Test Application Revision: A.09 and above. |
|
OUTPUT 714;"CALL:SETup:RBReconfig:DPCHannel:DOFFset 3" ! Sets RBR Default DPCH Offset (DOFF) to 3 x 512 chips. |
|
|
Sets/queries RBR Manual Uplink DPCH Bc . This command is only applicable when CALL:SETup:RBReconfig:DPCHannel:BETA:AUTO is set to OFF (Manual). |
|
| Same as setting | |
| *RST setting | 8 |
|
Test Application Revision: A.09 and above. Lab Application Revision: C.04 or D.00.04 and above. Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, range is 1 to 15 (vs. 2 to 15) |
|
OUTPUT 714;"CALL:SETup:RBReconfig:DPCHannel:MANual:CBETa 10" ! Sets RBR Manual Uplink DPCH Bc to 10. |
|
|
Sets/queries RBR Manual Uplink DPCH Bd . This command is only applicable when CALL:SETup:RBReconfig:DPCHannel:BETA:AUTO is set to OFF (Manual). |
|
| Same as setting | |
| *RST setting | 15 |
OUTPUT 714;"CALL:SETup:RBReconfig:DPCHannel:MANual:DBETa 10" ! Sets RBR Manual Uplink DPCH Bd to 10. |
|
|
Sets/queries RBR Relative DPCH Frame Offset . This command is only applicable when CALL:HANDoff:RBReconfig:CFNHandling is set to MAINtain. |
|
| Same as setting | |
| 0 chips | |
OUTPUT 714;"CALL:SETup:RBReconfig:DPCHannel:RFOFfset -256" ! Sets RBR Relative DPCH Frame Offset to -256 chips. |
|
|
This command sets/queries the RBR Uplink DTCH RMC CRC Presence . |
|
| Range: PRES|DAT | |
| *RST Setting | PRES |
| Requirements | |
OUTPUT 714;"CALL:SETup:RBReconfig:DTCHannel:CRC DATa" ! Sets RBR Uplink DTCH RMC CRC Presence to Used for Data. |
|
|
Sets/queries the RBR UE Loopback Type . |
|
| Same as setting. | |
| TYPE1 | |
OUTPUT 714;"CALL:SETup:RBReconfig:MS:LOOPback:TYPE TYPE2" ! Sets RBR UE Loopback Type to Type 2. |
|
|
This command sets/queries the RB Test Mode RBR RAB . |
|
| Same as setting | |
| *RST Setting | RMC12 |
| Requirements | |
OUTPUT 714;"CALL:SETup:RBReconfig:RBTest:RAB RMC64" ! Sets RB Test Mode RBR RAB to 64k RMC. |
|
|
Sets/queries the RBR Uplink Dummy DCCH Data state. |
|
| *RST setting | 0 (off) |
OUTPUT 714;"CALL:SETup:RBReconfig:UPLink:DCCHannel:DDATa OFF" ! Sets RBR Uplink Dummy DCCH Data to Off |
|
|
THIS COMMAND IS OBSOLETE. Please use the CALL:HANDoff:SYSTem[:GSM][:IMMediate] command to perform a system handoff. Sets/queries the system type that the mobile station will be handed off to when the CALL:HANDoff command is used. The intersystem handoff can be performed only from W-CDMA to GSM. This setting cannot be changed to GSM while the E1968A test applications (TA) are not present in the test set and licensed for operation. Attempting to change this setting while the E1968A TA is not available will result in an error message to alert you this condition. |
|
| FDD | |
| Requirements | |
OUTPUT 714;"CALL:SETup:SYSTem GSM" !Selects GSM as the handoff system type. |
|
|
Sets/queries RB Test Mode to GSM Handover Alerting State . |
|
| 1|0 | |
| 1 (On) | |
| Requirements | |
OUTPUT 714;"CALL:SETup:SYSTem:GSM:ALERting OFF" ! Sets RB Test Mode to GSM Alerting State to Off (the UE will not ring). |
|
|
Sets/queries the TCR HSDPA MIMO Antenna 2 Pilot Configuration . |
|
| Same as setting | |
| PCPichannel | |
| Requirements | |
OUTPUT 714;"CALL:SETup:TCReconfig:ANTenna2:PILot:CONFig SCPichannel" ! Sets the pilot channel the UE uses for the antenna 2 to SCPichannel, which is signalled to the UE during Transport Channel Reconfiguration procedure. |
|
|
Sets/queries the TCR Band Arbitrator . This setting is only applicable when TCR Downlink Channel (UARFCN) is set to a channel in Band VI.
This setting is only applicable when
TCR Channel (UARFCN) State
is set to |
|
| Same as setting | |
| Requirements | |
OUTPUT 714;"CALL:SETup:TCReconfig:CHANnel:BARBitrator BAND6" |
|
|
Sets/queries the TCR Downlink Channel (UARFCN) .
This setting is only applicable when
TCR Channel (UARFCN) State
is set to
If the entered |
|
|
|
| Same as setting | |
| Requirements |
Test Application Revision A.11 and above. Lab Application Revision D.02 and above. Test Application Revision A.14 and Lab Application Revision F.00, added 3837 - 3903, 3927, 3932, 3957, 3962, 3987, 3992, 4017 - 4043, 4067, 4092, 4117 - 4143, 4167, 4192 Test Application Revision A.18.00 and Lab Application Revision H.00.00 and above, added 712 to 763, 787, 812, 837, 4512 to 4638 and 862 to 912 |
OUTPUT 714;"CALL:SETup:TCReconfig:CHANnel:DOWNlink 10730" |
|
|
The setting form of this command performs two functions: (1) sets TCR Uplink Channel (UARFCN) to a specific UARFCN (see CALL:SETup:TCReconfig:CHANnel:UPLink:CHANnel ), and (2) sets TCR uplink channel control to off (manual) (see CALL:SETup:TCReconfig:CHANnel:UPLink:CONTrol:AUTO ). The query form of this command returns the TCR uplink UARFCN that is used by the test set when CALL:SETup:TCReconfig:CHANnel:UPLink:CONTrol:AUTO is set to off (manual). Note, when CALL:SETup:TCReconfig:CHANnel:UPLink:CONTrol:AUTO is set to on (auto), the TCR uplink UARFCN used by the test set is determined by CALL:SETup:TCReconfig:CHANnel:DOWNlink .
This setting is only applicable when
TCR Channel (UARFCN) State
is set to The TCR uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup:TCReconfig:CHANnel:UPLink[:CHANnel]? .
If the entered |
|
|
Range: see CALL:SETup:TCReconfig:CHANnel:UPLink:CHANnel |
|
| Same as setting | |
|
TCR uplink UARFCN = 9780, TCR uplink channel control = on (auto) |
|
| Requirements | |
OUTPUT 714;"CALL:SETup:TCReconfig:CHANnel:UPLink 9780" ! Sets the TCR uplink channel UARFCN to 9780 and selects manual control mode ! for TCR uplink channel. |
|
|
The setting form of this command sets TCR Uplink Channel (UARFCN) to a specific UARFCN.
This setting is only applicable when
TCR Channel (UARFCN) State
is set to Note, this TCR uplink UARFCN is only used by the test set when CALL:SETup:TCReconfig:CHANnel:UPLink:CONTrol:AUTO is set to off (manual). When CALL:SETup:TCReconfig:CHANnel:UPLink:CONTrol:AUTO is set to on (auto), the TCR uplink UARFCN used by the test set is determined by CALL:SETup:TCReconfig:CHANnel:DOWNlink . The query form of this command returns the TCR uplink UARFCN that is used by the test set when CALL:SETup:TCReconfig:CHANnel:UPLink:CONTrol:AUTO is set to off (manual). The TCR uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup:TCReconfig:CHANnel:UPLink[:CHANnel]? .
If the entered |
|
|
|
| Same as setting | |
| 9780 | |
| Requirements |
Test Application Revision A.11 and above. Lab Application Revision D.02 and above. Lab Application Revision: E.00.34 and above, added 3487 - 3587. Test Application Revision A.14 and Lab Application Revision F.00 and above, added 3612 - 3678, 3702, 3707, 3732, 3737, 3762, 3767, 3792 - 3818, 3842, 3867, 3892 - 3918, 3942, 3967 Test Application Revision: A.18.00 and Lab Application Revision H.00.00 and above, added 312 to 363, 387, 412, 437, 4287 to 4413 and 462 to 512 |
OUTPUT 714;"CALL:SETup:TCReconfig:CHANnel:UPLink:CHANnel 9780" ! Sets the TCR uplink channel UARFCN to 9780. |
|
|
Sets/queries the TCR Uplink Channel (UARFCN) control mode.
This setting is only applicable when
TCR Channel (UARFCN) State
is set to
The TCR uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:SETup:TCReconfig:CHANnel:UPLink[:CHANnel]? . |
|
| Range: 1|0 | |
| Requirements | |
OUTPUT 714;"CALL:SETup:TCReconfig:CHANnel:UPLink:CONTrol:AUTO ON" ! Sets TCR uplink control mode to auto. |
|
|
Sets/queries TCR DPCH Bc/Bd Control . |
|
| 1|0 | |
| 1 (auto) | |
| Requirements |
Test Application Revision: A.09 and above |
OUTPUT 714;"CALL:SETup:TCReconfig:DPCHannel:BETA:AUTO OFF" ! Sets TCR DPCH Bc/Bd Control to Manual. |
|
|
Sets/queries TCR Default DPCH Offset (DOFF) . This command is only applicable when CALL:HANDoff:TCReconfig:CFNHandling is set to INITialise. |
|
| Same as setting | |
| 0 (0 x 512 chips) | |
|
Test Application Revision: A.09 and above |
|
OUTPUT 714;"CALL:SETup:TCReconfig:DPCHannel:DOFFset 3" ! Sets TCR Default DPCH Offset (DOFF) to 3 x 512 chips. |
|
|
Sets/queries TCR Manual Uplink DPCH Bc . This command is only applicable when CALL:SETup:TCReconfig:DPCHannel:BETA:AUTO is set to MANual. |
|
| Same as setting | |
| 8 | |
| Requirements |
Test Application Revision: A.09 and above Lab Application Revision: C.04 and above Lab Application Revision: D.00, range is 1 to 15 (but 1 is not recommended) Lab Application Revision D.01, range is 2 to 15 Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, range is 1 to 15 (vs. 2 to 15) |
OUTPUT 714;"CALL:SETup:TCReconfig:DPCHannel:MANual:CBETa 15" ! Sets TCR Manual Uplink DPCH Bc to 15. |
|
|
Sets/queries TCR Manual Uplink DPCH Bd . This command is only applicable when CALL:SETup:TCReconfig:DPCHannel:BETA:AUTO is set to MANual. |
|
| Same as setting | |
| 15 | |
| Requirements |
Test Application Revision: A.09 and above |
OUTPUT 714;"CALL:SETup:TCReconfig:DPCHannel:MANual:DBETa 8" ! Sets TCR Manual Uplink DPCH Bd to 8. |
|
|
Sets/queries TCR Relative DPCH Frame Offset . This command is only applicable when CALL:HANDoff:TCReconfig:CFNHandling is set to MAINtain. |
|
| Same as setting | |
| 0 chips | |
|
Test Application Revision: A.09 and above |
|
OUTPUT 714;"CALL:SETup:TCReconfig:DPCHannel:RFOFfset -256" ! Sets TCR Relative DPCH Frame Offset to -256 chips. |
|
|
Sets/queries the TCR 16QAM State . |
|
| Range: 1|0 | |
OUTPUT 714;"CALL:SETup:TCReconfig:EDCHannel:QAM16 1" ! Sets the 16QAM State to On. |
|
|
Sets/queries the TCR E-DPCCH/DPCCH Power Offset . |
|
| Same as setting. | |
|
Test Application Revision: A.12 and above, with the required feature license |
|
OUTPUT 714;"CALL:SETup:TCReconfig:EDPCchannel:POFFset 0" ! Sets the TCR E-DPCCH/DPCCH Power Offset to 0. |
|
|
Sets/queries the TCR Reference E-TFCI Power Offsets . |
|
|
Range: DEF3410801|DEF3410802|DEF3412101|DEF3412102|DEF3412103|DEF3412104 |
|
| Same as setting. | |
|
Test Application Revision: A.12 and above, with the required feature license Lab Application Revision: E.00.16 and above Test Application Revision: A.17 and above: Added DEF3412103 and DEF3412104 Lab Application Revision: G.01.00 and above: Added DEF3412103 and DEF3412104 |
|
OUTPUT 714;"CALL:SETup:TCReconfig:ETFCi:POFFsets:REFerence DEF3410802" ! Sets the TCR Reference E-TFCI Power Offsets to Def 34108-02. |
|
|
Sets/queries TCR Number of HARQ Processes . |
|
| Same as setting | |
| 2 | |
OUTPUT 714;"CALL:SETup:TCReconfig:HARQ:PROCess:COUNt 1" ! Sets TCR Number of HARQ Processes to 1. |
|
|
Sets/queries TCR Number of HARQ Processes for MIMO . |
|
| Same as setting | |
| 12 | |
OUTPUT 714;"CALL:SETup:TCReconfig:MIMO:HARQ:PROCess:COUNt 16" ! Sets the Number of HARQ Processes that are active in the MAC-ehs layer for MIMO to 16, which is signalled to the UE during Transport Channel Reconfiguration procedure. |
|
|
Sets/queries TCR N_cqi_typeA/M_cqi Ratio . |
|
|
Range: R1To2|R2To3|R3To4|R4To5|R5To6|R6To7|R7To8|R8To9|R9To10|R1To1 |
|
| Same as setting | |
| R1To1 | |
OUTPUT 714;"CALL:SETup:TCReconfig:MIMO:NMRatio R4To5" ! Sets N_cqi_typeA/M_cqi ratio on the UL HS-DPCCH to 4/5, which is signalled to the UE during Transport Channel Reconfiguration procedure. |
|
|
Sets/queries the
TCR Measurement Power Offset
.
This parameter can only be set either while the call status is This setting only applies when "CALL:SETup:TCReconfig:MPOWer:OFFSet:CONTrol:AUTO" on page 498 is set to OFF (manual). |
|
| -6 dB | |
OUTPUT 714;"CALL:SETup:TCReconfig:MPOWer -6" ! Sets the TCR Measurement Power Offset to -6 dB. |
|
|
Sets/queries the automatic control state for the
TCR Measurement Power Offset
parameter. OFF = manual (see "CALL:SETup:TCReconfig:MIMO:HARQ:PROCess:COUNt" on page 497 or "CALL:SETup:TCReconfig:MPOWer:OFFSet:MANual" on page 500 )
This parameter can only be set either while the call status is |
|
| 0 (off) | |
OUTPUT 714;"CALL:SETup:TCReconfig:MPOWer:OFFSet:CONTrol:AUTO 0" ! Sets the TCR Measurement Power Offset control state to manual. |
|
|
Sets/queries the
TCR Measurement Power Offset
.
This parameter can only be set either while the call status is This setting only applies when "CALL:SETup:TCReconfig:MPOWer:OFFSet:CONTrol:AUTO" on page 498 is set to OFF (manual). |
|
| -6 dB | |
OUTPUT 714;"CALL:SETup:TCReconfig:MPOWer:OFFSet:MANual -6" ! Sets the TCR Measurement Offset Power to -6 dB. |
|
|
Sets/queries TCR UE IR Buffer Allocation . |
|
| Same as setting | |
| IMPL | |
OUTPUT 714;"CALL:SETup:TCReconfig:MS:IREDundancy:BUFFer:ALLocation EXPLicit" ! Sets TCR UE IR Buffer Allocation to Explicit. |
|
|
Sets/queries TCR Explicit UE IR Buffer Size . This setting is only applicable when CALL:SETup:TCReconfig:MS:IREDundancy:BUFFer:ALLocation is set to EXPLicit. |
|
|
Range: 800, 1600, 2400, 3200, 4000, 4800, 5600, 6400, 7200, 8000, 8800, 9600, 10400, 11200, 12000, 12800, 13600, 14400, 15200, 16000, 17600, 19200, 20800, 22400, 24000, 25600, 27200, 28800, 30400, 32000, 36000, 40000, 44000, 48000, 52000, 56000, 60000, 64000, 68000, 72000, 76000, 80000, 88000, 96000, 104000, 112000, 120000, 128000, 136000, 144000, 152000, 160000, 176000, 192000, 208000, 224000, 240000, 256000, 272000, 288000, 304000 |
|
| Same as setting | |
| 19200 | |
OUTPUT 714;"CALL:SETup:TCReconfig:MS:IREDundancy:BUFFer:SIZe 9600" ! Sets TCR Explicit UE IR Buffer Size to 9600. |
|
|
Sets/queries the RB Test Mode TCR RAB . |
|
| Same as setting | |
| RMC12 | |
| Requirements | |
OUTPUT 714;"CALL:SETup:TCReconfig:RBTest:RAB RMC64" ! Sets the handover RB test mode RAB to 64k RMC. |
|
|
Sets/queries the TCR Absolute Grant (16QAM) . |
|
|
Range: ZGRant|INDex0|INDex1|INDex2|INDex3...|INDex37|INDex38 |
|
| Same as setting. | |
|
Test Application Revision: A.17.00 and above |
|
OUTPUT 714;"CALL:SETup:TCReconfig:SGRant:ABSolute:QAM16 INDex36" ! Sets the TCR Absolute Grant 16QAM to 37:4(377/15)^2. |
|
|
Sets/queries the TCR Absolute Grant . |
|
| Same as setting. | |
|
Test Application Revision: A.12 and above, with the required feature license |
|
OUTPUT 714;"CALL:SETup:TCReconfig:SGRant:ABSolute INDex37" ! Sets the TCR Absolute Grant to 37:6(168)^2. |
|
| Sets/queries TCR Ack-Nack Repetition Factor . | |
| Same as setting | |
| 1 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:SETup:TCReconfig:UPLink:ANACk:RFACtor 3" ! Sets TCR Ack-Nack Repetition Factor to 3. |
|
Sets/queries
TCR CQI Feedback Cycle (k)
.
TCR CQI Feedback Cycle (k)
must be greater than or equal to
TCR CQI Repetition Factor
* 2ms (except for the case when
TCR CQI Feedback Cycle (k)
equals 0 ms). See
CALL:SETup:TCReconfig:UPLink:CQI:RFACtor
. |
|
| Same as setting | |
| 0.002 seconds (2 ms) | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:SETup:TCReconfig:UPLink:CQI:FCYCle 4MS" ! Sets TCR CQI Feedback Cycle (k) to 4 ms. |
|
Sets/queries
TCR CQI Repetition Factor
.
TCR CQI Feedback Cycle (k)
must be greater than or equal to
TCR CQI Repetition Factor
* 2ms (except for the case when
TCR CQI Feedback Cycle (k)
equals 0 ms). See
CALL:SETup:TCReconfig:UPLink:CQI:FCYCle
. |
|
| Same as setting | |
| 1 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:SETup:TCReconfig:UPLink:CQI:RFACtor 2" ! Sets TCR CQI Repetition Factor to 2. |
|
| Sets/queries TCR DeltaACK . | |
| Same as setting | |
| 3 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:SETup:TCReconfig:UPLink:DACK 8" ! Sets TCR DeltaACK to 8. |
|
| Sets/queries TCR DeltaCQI . | |
| Same as setting | |
| 5 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:SETup:TCReconfig:UPLink:DCQI 7" ! Sets TCR DeltaCQI to 7. |
|
| Sets/queries TCR DeltaNACK . | |
| Same as setting | |
| 3 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"CALL:SETup:TCReconfig:UPLink:DNACk 8" ! Sets TCR DeltaNACK to 8. |
|