This section is only applicable to the lab application.
Manual Operation: You can access the following menu from the
CALL SETUP
hardkey, go to the left side
Handovers (
F5
)
, then navigate to the
PS/SRVCC Handover 2 of 2
(
F2
).
For PS/SRVCC handover, the parameters and actions available to you include:
Setup Inbound
This action puts the test set into a "handover" state. The test set sets up dedicated resources and prepares for the UE's handover from another RAT. The dedicated channels are setup according to the general system settings, and as per the information queried via the external EPC. The type of resources (PS, CS or both) setup depends on the values of SRVCC State and PS State
During the "handover" state, the content of the HANDOVER TO UTRAN COMMAND message (ACSII hex string) can be queried by CALL:HANDoff:PSSRvcc:INBound:HOCommand? (GPIB command only).
The test set remains in the "handover" state until an Abort Inbound or preset occurs, or a successful handover.
GPIB Command: CALL:HANDoff:PSSRvcc:INBound[:IMMediate]
SRVCC State
This setting enables or disables SRVCC handover as part of an inbound PS/SRVCC handover.
GPIB Command: CALL:HANDoff:PSSRvcc:INBound:SRVCc:STATe
SRVCC EPS Bearer ID
This setting specifies the EPS Bearer ID which carries the IMS voice traffic on LTE.
GPIB Command: CALL:HANDoff:PSSRvcc:INBound:SRVCc:EBID
RTP Payload Type
This setting controls the payload type being used in the RTP IMS audio stream.
GPIB Command: CALL:HANDoff:PSSRvcc:INBound:SRVCc:RPT:AUTO CALL:HANDoff:PSSRvcc:INBound:SRVCc:RPT:MVALue . CALL:HANDoff:PSSRvcc:INBound:SRVCc:RPT:VALue
PS State
This setting enables or disables PS handover as part of an inbound PS/SRVCC handover.
GPIB Command: CALL:HANDoff:PSSRvcc:INBound:PS:STATe
PS EPS Bearer ID
This setting determines the EPS Bearer ID on LTE for PS handover.
GPIB Command: CALL:HANDoff:PSSRvcc:INBound:PS:EBID
Security
This setting controls the inbound handover security type. Three inbound handover security types are supported:
Renegotiate
, an unciphered handover is initiated and recalculation of AUTN procedure is performed.
Integrity
, an unciphered handover is initiated, and the IK is derived from the security information provided by the EPC to continue the security keys negotiated on LTE. The authentication procedure begins with the SecurityModeCommand, that is, omitting issuing the AUTN messaging.
Ciphered
, it functions like setting as Integrity except that it generates a handover message with the ciphering information present.GPIB Command: CALL:HANDoff:PSSRvcc:INBound:SECurity
This immediate action aborts the pending inbound PS/SRVCC handover event.
GPIB Command: CALL:HANDoff:PSSRvcc:INBound:ABORt
Activation Time
This parameter specifies the time delay (in frames) from issuing the outbound handover command to the handover actually taking effect. If this value is set to
0
, the outbound PS handover takes effect immediately.
GPIB Command: CALL:HANDoff:PS:OUTBound:ATIMe
Execute Handover
Issues the HANDOVER FROM UTRAN COMMAND command to the UE. You must use the CALL:HANDoff:PS:OUTBound:TMessage command to set up the HANDOVER FROM UTRAN COMMAND message before attempting to execute the handover (This is a GPIB command only).
GPIB Command: CALL:HANDoff:PS:OUTBound[:IMMediate]
You can use the test set as a WCDMA network simulator to test the WCDMA/LTE Packet Switched (PS) handover capabilities of your UE, by setting up a connection between the test set and the Keysight E6621A PXT. See E-UTRAN / WCDMA Interworking on how to set up the connections.
See SIB19 Information on how to set up the inter-RAT frequency and priority information.
PS Handovers requires the target cell to setup dedicated resources for an incoming UE. The source cell queries the target cell for the resources, and then communicate them to the UE to access the target cell. This bypasses the RRC connection setup procedure, thus minimizing the data flow interruptions.The test set supports two types of PS handover:
IMS is the 3GPP voice over IP solution which is being deployed in the LTE networks as the voice solution. When a UE is camped on the LTE network, it would need to fallback to the legacy 2G/3G networks when coverage or capacity dictates. SRVCC provides the solution for the UE to transfer the voice call from IMS/IP to standard CS domain. As defined in 3GPP TS 23.216 V8.8.0 "SRVCC (Single Radio Voice Call Continuity) refers to the voice call continuity between IMS over PS access and CS access for calls that are anchored in IMS when the UE is capable of transmitting/receiving on only one of those access networks at a given time."
With the support of the Keysight PXT (E6621A) as the LTE BSE emulator, the test set can be used to test the UE SRVCC implementation.
Operating Mode
is
Active Cell
. The setting will be ignored in other operating modes.The following table shows the result of attempting to perform SRVCC Handover in each of the possible UE states.
| State | Inbound SRVCC Handover Setup |
|---|---|
| Idle | OK |
| Attached | OK |
| PDP Active | OK |
| Transferring | Error |
| Connected | Error |
| Connected/Attached | Error |
| Connected/Suspended | Error |
| Connected/PDP Active | Error |
| Connected/Transferring | Error |
| Handover | Error |
The general network procedure for SRVCC from E-UTRAN to UTRAN is as follows:
The UE sends measurement reports to E-UTRAN.
The E-UTRAN (based on measurement reports or some triggers) decides to initiate an SRVCC handover to UTRAN and sends the Handover Required message to the MME.
The MME triggers the SRVCC procedure for the voice bearer towards MSC Server.
The MSC Server initiates the Session Transfer procedure to IMS and coordinates it with the CS handover procedure to the UTRAN. And standard IMS Service Continuity procedures are applied for execution of the Session Transfer.
The MSC Server sends PS-CS handover response to MME, including CS handover command information for the UE to access the UTRAN.
The MME sends a Handover Command message to the E-UTRAN, which includes the information about the voice bearer.
This message is encapsulated within a Mobility From E-UTRA Command and sent to the UE.
The UE tunes to UTRAN and resumes its voice call.
The figure below shows a typical Physical connection for SRVCC Test.
For detailed guidance on how to use the E6621A PXT, please refer to the E6621A user's guide at
http://cp.literature.keysight.com/litweb/pdf/E6621-90002.pdf
Note that there are two LAN Ports on the rear panel of the test set (See Rear Panel Connectors ). For E-UTRAN /UTRAN interworking, LAN 2 PORT is required to exchange signaling message or packet data. LAN 1 PORT is optional, but it is still useful for other LAN operations such as protocol logging, firmware downloads or screen captures.
Before the test, you need to make the following operations:
The following steps are required to configure the test set:
Call Status
should switch to
Handover
At this point, the scenario file can be used for the SRVCC test. Phase 1 is only required to create the mobility message, which is only subject to the change of the 8960 configuration.
Using the scenario file created in Phase 1.
Call Status
should switch to
Handover
Control 1 of 2
,
LAN IP Address 2(Data+)
setting is at the bottom of
Instrument Setup
(F1) menu.
Ext EPC IP Addr
must not be identical to the
LAN IP Address
setting. When the connection is successfully set up,
Ext EPC IP Addr
can not be changed.