Last updated: January 16, 2009
|
Sets/queries the RF Generator mode:
Normal: This mode is the normal CW operating mode is in which the test set generates a CW signal. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . See FM Broadcast for more information. |
||
| Range: NORM | FMBR | ||
| NORMal | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:CONFigure FMBRoadcast" ! Sets RF Generator mode to FM Broadcast. |
||
|
Sets/queries the loss of the FM Adapter. This parameter compensates the loss by increasing the signal strength at the RF OUT ONLY port. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . See FM Broadcast for more information. |
||
| -19.75 dB | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:FMBRoadcast:ADAPter:GAIN -19.75" ! Sets FM Broadcast Adapter Gain to -19.75 dB. |
||
|
Sets/queries the FM Broadcast mode Amplitude Offset setting that is applied to the RF OUT ONLY port. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . See FM Broadcast for more information. |
||
| 0 dB | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:FMBRoadcast:CORRection:GAIN 0" ! Sets FM Broadcast Correction Gain to 0 dB. |
||
|
Sets/queries whether the FM Broadcast mode Amplitude Offset setting is applied. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . See FM Broadcast for more information. |
||
| Range: 1 | 0 | ||
| OFF | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:FMBRoadcast:CORRection:STATe 0" ! Sets FM Broadcast Correction State to OFF. |
||
|
Sets/queries the frequency at which the test set broadcasts the FM signal. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. See FM Broadcast for more information. |
||
| 98.1 MHz | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:FMBRoadcast:FREQuency 100" ! Sets FM Broadcast Frequency to 100 Hz. |
||
|
Sets/queries FM Deviation of the internal audio source. The internal audio source is the amount the modulated signal deviates from the carrier frequency. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. See FM Broadcast for more information. |
||
| 22.5 kHz | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:FMBRoadcast:FM:INTernal 22.5 kHz" ! Sets Internal FM Deviation to 22.5 kHz. |
||
|
Sets/queries the test set's internal FM frequency. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. See FM Broadcast for more information. |
||
| 1 kHz | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:FM:INTernal:FREQuency 1 kHz" ! Sets the Internal FM Frequency to 1 kHz. |
||
|
Sets/queries whether the FM Broadcast mode Internal FM Deviation setting is applied. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . See FM Broadcast for more information. |
||
| Range: 1 | 0 | ||
| 1 (ON) | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:FMBRoadcast:FM:INTernal:STATe ON" ! Sets Internal FM Deviation State to ON. |
||
|
Sets/queries the power at which the test set broadcasts the FM signal. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . See FM Broadcast for more information. When this parameters is set to > -30 and < -120, "Over Range" and "Under Range" error message is displayed respectively. |
||
| -50 dBm | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:FMBRoadcast:POWer -50 dBm ! Sets FM Broadcast Power Amplitude to -50 dBm. |
||
|
Sets/queries whether the FM Broadcast Power setting is applied. Operating mode = Test Mode and Downlink Function = CW. See CW Operating Mode . See FM Broadcast for more information. |
||
| Range: 1 | 0 | ||
| 1 (OFF) | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGENERATOR:FMBRoadcast:POWer:STATe ON" ! Sets FM Broadcast Power State to ON. |
||
|
Sets/queries RF Gen Freq .
This command is only applicable when
CALL[:CELL]:CONTrol:DOWNlink:FREQuency:AUTO
( If no units are specified the setting defaults to Hz. This command is only available in FDD Test and CW operating modes.
Note, when changing between operating modes, the |
|
OUTPUT 714;"CALL:RFGenerator:FREQuency 450 MHZ" !Set downlink channel frequency to 450 MHz. |
|
|
Sets/queries the filter that is used to filter the GPS baseband signal. A Gaussian or Rectangle filter with 10 MHz bandwidth is supported in this setting. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System . |
||
| GAUSsian | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGenerator:GPS:BFILter GAUSsian" ! Sets the type of filter to be GAUSsian |
||
|
Queries the frequency of RF source 1. This parameter is fixed at 1575.42MHz and displayed on the MUI. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System . |
||
| Requirements | ||
OUTPUT 714;"CALL:RFGenerator:GPS:FREQuency?" ! Queries the frequency of RF source 1. It will return the value:+1.57542000E+009 |
||
|
Queries the frequency of RF source 2. This parameter is fixed at 871MHz. RF source 2 is only available in those TA that use two RF Sources. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System . |
||
| Requirements | ||
OUTPUT 714;"CALL:RFGenerator:GPS:FREQuency2?" ! Queries the frequency of RF source 2. It will return the value:+8.71000000E+008 |
||
|
Sets/queries the type of GPS navigation message that is transmitted on GPS frames. Default Navigation (also called TLM): the GPS frames is filled according to the default navigation data (Alternating ones and zeros in word 3 through 10) Raw: the GPS frames is filled with PN sequence. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System . |
||
| DEFault | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGenerator:GPS:NMESsage RAW" ! Sets the type of GPS navigation message to be RAW |
||
|
Sets/queries the power at which the test set generates the GPS signal. Setting this parameter is also set the GPS State to ON. The actual power range is -125dBm to -70dBm. However, it is affected when there is an amplitude offset. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System .
|
||||
|
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset . |
||||
|
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset . |
||||
| -80 dBm | ||||
| Requirements | ||||
OUTPUT 714;"CALL:RFGenerator:GPS:POWer -80 dBm !Sets GPS Power State to ON and Amplitude to -80dBm. |
||||
|
Sets/queries the power at which the test set generates the GPS signal. The actual power range is -125dBm to -70dBm. However, it is affected when there is an amplitude offset. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System .
|
||||
|
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset . |
||||
|
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset ) |
||||
| -80 dBm | ||||
| Requirements | ||||
OUTPUT 714;"CALL:RFGenerator:GPS:POWer:AMPLitude -80 dBm ! Sets GPS Power Amplitude to -80dBm. |
||||
|
Sets/queries whether the GPS power setting is applied. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System . |
||
| Requirements | ||
OUTPUT 714;"CALL:RFGenerator:GPS:POWer:STATe ON" ! Sets GPS Power State to ON. |
||
|
Sets/queries the date type that is transmitted on GPS frames. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System . GPS Navigation Message Type = RAW. |
||
| Requirements | ||
OUTPUT 714;"CALL:RFGenerator:GPS:RAW:PPATtern PN15" ! Sets the date type to be PN15 |
||
|
Sets/queries which satellite is generating the GPS signal. Operating mode = CW. See CW Operating Mode . RF Gen Config = GPS. See Global Position System . Note: The SV ID will affect the spreading code phase. |
||
| 1 | ||
| Requirements | ||
OUTPUT 714;"CALL:RFGenerator:GPS:SVID 2 !Sets GPS satellite ID to be 2. |
||