Last updated: January 16, 2009
This section is only applicable to the lab application.
 Call Limit State 
to
 Off 
using the 
CALL:CONNected:LIMit[:STATe][:SELected]
 command.
 PRACH Signature 
as needed using the 
CALL:UPLink:PRAChannel:SMASk
 command.
 PRACH Preambles 
to at least 3 using the 
CALL:UPLink:PRAChannel:PREambles:NUMBer
 command.
 Available Subchannels (Bit Mask) 
to specify only one available subchannel using the 
CALL:UPLink:PRAChannel:ASUBchannels
 command.
 Cell Power 
as needed using the 
CALL[:CELL]:POWer[:SAMPLitude][:SELected]
 command.