The setting form of this command performs two functions: (1) sets Uplink Channel to a specific UARFCN (see CALL:UPLink:CHANnel:CHANnel ) and (2) sets uplink channel control to off (manual) (see CALL:UPLink:CHANnel:CONTrol:AUTO ). The query form of this command returns the uplink UARFCN that is used by the test set when CALL:UPLink:CHANnel:CONTrol:AUTO is set to off (manual). Note, when CALL:UPLink:CHANnel:CONTrol:AUTO is set to on (auto), the uplink UARFCN used by the test set is determined by CALL:CHANnel . The uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:UPLink:CHANnel? . This setting cannot be changed while in the active cell operating mode. Attempting to change this setting while in this mode results in an error issued and the test set will reject the change. Use the cell off operating mode when changing this value. See CALL:OPERating to select operating modes. If the |
|
Range: see CALL:UPLink:CHANnel:CHANnel |
|
| Same as setting | |
Test or Lab Application Revision: A.01 and above Test Application Revision A.05.28 and Lab Application Revision B.01.29, added 812 - 837 Test Application Revision A.08 and Lab Application Revision C.03, changed channel ranges to match 3GPP TS 25.101 v6.7.0 (previously, channels supported were: 12-287, 812-837, 4095-4270, 4375-4600, 8525-8950 and 9225-9925, resolution = 1). Test Application Revision A.09 and Lab Application Revisions C.04 and D.00, changed channel ranges to match 3GPP TS 25.101 v7.2.0 (previously channels supported were: 12, 37, 62, 87, 112, 137, 162, 187, 212, 237, 262, 287, 782, 787, 807, 812, 837, 862, 1162, 1187, 1212, 1237, 1262, 1287, 1312, 1337, 1362, 4132-4233 -- resolution = 1, 8562-8913 -- resolution = 1, 9262-9538 -- resolution = 1, 9612-9888 -- resolution = 1). Test Application Revision A.10 and Lab Application Revision D.01, added 2012 - 2338, 2362, 2387, 2412, 2437, 2462, 2487, 2512, 2537, 2562, 2587, 2612, 2637, 2662, 2687 Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, added 2887 to 3163, 3187, 3212, 3237, 3262, 3287, 3312, 3337, 3362, 3387, 3412, 3437, 3462 Lab Application Revision E.00.34 and above, added 3487 - 3587. Test Application Revision A.14 and Lab Application Revision F.00 and above, added 3612 - 3678, 3702, 3707, 3732, 3737, 3762, 3767, 3792 - 3818, 3842, 3867, 3892 - 3918, 3942, 3967
Test Application Revision A.18.00 and Lab Application Revision H.00.00 and above, added 312 to 363, 387, 412, 437, 4287 to 4413 and 462 to 512 |
|
OUTPUT 714;"CALL:UPLink:CHANnel 9755" ! Sets the uplink channel UARFCN to 9755 and selects manual control mode for uplink channel. |
|
The setting form of this command sets Uplink Channel to a specific UARFCN. Note, this uplink UARFCN is only used by the test set when CALL:UPLink:CHANnel:CONTrol:AUTO is set to off (manual). When CALL:UPLink:CHANnel:CONTrol:AUTO is set to on (auto), the uplink UARFCN used by the test set is determined by CALL:CHANnel . The query form of this command returns the uplink UARFCN that is used by the test set when CALL:UPLink:CHANnel:CONTrol:AUTO is set to off (manual). The uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:UPLink:CHANnel? . This setting cannot be changed while in the active cell operating mode. Attempting to change this setting while in this mode results in an error issued and the test set will reject the change. Use the cell off operating mode when changing this value. See CALL:OPERating to select operating modes. If the |
|
|
|
| Same as setting | |
Test Application Revision: A.06 and above Lab Application Revision: C.01 and above Test Application Revision A.08 and Lab Application Revision C.03, changed channel ranges to match 3GPP TS 25.101 v6.7.0 (previously, channels supported were: 12-287, 812-837, 4095-4270, 4375-4600, 8525-8950 and 9225-9925, resolution = 1). Test Application Revision A.09 and Lab Application Revisions C.04 and D.00, changed channel ranges to match 3GPP TS 25.101 v7.2.0 (previously channels supported were: 12, 37, 62, 87, 112, 137, 162, 187, 212, 237, 262, 287, 782, 787, 807, 812, 837, 862, 1162, 1187, 1212, 1237, 1262, 1287, 1312, 1337, 1362, 4132-4233 -- resolution = 1, 8562-8913 -- resolution = 1, 9262-9538 -- resolution = 1, 9612-9888 -- resolution = 1). Test Application Revision A.10 and Lab Application Revision D.01, added 2012 - 2338, 2362, 2387, 2412, 2437, 2462, 2487, 2512, 2537, 2562, 2587, 2612, 2637, 2662, 2687 Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, added 2887 to 3163, 3187, 3212, 3237, 3262, 3287, 3312, 3337, 3362, 3387, 3412, 3437, 3462 Lab Application Revision: E.00.34 and above, added 3487 - 3587. Test Application Revision A.14 and Lab Application Revision F.00 and above, added 3612 - 3678, 3702, 3707, 3732, 3737, 3762, 3767, 3792 - 3818, 3842, 3867, 3892 - 3918, 3942, 3967 Test Application Revision: A.18.00 and Lab Application Revision H.00.00 and above, added 312 to 363, 387, 412, 437, 4287 to 4413 and 462 to 512 |
|
OUTPUT 714;"CALL:UPLink:CHANnel:CHANnel 9755" ! Sets the uplink channel UARFCN to 9755. |
|
Sets/queries the Uplink Channel control mode.
The uplink UARFCN being used by the test set at any given time can be determined by CALL:STATus:UPLink:CHANnel? . This setting cannot be changed while in the active cell operating mode. Attempting to change this setting while in this mode results in an error issued and the test set will reject the change. Use the cell off operating mode when changing this value. See CALL:OPERating to select operating modes. |
|
| Range: 1|0 | |
OUTPUT 714;"CALL:UPLink:CHANnel:CONTrol:AUTO OFF" ! Sets uplink channel control mode to manual. |
|
THIS
COMMAND IS OBSOLETE. The Sets/queries When CALL:UPLink:CHANnel:CONTrol:AUTO is set to
on (auto), the uplink UARFCN used by the test set is determined
by this If CALL:UPLink:CHANnel:CONTrol:AUTO is set to
on (auto) and you attempt to set This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in an error issued and the test set will reject the change. Use the cell off operating mode when changing this value. See CALL:OPERating to select operating modes. |
|
| Same as setting | |
| MHZ190 | |
Test Application Revision: A.06 and above Test Application Revision A.08 and Lab Application Revision C.03, added VMHZ45 |
|
OUTPUT 714;"CALL:UPLink:CHANnel:SEParation MHZ80" |
|
Sets/queries the Uplink Dummy DCCH Data state. |
|
| *RST setting | 0 (off) |
OUTPUT 714;"CALL:UPLink:DCCHannel:DDATa OFF" |
|
| *RST setting | 0 (off) |
| Lab Application Revision H.01.00 and above | |
OUTPUT 714;"CALL:UPLink:DPCChannel:DTX:DETection On" |
|
Queries the expected initial power level for the uplink dedicated physical control channel (see Initial DPCCH TX Power ). |
|
OUTPUT 714;"CALL:UPLink:DPCChannel:POWer:INITial?" |
|
Sets/queries the the uplink DPCCH slot format to UE for UL DTX or UL DTX+DL DRX operation. |
|
| *RST setting | 1 |
OUTPUT 714;"CALL:UPLink:DPCChannel:SLOT:FORMat 1" |
|
Sets/queries the power gain control mode for the uplink dedicated physical channel (DPCH) which consists of the dedicated physical data channel (DPDCH) and the dedicated physical control channel (DPCCH). See Uplink DPCH Bc/Bd Control for details. This setting cannot be changed while in the active cell operating mode. Attempting to change this setting while in this mode results in an error issued and the test set will reject the change. Use the cell off or FDD test operating mode when changing this value. See CALL:OPERating to select operating modes. |
|
| *RST setting | 1 (on) |
Test Application Revision: A.03 and above. Lab Application Revision: A.01 and above. Test Application Revision A.07 and above, this command applies to FDD test operating mode. Lab Application Revision C.02 and above, this command applies to FDD test operating mode. |
|
OUTPUT 714;"CALL:UPLink:DPCHannel:BETA:AUTo OFF" ! Enables manual control of the DPCH power gain. |
|
Sets/queries the power gain of the dedicated physical control channel (DPCCH) when the DPCH power gain control mode is MANual (see CALL:UPLink:DPCHannel:BETA:AUTo ). See Manual Uplink DPCH Bc . This setting
cannot be changed while in the active cell operating mode.
Attempting to change this setting while in this mode results
in an error issued and the test set will reject the change.
Use the |
|
| Same as setting | |
| *RST setting | 8 |
Test Application Revision: A.03 and above. Lab Application Revision: A.01 and above. Test Application Revision A.07 and Lab Application Revision C.02, this command applies to FDD test operating mode. Lab Application Revision: D.00, range is 1 to 15 (but 1 is not recommended) Lab Application Revision D.01, range is 2 to 15 Test Application Revision A.11 and Lab Application Revisions D.02 and E.00, range is 1 to 15 (vs. 2 to 15) |
|
OUTPUT 714;"CALL:UPLink:DPCHannel:MANual:CBETa 10" ! Sets manual control of power gain for the DPCCH to 10. |
|
Sets/queries the power gain of the dedicated physical data channel (DPDCH) when the DPCH power gain control mode is MANual (see CALL:UPLink:DPCHannel:BETA:AUTo ). See Manual Uplink DPCH Bd . This setting
cannot be changed while in the active cell operating mode.
Attempting to change this setting while in this mode results
in an error issued and the test set will reject the change.
Use the |
|
| *RST setting | 15 |
Test Application Revision: A.03 and above. Lab Application Revision: A.01 and above. Test Application Revision A.07 and above, this command applies to FDD test operating mode. Lab Application Revision C.02 and above, this command applies to FDD test operating mode. |
|
OUTPUT 714;"CALL:UPLink:DPCHannel:MANual:DBETa 5" ! Sets manual control of power gain for the DPDCH to 5. |
|
Sets/queries the uplink dedicated physical channel's scrambling code. See Uplink Parameters for details. This setting cannot be changed while in the active cell operating mode. Attempting to change this setting while in this mode results in an error issued and the test set will reject the change. Use the cell off operating mode when changing this value. See CALL:OPERating to select operating modes. |
|
| Same as setting | |
OUTPUT 714;"CALL:UPLink:DPCH:SCODe 10" ! Sets the uplink DPCH scrambling code to 10. |
|
Function |
Sets/queries Enh PRACH Available Subchannels (Bitmask). This setting can only be changed when Call
Status is |
Setting |
Range: 12 characters from the set of "0" or "1" |
Query |
same as the settings |
*RST Setting |
111111111111 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:ASUBchannels 111111111111" ! Sets the Enhanced PRACH Available Access Sub Channel to 111111111111. |
|
Function |
Sets/queries EAI Configuration. This setting can only be changed when Call
Status is |
Setting |
Range: 1|On | 0 |Off |
Query |
same as the settings |
*RST Setting |
1 (On) |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:EAINdicator 1" ! Sets the EAI Configuration to On. |
|
Function |
Sets/queries NB01max. This setting can only be changed when Call
Status is |
Setting |
Range: 0 to 50 Increment: 1 |
Query |
same as the settings |
*RST Setting |
0 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:NB01:MAXimum 0" ! Sets the NB01max to 0. |
|
Function |
Sets/queries NB01min. This setting can only be changed when Call
Status is |
Setting |
Range: 0 to 50 Increment: 1 |
Query |
same as the settings |
*RST Setting |
0 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:NB01:MINimum 0" ! Sets the NB01min to 0. |
|
Function |
Sets/queries Power offset Pp-e. This setting can only be changed when Call
Status is |
Setting |
Range: -5 to 10 Increment: 1 Units: dB |
Query |
same as the settings |
*RST Setting |
0 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:POFFset:PE 0" ! Sets the Power offset Pp-e to 0. |
|
Function |
Sets/queries Enh PRACH Ramping Cycles (MMAX). This setting can only be changed when Call
Status is |
Setting |
Range: 1 to 32 Increment: 1 |
Query |
same as the settings |
*RST Setting |
2 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:POWer[:RAMP]:RCYCles[:MMAX] 2" ! Sets the Enhanced PRACH number of Ramping Cycles to 2. |
|
Function |
Sets/queries Enh PRACH Power Ramp Step. This setting can only be changed when Call
Status is |
Setting |
Range: 1 to 8 Increment: 1 |
Query |
same as the settings |
*RST Setting |
3 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:POWer[:RAMP]:STEP[:LEVel] 3" ! Sets the Enhanced PRACH Power Ramp Step Size to 3. |
|
Function |
Sets/queries Enh PRACH Preambles. This setting can only be changed when Call
Status is |
Setting |
Range: 1 to 64 Increment: 1 |
Query |
same as the settings |
*RST Setting |
64 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:PREambles:NUMBer 64" ! Sets the Enhanced PRACH Number of Preambles per Cycle to 64. |
|
Function |
Sets/queries Enh PRACH Scrambling Code word. This setting can only be changed when Call
Status is |
Setting |
Range: 0 to 15 Increment: 1 |
Query |
same as the settings |
*RST Setting |
0 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:PREambles:SCODe 0" ! Sets the Enhanced PRACH Preamble Scrambling code number to 0. |
|
Function |
Sets/queries Enh PRACH Signature, Upper (Bit Mask). This setting can only be changed when Call
Status is |
Setting |
Range: 16 characters from the set of '0' or '1' |
Query |
same as the settings |
*RST Setting |
1000000000000000 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:UPLink:EPRachannel:SMASk 1000000000000000" ! Sets the Enhanced Uplink PRACH signature Mask to 1000000000000000. |
|
Sets/queries the Available Subchannels (Bit Mask) . This setting
can only be changed when call status is |
|
Range:
0 to 111111111111 |
|
Range:
"000000000000" to "111111111111" |
|
OUTPUT 714;"CALL:UPLink:PRAChannel:ASUBchannels '111111111111'" ! Sets all twelve PRACH access subchannels avai1able for use. |
|
Sets/queries the power gain control mode for the message portion of the uplink physical random access channel (PRACH). See Uplink Parameters for details. This setting
can only be changed when call status is |
|
| *RST setting | 1 (automatic) |
OUTPUT 714;"CALL:UPLink:PRAChannel:BETA:AUTo OFF" ! Enables manual control of the PRACH power level. |
|
Sets/queries the Manual PRACH Bc . This command is only applicable when CALL:UPLink:PRAChannel:BETA:AUTo ) is set to auto. This setting
can only be changed when call status is |
|
| *RST setting | 15 |
OUTPUT 714;"CALL:UPLink:PRAChannel:MANual:CBETa 10" ! Sets manual control of power gain for the control data ! of the message portion of the PRACH to 10. |
|
Sets/queries the Manual PRACH Bd . This command is only applicable when CALL:UPLink:PRAChannel:BETA:AUTo ) is set to auto. This setting
can only be changed when call status is |
|
| *RST setting | 15 |
OUTPUT 714;"CALL:UPLink:PRAChannel:MANual:DBETa 5" ! Sets manual control of power gain for message data of ! the message portion of the PRACH to 5. |
|
Queries the expected initial power level for the uplink physical random access channel (see Initial PRACH TX Power ). |
|
OUTPUT 714;"CALL:UPLink:PRAChannel:POWer:INITial?" |
|
Sets/queries the PRACH Power Ramp Step . This setting
can only be changed when call status is |
|
OUTPUT 714;"CALL:UPLink:PRAChannel:POWer:STEP:LEVel 5" |
|
Sets/queries the PRACH Preambles . This setting
can only be changed when call status is |
|
OUTPUT 714;"CALL:UPLink:PRAChannel:PREambles:NUMBer 15" ! Sets the maximum number of preambles per ! PRACH Ramping Cycle to 15. |
|
Sets/queries PRACH Ramping Cycles (MMAX) . This setting
can only be changed when call status is |
|
OUTPUT 714;"CALL:UPLink:PRAChannel:PREambles:RCYCles 5" ! Sets the PRACH ramping cycles per PRACH access request to 5. |
|
Sets/queries the PRACH Scrambling Codeword . This parameter can not be set in active cell operating mode. |
|
OUTPUT 714;"CALL:UPLink:PRAChannel:SCODe 5" |
|
This command is obsolete, please use the CALL:UPLink:PRAChannel:SMASk command instead. Sets/queries the uplink physical random access channel's preamble signature. Changing this setting changes the CALL:UPLink:PRAChannel:SMASk setting as well. While in the active cell operating mode, this setting can only be changed when the call status is Idle. |
|
| Same as setting | |
Test Application Revision: A.02 and above, obsolete as of A.05. |
|
OUTPUT 714;"CALL:UPLink:PRAChannel:SIGNature 11" ! Set the PRACH signature to 11. |
|
Sets/queries the PRACH Signature . This setting
can only be changed when call status is |
|
Range: "0000000000000000" to "1111111111111111" (The return string is always 16 characters from the set 0 and 1) |
|
| "0000000000000001" | |
OUTPUT 714;"CALL:UPLink:PRAChannel:SMASk '0000000000000001'" |
|
Sets/queries Uplink Timing Offset . This setting cannot be changed while in the active cell operating mode. Attempting to change this setting while in this mode results in an error issued and the test set will reject the change. Use the cell off operating mode when changing this value. See CALL:OPERating to select operating modes. |
|
| Same as setting | |
OUTPUT 714;"CALL:UPLink:TIMing 16" |
|
Sets/queries Maximum Uplink Transmit Power Level . This setting
can only be changed when call status is |
|
| Same as setting | |
| 33 dBm | |
OUTPUT 714;"CALL:UPLink:TXPower:LEVel:MAXimum 24" ! Sets Maximum Uplink Transmit Power Level to +24 dBm. |
|