InfiniiSim-DCA Waveform Transformation Toolset

Flex Apps:
FlexDCA

The InfiniiSim-DCA Waveform Transformation Toolset (F-SIM or N1010A F-SIM) feature provides de-embedding and embedding capability to the FlexDCA application. Once the license is installed, access this feature from the Waveform Signal Processing tool's Simulation operators. Click Measure > Waveform Signal Processing.

You can use the Waveform Transformation Toolset to perform the following tasks:

  • Embed and de-embed fixtures, cables, probes, and other circuit elements
  • Improve measurements margins and insight
  • Simultaneously display measured and simulated waveforms
  • Perform oscilloscope, eye diagram, and jitter measurements on simulated signals

Easy to Use

  • Drag-and-drop network setup components
  • Flexible use from simple insertion loss removal/addition to accounting for all reflections between circuit elements
  • Completely integrated, no external scripts required to generate de-embed files
  • Display any combination of measured or simulated nodes at the same time, ideal for "what-if" experiments

Describe Circuit Elements

  • Import S-Parameter files (Touchstone, .cit, or .cti formats) from a TDR or VNA.
  • Define an RLC network using the built-in editor.
  • Enter a transmission line's characteristic impedance and propagation delay.
  • Define a circuit element as a simple "thru" or "open".