:CALibrate:ACAL:TIME
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:ACAL:TIME <elapsed-time>
Where <elapsed-time> is a double that indicates hours.
Description
Specifies the maximum elapsed time allowed, in hours, before a DCA-M module AutoCal is performed. The time can be entered as a double, but the entered time rounded to the nearest hour. For example, if 2.6 hours is entered, the maximum elapsed time limit is set to 3 hours. The default elapsed time is 24 hours. Entering the elapsed time as a string instead of a double, for example "4:00" results in an error.
To enable or disable automatic calibrations, use the :CALibrate:ACAL:ENABle command. To specify the maximum allowed temperature change, use the :CALibrate:ACAL:TEMPerature command.