:CALibrate:DARK:STATus:DETails?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:CALibrate:DARK:STATus:DETails? "<DCA-M-name>", "<DCA-M-channel>"
Where <DCA-M-name> is the N109x-series DCA module's name that is shown on the DCA-M block on the Hardware Diagram. For example, "N1092B-US12345678".
Where <DCA-M-channel> DCA module's optical input channel. For example, "B".
Description
Queries details concerning the dark calibration status of a N109x-series DCA-M module's optical channel. The targeted optical channel is identified by a single channel letter (for example, A, B, C, or D) and does not include a module slot number.
Example Command
:CALibrate:DARK:STATus:DETails? "N1092A-US12341678", "A"
Example Response
"Elapsed cal time has exceeded 7 days, Time of last Calibration: 01/24/2023 10:30:19, Elapsed Calibration Time: 21 days, Temperature Change: 0.25degreesC"