:CONFigure:PORT:CONNect:ALL?

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram

Query Syntax

:CONFigure:PORT:CONNect "<device-name>", "<port-name>"

Where <device-name> is a string that identifies a block on the Hardware Diagram.

Where <port-name> is a string that identifies a port on the specified block.

Query Response

"<device-name>","<port-name>"

Description

Returns two comma-separated values ("<device-name>","<port-name>") that identify a connected port. If there is no connection to this port, an empty string is returned. For example, if an N7731A (Switch 1) port A is connected to an N1092A DCA-M module the following query:

:CONFigure:PORT:CONNect:ALL? "N7731A (Switch 1)","A"

would return a response similar to:

"N1092A-US59310001,A"

If the port that you specify is an N107x-series "Clock Out" port, the returned string can identify multiple connected ports. which is connected to the "Clock In" port on multiple N1092D DCA-Ms, this query will return a string of comma separated multiple connected ports. This is a unique case of a Hardware Diagram port that can be connected to multiple ports.

Example <device-name> Arguments
Device <device-name> Argument Fields Argument Examples To Rename a Device 1
Switches
Keysight N7731A "N7731A (Switch <switch-number>)" "N7731A (Switch 1)"
"N7731A (Switch 2)"
—
Keysight N7733C "N7733C" "N7733C" —
Keysight N7734A "N7734A" "N7734A" —
DiCon GP750 "DiCon GP750 (<module-slot>:<module>)" "DiCon GP750 (SL1:M3)" 2
"DiCon GP750 (SL2:X1)"
—
DiCon GP600 "DiCon GP600 (<module>)" "DiCon GP600 (M1)" 2
"DiCon GP600 (X1)"
—
Polatis 6000 "Polatis 6000" "Polatis 6000" —
Switch (installed with custom driver) "<model number> (<serial number>)" "Acme 1200A (A12345)" — 3
DCA-M Modules
N1092-series DCA-M "<model number>-<serial number>" "N1092D-US92000003" —
N107x-series DCA-M "<model number>-<serial number>" "N1078A-US78000002" —
Fixtures
DUT Fixture "<name>" "DUT Fixture 1" :CONFigure:FIXTure:REName
WDM DUT Fixture "<name>" "WDM DUT Fixture 2" :CONFigure:FIXTure:REName
Impairments, Instrument, and Demultiplexers
Impairment "<name>" "Impairment 1" :CONFigure:IMPairment:REName
Instrument (installed with custom driver) "<model number> (<serial number>)" "Power Meter (US123456PM)" — 4
Demultiplexer "<name>" "Demux 4" :CONFigure:DEMux:REName

A dash character (—) indicates that the name of the device cannot be changed.

The module identification strings (for example, "X1" and "M1") match the module identification label shown on Switch blocks. These example strings may not match the modules installed in your switch.

A name for a Switch (model number and serial number) is defined in a Switch driver and read by FlexOTO.

A name for an Instrument (model number and serial number) is defined in your Instrument driver and read by FlexOTO.

Example <port-name> Arguments
  Input Ports 1 Output Ports 1
Switches
Keysight N7731A "1" | "2" | "3" | "4" "A"
Keysight N7733C "1" | "2" | "3" | .... "16" "A"
Keysight N7734A "1" | "2" | "3" | .... "13" "A"
DiCon GP750
X1 module "1" | "2" | "3" | "4" ... "IN 1" | "IN 2" ...
M1 module "1" | "2" | "3" | "4" ... "IN"
DiCon GP600
X1 module "1" | "2" | "3" | "4" ... "IN 1" | "IN 2" ....
M1 module "1" | "2" | "3" | "4" ... "IN"
Polatis 6000 "1" to "24" "25" to "48"
Switch (installed with custom driver) defined in driver 2 —
DCA-M Modules
N107x-series DCA-M "Data In" "Data Out"
— "Clock Out"
N1092-series DCA-M "Clock In" "Clock Out"
"A" —
"B" —
"C" —
"D" —
Fixtures
DUT Fixture — "1" | "2" | "3" ... | "8"
WDM DUT Fixture — "1"
Impairments, Instrument, and Demultiplexers
Impairment "In" "Out"
Instrument (installed with custom driver) defined in driver 3 —
Demux "In" "1" | "2" | "3" ... | "8"

Port argument strings match the port labels shown on Switch blocks. Argument strings may or may not match the label on the switch's front panel. These example strings may not match the modules installed in your switch. Use the :CONFigure:PORT:ALL? query to return all valid port names for a hardware block.

Switch measurement port argument strings are defined in your Switch driver and read by FlexOTO.

Instrument measurement port argument strings are defined in your Instrument driver and read by FlexOTO.

Examples

Command Examples for :CONFigure:PORT:CONNect:ALL?
Optical Switch Example Command Arguments for :CONFigure:PORT:CONNect 12
Keysight N7731A :CONFigure:PORT:CONNect:ALL? "N7731A Switch 1", "2"
:CONFigure:PORT:CONNect:ALL? "N7731A Switch 2", "1"
Keysight N7733C :CONFigure:PORT:CONNect:ALL? "N7733C", "6"
Keysight N7734A :CONFigure:PORT:CONNect:ALL? "N7734A", "5"
DiCon GP750 :CONFigure:PORT:CONNect:ALL? "DiCon GP750 (SL2:X1)", "12"
:CONFigure:PORT:CONNect:ALL? "DiCon GP750 (SL1:M1)", "8"
:CONFigure:PORT:CONNect:ALL? "DiCon GP750 (SL3:X1)", "28"
DiCon GP600 :CONFigure:PORT:CONNect:ALL? "DiCon GP600 (X1)", "15"
:CONFigure:PORT:CONNect:ALL? "DiCon GP600 (M1)", "4"
Polatis 6000 :CONFigure:PORT:CONNect:ALL? "Polatis 6000", "5"

Due to the variety of options available, use FlexOTO's SCPI recorder when not sure about valid parameter strings.

Maximum port number depends on installed switch module.