:CONFigure:PORT:CONNect

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram

Command Syntax

:CONFigure:PORT:CONNect "<device-name-1>","<port-name-1>","<device-name-2>","<port-name-2>"

Where <device-name> is a string name that identifies a device on the Hardware Diagram.

Where <port-name> is a string that identifies a port on the specified device.

Query Syntax

:CONFigure:PORT:CONNect "<device-name-1>","<port-name-1>","<device-name-2>","<port-name-2>"

Query Response

The command is queried, one of the following tokens is returned

1
The two specified ports are connected.
0
The two specified ports are not connected.

Description

This universal port connect command connects any two valid ports on the Hardware Diagram including:

  • An optical switch port and ports on Fixtures, DUT Fixtures, DCA-M module input channels (A, B, C, or D), Impairments, and Instruments.
  • The Clock Out port on an N1078A to an N1092D's Clock In port.
  • The Clock Out port on an N1092B to an N1092D's Clock In port.
  • The Data Out port on an N1078A to an N1092D's input channel (A, B, C, or D).

You can connect an N107x-series Clock Out port to the Clock In port on multiple N1092D DCA-Ms. This is a unique case where a port can be connected to multiple ports. When using FlexOTO's GUI, this connection can only be made when you click on the N1092D's "Clock In" port and afterward click on the N1078A's "Clock Out" port.

The following picture shows the connection between an N7734A Switch's "A" output port to an N1092B's channel A input port:

:CONF:PORT:CONNect "N7734A","A","N1092B-US78000001","A"

It makes no difference the order in which the ports are listed. For example, these two commands are equivalent:

:CONF:PORT:CONNect "N7734A", "A", "N1092B-US78000001", "A"

:CONF:PORT:CONNect "N1092B-US78000001", "A", "N7734A", "A"

Here is another example where an Impairment block has been renamed to "Fiber Spool". The command to connect an N7731A switch output port to the Impairment's input port would be similar to this:

:CONFigure:PORT:CONNect "N7731A (Switch1)","A","Fiber Spool","In"

Example <device-name> Arguments
Device <device-name> Argument Fields Argument Examples To Rename a Device 1
Switches
Keysight N7731A "N7731A (Switch <switch-number>)" "N7731A (Switch 1)"
"N7731A (Switch 2)"
—
Keysight N7733C "N7733C" "N7733C" —
Keysight N7734A "N7734A" "N7734A" —
DiCon GP750 "DiCon GP750 (<module-slot>:<module>)" "DiCon GP750 (SL1:M3)" 2
"DiCon GP750 (SL2:X1)"
—
DiCon GP600 "DiCon GP600 (<module>)" "DiCon GP600 (M1)" 2
"DiCon GP600 (X1)"
—
Polatis 6000 "Polatis 6000" "Polatis 6000" —
Switch (installed with custom driver) "<model number> (<serial number>)" "Acme 1200A (A12345)" — 3
DCA-M Modules
N1092-series DCA-M "<model number>-<serial number>" "N1092D-US92000003" —
N107x-series DCA-M "<model number>-<serial number>" "N1078A-US78000002" —
Fixtures
DUT Fixture "<name>" "DUT Fixture 1" :CONFigure:FIXTure:REName
WDM DUT Fixture "<name>" "WDM DUT Fixture 2" :CONFigure:FIXTure:REName
Impairments, Instrument, and Demultiplexers
Impairment "<name>" "Impairment 1" :CONFigure:IMPairment:REName
Instrument (installed with custom driver) "<model number> (<serial number>)" "Power Meter (US123456PM)" — 4
Demultiplexer "<name>" "Demux 4" :CONFigure:DEMux:REName

A dash character (—) indicates that the name of the device cannot be changed.

The module identification strings (for example, "X1" and "M1") match the module identification label shown on Switch blocks. These example strings may not match the modules installed in your switch.

A name for a Switch (model number and serial number) is defined in a Switch driver and read by FlexOTO.

A name for an Instrument (model number and serial number) is defined in your Instrument driver and read by FlexOTO.

Example <port-name> Arguments
  Input Ports 1 Output Ports 1
Switches
Keysight N7731A "1" | "2" | "3" | "4" "A"
Keysight N7733C "1" | "2" | "3" | .... "16" "A"
Keysight N7734A "1" | "2" | "3" | .... "13" "A"
DiCon GP750
X1 module "1" | "2" | "3" | "4" ... "IN 1" | "IN 2" ...
M1 module "1" | "2" | "3" | "4" ... "IN"
DiCon GP600
X1 module "1" | "2" | "3" | "4" ... "IN 1" | "IN 2" ....
M1 module "1" | "2" | "3" | "4" ... "IN"
Polatis 6000 "1" to "24" "25" to "48"
Switch (installed with custom driver) defined in driver 2 —
DCA-M Modules
N107x-series DCA-M "Data In" "Data Out"
— "Clock Out"
N1092-series DCA-M "Clock In" "Clock Out"
"A" —
"B" —
"C" —
"D" —
Fixtures
DUT Fixture — "1" | "2" | "3" ... | "8"
WDM DUT Fixture — "1"
Impairments, Instrument, and Demultiplexers
Impairment "In" "Out"
Instrument (installed with custom driver) defined in driver 3 —
Demux "In" "1" | "2" | "3" ... | "8"

Port argument strings match the port labels shown on Switch blocks. Argument strings may or may not match the label on the switch's front panel. These example strings may not match the modules installed in your switch. Use the :CONFigure:PORT:ALL? query to return all valid port names for a hardware block.

Switch measurement port argument strings are defined in your Switch driver and read by FlexOTO.

Instrument measurement port argument strings are defined in your Instrument driver and read by FlexOTO.

Examples

Command Examples for :CONFigure:PORT:CONNect
Optical Switch Example Command Arguments for :CONFigure:PORT:CONNect 1, 2
Keysight N7731A :CONFigure:PORT:CONNect "DUT Fixture 1", "3", "N7731A (Switch 1)", "2"
:CONFigure:PORT:CONNect "DUT Fixture 1", "2", "N7731A (Switch 2)", "1"
:CONFigure:PORT:CONNect "N7731A (Switch 2)", "A", "N7731A (Switch 1)", "4"
Keysight N7733C :CONFigure:PORT:CONNect "DUT Fixture 1", "7", "N7733C", "7"
Keysight N7734A :CONFigure:PORT:CONNect "DUT Fixture 1", "1", "N7734A", "5"
DiCon GP750 :CONFigure:PORT:CONNect "Impairment 1, "Out", "DiCon GP750 (SL2:X1)", "12"
:CONFigure:PORT:CONNect "WDM DUT Fixture 1", "3", "DiCon GP750 (SL1:M1)", "8"
:CONFigure:PORT:CONNect "DiCon GP750 (SL1:X1)", "28", "Impairment 1, "Out"
DiCon GP600 :CONFigure:PORT:CONNect "Demux 1", "3", "DiCon GP600 (X1)", "15"
:CONFigure:PORT:CONNect "WDM DUT Fixture 1", "3", "DiCon GP600 (M1)", "4"
Polatis 6000 :CONFigure:PORT:CONNect "Polatis 6000", "5", "DUT Fixture 2", "4"

Due to the variety of options available, use FlexOTO's SCPI recorder when not sure about valid parameter strings.

Maximum port number depends on installed switch module.