:CONFigure:SWITch:ALL?
Query Syntax
:CONFigure:SWITch:ALL?
Query Response
"<switch>","<switch>",..."
Description
Returns a name of a recognized optical switch located either on the Detected Switch Modules palette or placed on the Hardware Diagram. For example:
"N7734A"
If the optical switch includes multiple internal switch modules, the names of all internal switch modules are returned. Each switch name is enclosed in double-quote characters and comma-separated. For example,
"DiCon GP600 (M1),DiCon GP600 (X1)"
FlexOTO will never detect more than one supported optical switch. As a result, this query will never return a string such as this:
N7734A,DiCon GP750(SL1:M1),Polatis 6000"
To place a switch on the Hardware Diagram, use the :CONFigure:SWITch:ACTive command.