:DISPlay:CTHeme
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations
Command Syntax
:DISPlay:CTHeme {"Tungsten" | "Aluminum"}
Query Syntax
:DISPlay:CTHeme?
Description
Selects one of two user-interface themes that affects the look of FlexOTO's window and dialogs. The placing of double or single quotes around the string argument is required. Tungsten is the Factory Preset theme. A Default Setup does not change the selected theme.
This command supports the DEFault common child command.