:DISPlay:VIEW

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram

Command Syntax

:DISPlay:VIEW {PRIMary | SESSionN}

Where N identifies a specific session from 1 to 16.

Query Syntax

:DISPlay:VIEW?

The query response is: {PRIM | SESS}

Description

While FlexOTO sessions are running, use this command to selects the Hardware Diagram or Station tab to have focus. This command must be sent to FlexOTO's Hardware Diagram SCPI address instead of the address of one of the Stations. For example,

TCPIP0::<computer name>::hislip0,4880::INSTR