:INSTrument:CONNected?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:INSTrument{1:8}:CONNected?
Where {1:8} specifies one of eight Instrument blocks that can be created on the User Instruments palette.
Query Response
{1 | 0}
Description
Returns a 1 if the selected instrument driver is connected (running) which indicates that the Instrument block is available on the User Instruments palette or 0 if the instrument driver is not connected. To connect the instrument driver, use the :INSTrument:RDRiver command.
Example
state = hwdiagram.query(':INSTrument4:CONNected?')