:INSTrument:DISConnect

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram

Command Syntax

:INSTrument{1:8}:DISConnect

Where {1:8} specifies one of eight Instrument blocks that can be created on the User Instruments palette.

Description

Removes a currently installed instrument from the Hardware Diagram and from the User Instruments palette. This command is equivalent to clicking Exit in the Instrument Connection Setup dialog.

Example

hwdiagram.write(':INSTrument4:DISConnect')