:JOBS:RESults:INFO:AMODule?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:RESults:INFO:AMODule? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
A string that includes module's model number, serial number, and installed options. For example,
"N1092D,US92123456,280,40A,FS1,LOJ,PLK,IRC"
Description
For the specified Job ID returns the acquisition module's model number, serial number, and installed options. This is the module that is part of the acquisition engine for this Job ID. For more information on the acquisition engine, refer to the :JOBS:RESults:INFO:AENGine? command.
Use the following queries to determine the status of the Transition Time measurement: