:JOBS:RESults:INFO:CID?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:RESults:INFO:CID? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
{1:8}{A|B|C|D}
Returns a specific module installation slot {1:8} and channel input {A|B|C|D}. For example, 1A.
Description
For the specified Job ID, returns the clock input channel on the N109x-series acquisition module. Normally, this is the output from the N107x-series clock recovery module. If the acquisition module has integrated clock recovery, the returned channel is the channel input being measured as clock recovery is performed on this channel's input.