:RUNNing?
FlexOTO Instance:
Hardware Diagram
Query Syntax
:RUNNing?
Description
Returns the state of the FlexOTO's Station processes: 0 or 1.
- 0
- Stations are not running. The
:START root command has not been sent, or the :STOP root command has ended all running Stations.
- 1
- Stations are currently running. The
:START root command has been sent.