:STARt
Command Syntax
:STARt
Description
Launches FlexOTO's Station processes. This command is equivalent to clicking the Start button. Before sending this command, specify the number of sessions (:CONFigure:NSESsions) to create and assign the DUTs to individual sessions (:CONFigure:DUT:SESSion). To end all Station processes, use the (:STOP) root command.
Starting Stations is complex process that can consume approximately 10 seconds, so always follow a :STARt command with an *OPC? query. After the Stations are started, connecting to them, configuring their Test Programs, and returning measurements is very fast. If changes to the Test Program are needed during testing, avoid stopping and restarting Stations. Instead, use the :TPRogram subsystem commands to edit the existing Test Program and re-run the Test Program.
Use an *OPC? query to pause program execution while waiting for this command to execute.
Each session is automatically assigned a VISA HiSLIP address in numerical order as shown in the following table.
| Station Number |
HiSLIP Address |
|---|---|
| 1 | TCPIP0::<computer name>::hislip1,4880::INSTR
|
| 2 | TCPIP0::<computer name>::hislip2,4880::INSTR
|
| 3 | TCPIP0::<computer name>::hislip3,4880::INSTR
|
| 4 | TCPIP0::<computer name>::hislip4,4880::INSTR
|
| 5 | TCPIP0::<computer name>::hislip5,4880::INSTR
|
| 6 | TCPIP0::<computer name>::hislip6,4880::INSTR
|
| 7 | TCPIP0::<computer name>::hislip7,4880::INSTR
|
| 8 | TCPIP0::<computer name>::hislip8,4880::INSTR
|
| 9 | TCPIP0::<computer name>::hislip9,4880::INSTR
|
| 10 | TCPIP0::<computer name>::hislip10,4880::INSTR
|
| 11 | TCPIP0::<computer name>::hislip11,4880::INSTR
|
| 12 | TCPIP0::<computer name>::hislip12,4880::INSTR
|
| 13 | TCPIP0::<computer name>::hislip13,4880::INSTR
|
| 14 | TCPIP0::<computer name>::hislip14,4880::INSTR
|
| 15 | TCPIP0::<computer name>::hislip15,4880::INSTR
|
| 16 | TCPIP0::<computer name>::hislip16,4880::INSTR
|
Example
hwdiagram.write(':CONFigure:NSESsions 2') # Number of Stations.
hwdiagram.write(':CONFigure:FIXTure:SESSion "My DUT #1", SESSion1') # Assign DUT to Station.
hwdiagram.write(':CONFigure:FIXTure:SESSion "My DUT #2", SESSion2')
hwdiagram.write(':STARt') # Start all Stations.
hwdiagram.query('*OPC?') # About 10 second wait.
rm = visa.ResourceManager()
session1 = rm.open_resource('TCPIP0::<computer name>::hislip1,4880::INSTR')
session1.write('SYStem:DEFault') # Set Station to default setting.
session1.query('*OPC?')