:STOP
FlexOTO Instance:
Hardware Diagram
Command Syntax
:STOP
Description
Ends all running Station child processes. This command is equivalent to clicking the Stop button of FlexOTO's Hardware Diagram GUI. To launch Station processes, use the (:STARt) root command.
Use an *OPC? query to pause program execution while waiting for this command to execute.