Measure Elapsed Times for Tasks
FlexOTO Instance:
Hardware Diagram
Stations
In addition to FlexOTO's Job Timing Diagram, you can easily measure the amount of time that is consumed by specific FlexOTO tasks by using the FlexOTO's FlexOTO's SCPI Recorder. To open the SCPI Recorder, on FlexOTO's menu click Tools > SCPI Programming Tools > SCPI Recorder. Use the following steps to record the SCPI commands required for a task and then play the recorded commands at the Fast playback speed.
- In the SCPI Recorder, click
Clearand set the Playback Speed to Fast. - Click
RECto set the recorder to record. - Click the Station's
Runbutton. - When the commands are finished, click
STOPin the SCPI Recorder. - In the SCPI Recorder, click
PLAY. As each command is run, the recorder lists the elapsed time.