:ACQuire:AVERaging:COUNt
Flex Apps:
FlexPLL
Command Syntax
:ACQuire:AVERaging:COUNt <count>
<count> is an int.
Query Syntax
:ACQuire:AVERaging:COUNt?
Description
Sets the number of data points measurements to average together when averaging is turned on. Use the :ACQuire:AVERaging command to turn on averaging. The default value for the number of averages is 4. The minimum value is 2 and the maximum value is 64.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.