:ACQuire:RLENgth?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:ACQuire:RLENgth?
Description
Queries the total number of points acquired in FlexPLL's swept jitter frequency acquisition and subsequently shown in the JTF graph. The total number of points acquired is determined by the points-per-jitter frequency decade acquired (:ACQuire:FREQuency:PPDecade command) and with the following :DISPlay subsystem scaling commands:
:DISPlay:GRAPh:X:STARt(Start Frequency):DISPlay:GRAPh:X:STOP(Stop Frequency)
The minimum number of point that can be acquired is 1, the maximum number is 100, and the default number is 15.