:ACQuire:RUN
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:ACQuire:RUN
Description
Starts FlexPLL's continuous jitter transfer data acquisition. When the number of data points has been acquired, the acquisition restarts at the start jitter frequency. Specify the jitter frequency range and the number of data points-per-decade acquired using these commands:
:ACQuire:FREQuency:PPDecade(point-per-decade):DISPlay:GRAPh:X:STARt(Start Frequency):DISPlay:GRAPh:X:STOP(Stop Frequency)
To stop the acquisition, use the :ACQuire:STOP command. To delete the current acquired data points, use the :ACQuire:CDISplay command.