:ACQuire:FREQuency:PPDecade
Flex Apps:
FlexPLL
Command Syntax
:ACQuire:FREQuency:PPDecade <count>
<count> is an int.
Query Syntax
:ACQuire:FREQuency:PPDecade?
Description
Sets the number of data acquisition points-per-frequency decade in the displayed Jitter Transfer Function graph. The default value is 15. The minimum value is 1 and the maximum value is 100. The point-per-decade setting does not change when you change the acquisition (graph) start and stop frequencies. However, FlexPLL automatically adjusts the total points-per-waveform which value can be queried using :ACQuire:RLENgth?.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.
With the :STEP common child command, positive arguments result in increasing points-per-decade and negative arguments result in decreasing points.