*ESR? (Event Status Register)

Flex Apps:
FlexDCA
FlexRT
FlexPLL

Query Syntax

*ESR?

Description

Reads the Standard Status Event Register to determine the status of individual status bits. The decimal-weighted value of the register is returned. Reporting of Standard Status Event Register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically "OR"ed, which results in a Bit 5 (ESB) being set in the Status Byte Register.

To enter a mask into the enable register, use the *ESE common command.

Standard Event Status Register Commands
Register Read Write Command
Event ♦   *ESR?
Enable (mask) ♦ ♦ *ESE
Standard Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
PON URQ CME EXE DDE QYE RQL OPC
Enable
Register
               
Sets to Bit 5 (ESB) in Status Byte Register

Bit Definitions

OPC
A true indicates that an operation is complete.
RQL
Not used. Permanently set to zero.
QYE
A true indicates that a query error has been detected.
DDE
A true indicates that a device-dependent error has been detected.
EXE
A true indicates that an execution error has been detected.
CME
A true indicates that a command error has been detected.
URQ
Not used. Permanently set to zero.
PON
A true indicates that an off-to-on transition has occurred.