*TRG (Trigger)
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
*TRG
Description
Acquires data for the active waveform display, if the trigger conditions are met, according to the current settings. The *TRG common command has the same effect as the :ACQuire:RUN command.