:DATA:PLLModel:ASCii:YDATa?
Flex Apps:
FlexPLL
Query Syntax
:DATA:PLLModel:ASCii:YDATa?
Query Response
The data is returned as comma-separated values.
Description
Returns the y-axis PLL model data from a Response or Response Memory in ASCII. Use the :DATA:PLLModel:SOURce command to select the the model plot from which to return the data.
This is the Jitter amplitude in dB. The data is sent as comma-separated values starting from the graticule's left side and progressing to the right side. Use the :DATA:PLLModel:ASCii:XDATa? query to return the x-axis data. Use the :DATA:PLLModel:POINts? query to return the number of points contained in the array. An example program is located in this subsystem's introduction.