:DATA Subsystem
FlexPLL's :DATA (Data) subsystem allows you to return the X and Y data points as well as the total number of points for a displayed plot. The plot can be a Response, Response (Model), Memory, or Memory (Model) plot.
Returning Response and Memory Data
Use the :DATA:SOURce command to select the Response or Memory plot for which you want to return data. A Response and Memory plot must be displayed before you can return data for the plot. Use the following :RESPonse subsystem command to display Response plots:
Use the following :RMEMory subsystem commands to display Memory plots:
Use the :DATA:POINts command to return the number of data points in the selected plot.
Use the :DATA:STATus? query to determine the validity of the plot data.
To return Response or Memory plot values in ASCii, use:
:DATA:ASCii:XDATa?to query for X values:DATA:ASCii:YDATa?to query for Y values
To return Response or Memory plot values in double floats, use:
:DATA:DOUBle:XDATa?to query for X values:DATA:DOUBle:YDATa?to query for Y values
Returning Response (Model) and Memory (Model) Data
Use the :DATA:PLLModel:SOURce command to select the model plot for which you want to return data. A Response (Model) and Memory (Model) plot must be displayed before you can return data for the plot.
Use the following :RESPonse subsystem commands to display Response Model plots:
Use the following :RMEMory subsystem commands to display Memory Model plots:
Use the :DATA:PLLModel:POINts command to return the number of data points in the selected plot.
Use the :DATA:PLLModel:STATus? query to determine the validity of the plot data.
To return Response or Memory plot values in ASCii, use:
:DATA:PLLModel:ASCii:XDATa?to query for X values:DATA:PLLModel:ASCii:YDATa?to query for Y values
To return Response or Memory plot values in double floats, use:
:DATA:PLLModel:DOUBle:XDATa?to query for X values:DATA:PLLModel:DOUBle:YDATa?to query for Y values
ASCII Data Example Program
The following Python program returns ASCii x and y data values for the JTF plot in Memory 1. The x and y values are displayed for each data point.
model_JTF_ascii_transfer.py
# -*- coding: utf-8 -*-
""" This script transfers Memory 1 (Model) ASCII JTF data from the FlexPLL
application. The source is response memory 1.
The data is returned in binary format using ':DATA:PLLModel:ASCii:XDATa?' and
':DATAPLLModel:ASCii:XDATa?'. """
import pyvisa as visa # import VISA library
ADDRESS = 'TCPIP0::localhost::hislip1,4880::INSTR'
def open_flexpll_connection(address):
""" Opens visa connection to FlexPLL. """
print('Connecting to FlexPLL ...')
try:
rm = visa.ResourceManager()
connection = rm.open_resource(address)
connection.timeout = 20000 # Set connection timeout to 20s
connection.read_termination = '\n'
connection.write_termination = '\n'
inst_id = connection.query('*IDN?')
print('\nFlexPLL connection established to:\n' + inst_id, flush=True)
except (visa.VisaIOError, visa.InvalidSession):
print('\nVISA ERROR: Cannot open instrument address.\n', flush=True)
return None
except Exception as other:
print('\nVISA ERROR: Cannot connect to instrument:', other, flush=True)
print('\n')
return None
return connection
def get_data_points(FlexPLL):
""" Returns ASCii x and y data for response memory.
"""
xdata = []
ydata = []
FlexPLL.write(':DATA:PLLModel:SOURce JTF1')
points = FlexPLL.query(':DATA:PLLModel:POINts?')
xdata = FlexPLL.query(':DATA:PLLModel:ASCii:XDATa?').split(',')
ydata = FlexPLL.query(':DATA:PLLModel:ASCii:YDATa?').split(',')
xypoints = list(zip(xdata, ydata))
return points, xypoints
FlexPLL = open_flexpll_connection(ADDRESS)
points, xypoints = get_data_points(FlexPLL)
print('\n\nLength of JTF Response data: {0:s} points.\n'.format(points))
for i, point in enumerate(xypoints, 1):
print('{0:d}. x = {1:s} Hz, y = {2:s} dB'.format(i, point[0], point[1]))
FlexPLL.write(':SYSTem:GTLocal')
FlexPLL.close()
Binary Data Example Program
The following Python program returns binary x and y data values (doubles) for the Model JTF plot in Memory 1. The x and y values are displayed for each data point. Notice that FlexPLL's current byte order (endianness) setting is saved, set to little-endian for the script, and then restored to FlexPLL's original setting.
memory1_JTF_binary_transfer.py
# -*- coding: utf-8 -*-
""" This script transfers Memory 1 (Model) binary JTF dat from the FlexPLL
application. The data is returned in binary format using
':DATA:PLLModel:DOUBle:XDATa?' and ':DATA:PLLModel:DOUBle:XDATa?'.
Requires that JTF plots for Response Memory 1 must be displayed before
script is run. """
import pyvisa as visa # import VISA library
ADDRESS = 'TCPIP0::localhost::hislip1,4880::INSTR'
def open_flexpll_connection(address):
""" Opens visa connection to FlexPLL. """
print('Connecting to FlexPLL ...')
try:
rm = visa.ResourceManager()
connection = rm.open_resource(address)
connection.timeout = 20000 # Set connection timeout to 20s
connection.read_termination = '\n'
connection.write_termination = '\n'
inst_id = connection.query('*IDN?')
print('\nFlexPLL connection established to:\n' + inst_id, flush=True)
except (visa.VisaIOError, visa.InvalidSession):
print('\nVISA ERROR: Cannot open instrument address.\n', flush=True)
return None
except Exception as other:
print('\nVISA ERROR: Cannot connect to instrument:', other, flush=True)
print('\n')
return None
return connection
def get_data_points():
""" Returns binary x and y data for response memory. """
global FlexPLL
xdata = []
ydata = []
FlexPLL.write(':DATA:PLLModel:SOURce JTF1')
points = int(FlexPLL.query(':DATA:PLLModel:POINts?'))
endiansetting = FlexPLL.query(':SYSTem:BORDER?')
FlexPLL.write(':SYSTem:BORDER LENDian')
FlexPLL.read_termination = ''
FlexPLL.write_termination = ''
command = ':DATA:PLLModel:DOUBle:XDATa?'
xdata = FlexPLL.query_binary_values(command, datatype='d', container=list, is_big_endian=False, header_fmt='ieee')
command = ':DATA:PLLModel:DOUBle:YDATa?'
ydata = FlexPLL.query_binary_values(command, datatype='d', container=list, is_big_endian=False, header_fmt='ieee')
FlexPLL.read_termination = '\n'
FlexPLL.write_termination = '\n'
FlexPLL.write(':SYSTem:BORDER ' + endiansetting)
xypoints = list(zip(xdata, ydata))
return points, xypoints
FlexPLL = open_flexpll_connection(ADDRESS)
points, xypoints = get_data_points()
print('\n\nLength of JTF Response data: {0:d} points.\n'.format(points))
for i, point in enumerate(xypoints, 1):
print('{0:d}. x = {1:e} Hz, y = {2:f} dB'.format(i, point[0], point[1]))
FlexPLL.write(':SYSTem:GTLocal')
FlexPLL.close()