:DATA:PLLModel:SOURce
Flex Apps:
FlexPLL
Command Syntax
:DATA:PLLModel:SOURce {JTF1 | OJTF1 | MJTFN | MOJTfN}
Query Syntax
:DATA:PLLModel:SOURce?
Where N identifies one of four {1:4} possible response memories.
Description
Selects a Model plot (Model JTF or Model OJTF) from which to return x and y-axis data. To select to return Response or Response Memory data, use the :DATA:PLLModel:SOURce command.
| Argument | Definition |
|---|---|
| JTF1 | The JTF Response data acquired during a measurement sweep |
| OJTF1 | The OJTF Response data acquired during a measurement sweep |
| MJTF1 | Model JTF data for Memory 1 |
| MOJTf1 | Model OJTF data for Memory 1 |
| MJTF2 | Model JTF data for Memory 2 |
| MOJTf2 | Model OJTF data for Memory 2 |
| MJTF3 | Model JTF data for Memory 3 |
| MOJTf3 | Model OJTF data for Memory 3 |
| MJTF4 | Model JTF data for Memory 4 |
| MOJTf4 | Model OJTF data for Memory 4 |