:DATA:SOURce
Flex Apps:
FlexPLL
Command Syntax
:DATA:SOURce {RESPonse1| RMEMoryN}
Where N identifies one of four {1:4} possible response memories.
Description
Selects the source (Response or Response Memory) from which to return Response plot x and y-axis data. To select to return data for a Model plot (Model JTF and Model OJTF) , use the :DATA:PLLModel:SOURce command.