:DISK:DWIZard:SMResults
Flex Apps:
FlexPLL
Command Syntax
:DISK:DWIZard:SMResults {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add a screen capture of the entire FlexDCA display (Entire UI Screen Capture.png).
If a displayed dialog is outside FlexDCA's window, it will not be included in the screen image capture. Use the Windows Print Screen function instead.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:SMResults?
Query Response
{1 | 0}
Requires FlexPLL revision A.06.80 and above.