:DISK Documentation Wizard Commands
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Configures and saves a Documentation Wizard file (.zip). Use the :DISK:DWIZard:FNAMe command to specify the name of saved file and the :DISK:DWIZard:SAVE command to actually save the file. To select the type of information that is saved in the zip file, use the commands shown in the following table.
| Option | Saved in Zip File |
|---|---|
| :DWIZard:SSCReen command (Screen Capture) | Screen capture of entire display (Entire UI Screen Capture.png) |
| :DWIZard:SSETup command (Instrument Setup) | Instrument state file (InstrumentSetup.setx) |
| :DWIZard:SMResults command (Measurement Results Window Data) | Saves all results to a CSV file. A screen capture of the window is also saved (??.csv) |
| :DWIZard:SRESponses command (Response Graph Window Data) | Saves a waveform file for each response displayed. A screen capture of the panel is also saved. By default, the responses are saved in the internal format. You can clear this setting to save data in the format. (???.???) |
| :DWIZard:SSINfo command (System Information) |
System information shown in the Help > About dialog (SystemInfo.txt) |
Example
:DISK:DWIZard:SSCReen ON :DISK:DWIZard:SSETup ON :DISK:DWIZard:SSINfo OFF :DISK:DWIZard:RESults:SDATa ON :DISK:DWIZard:FNAMe "%USER_DATA_DIR%\Documentation Results\DocumentationResults_PAM4.zip" :DISK:DWIZard:SAVe *OPC?