:DISK:DWIZard:WAVE:IINTernal
Flex Apps:
FlexDCA
FlexPLL
Command Syntax
:DISK:DWIZard:WAVE:IINTernal {ON | OFF}
Description
When saving Response Graph Window Data to a Documentation Wizard zip file (:DWIZard:SAVE), this command adds an additional waveform file to the standard waveform file type that is already saved in the zip file. The following command arguments are used:
ON- Includes internal format waveform files in Documentation Wizard zip file. This is the default setting.
OFF- Excludes internal format waveform files from being included in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:WAVE:IINTernal?
Query Response
{1 | 0}
Requires FlexPLL revision A.05.80 and above.