:DISPlay:GRAPh:Y:AUTO
Flex Apps:
FlexPLL
Command Syntax
:DISPlay:GRAPh:Y:AUTO
Description
For FlexPLL's graph of the Jitter Transfer Function, apply an offset to the graph's Y-axis in dB. The default value is -40 dB. To graph's amplitude range, use the :DISPlay:GRAPh:Y:RANGe command.
Example Command Sequence
:DISPlay:GRAPh:X:CENTer 10E6; :DISPlay:GRAPh:X:SPAN 20E6; :DISPlay:GRAPh:Y:RANGe 60E6; :DISPlay:GRAPh:Y:OFFSet 10;